Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
NPS-Slide4

All series of the NPS product range feature a universal input enabling them to be used anywhere in the world. They also come pre-certified with both Medical and ITE safety approvals. All models are comprehensively protected against overload and short-circuit conditions. Users also have the option of an enclosure kit to ensure maximum component protection. Other features include an adjustable output voltage and a demonstrated mean time between failures of more than 550,000 hours.

PTM Published on: 2011-05-06