Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
DisplayPort Overview Slide 6
Computer chipsets need to support multiple display interfaces including DVI and/or HDMI. On the chipset, this is achieved using only one set of AC-coupled I/Os capable of interfacing in multiple data format encoding schemes such as PCI Express, DVI, HDMI and DisplayPort. Current chipsets by Intel, AMD and nVidia implement re-configurable IOs.
PTM Published on: 2011-11-02