Open the source code file lab 3 mpu_runtime.c and use the comments as a guide. Fill in the blanks and get the code to build. Don’t worry the solution code is also included in case it’s needed. Once the code builds, if it is running properly, the LED should toggle to show the access violations occurring. Use a breakpoint and the memory window to observe that the write to address 0x6002 does not occur and the system issues an NMI when this access is attempted.