Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
MSP430FR5969 LaunchPad Part 8 Slide 7

This is where the next lab begins. The source code for the lab, as well as the complete series of power point presentations is available from the link shown on this slide. An easy way to find it is to go to the processors.wiki.ti.com site and then search for the term FR59xx Training Workshop. On the wiki page browse to the LaunchPad section and then download the lab zip file from the link marked “lab material.” Upon opening the zip file, copy and paste the folder lab3_MPU_runtime into a workspace directory. Now the project for the lab is set up.

PTM Published on: 2014-06-24