Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Lumisil Cap-Touch Sensor Competitive Comparison

As an example, taking a look at competitive comparison of IS31CS8974 MCU or IS31SE5117 sensor to the pin compatible competitor solution, the engineer should emphasize the larger Flash memory, wider applicability of Shield driver for liquid immunity, availability of LIN compatible interface, wider temperature range and the lower power consumption due to lower sleep mode and lower wake-on-touch mode standby current.