Maker.io main logo

How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

31

2025-08-26 | By DFRobot

Arduino ESP32

Hello community members,

Have you ever wanted to run YOLOv8 on a compact, affordable device? This tutorial is your gateway to running YOLOv8, the state-of-the-art object detection model, on the Unihiker single-board computer. Designed for Python enthusiasts and embedded systems developers.

This tutorial guides you through running YOLOv8 on the Unihiker, a next-gen open-source hardware platform designed for Python learning and usage. YOLOv8, the latest object detection model by Ultralytics, combines high accuracy and speed, making it ideal for real-time applications. However, its resource demands pose challenges for lightweight devices. The Unihiker, equipped with an RK3308 Arm 64-bit quad-core processor, provides a compact, cost-effective solution for deploying YOLOv8. You'll learn to set up the environment, install necessary libraries, and optimize performance by converting the model to ONNX format. This project is perfect for those seeking practical experience in embedded systems and AI.

1. Introduction

1.1 yolov8

As object detection technology continues to expand into various fields, more industrial and commercial users are turning to YOLO for real-time detection, object tracking, and other applications. In 2023, Ultralytics released YOLOv8, which has attracted significant attention. YOLOv8 offers higher detection accuracy and speed but requires substantial computational resources, potentially causing lagging issues on lightweight computing devices. While high-performance computers can meet YOLO's demands, they are often bulky and inconvenient for portability and deployment.

YOLOv8 (You Only Look Once version 8) is the latest version of the YOLO object detection model launched by Ultralytics. It has the following features:

1. High Accuracy and Speed: YOLOv8 enhances detection speed while maintaining high accuracy, making it ideal for real-time applications.

2. Multi-task Support: Besides object detection, YOLOv8 also supports object classification, semantic segmentation, and other tasks.

3. Lightweight Design: Although it requires considerable computational resources, optimization and acceleration techniques enable efficient operation on embedded devices.

YOLOv8 is widely used in fields such as intelligent security, autonomous driving, industrial inspection, and medical image analysis, significantly boosting automation and intelligence levels in these areas.

1.2 Introduction to Unihiker Hardware

The Unihiker is a next-generation, open-source hardware platform specifically designed for Python learning and usage. It features a single-board computer architecture with an integrated LCD color screen, WiFi, Bluetooth, various common sensors, and numerous expansion interfaces. It also comes with a built-in Linux operating system and Python environment, pre-installed with commonly used Python libraries, making it easy for teachers and students to conduct Python teaching with just two simple steps.

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

The Unihiker is based on the RK3308 Arm 64-bit quad-core processor, with a main frequency of up to 1.2GHz. It is equipped with 512MB DDR3 memory and a 16GB eMMC hard drive, running the Debian 10 operating system. It supports 2.4G Wi-Fi and Bluetooth 4.0, utilizing the RTL8723DS chip. The Unihiker also integrates a GD32VF103C8T6 RISC-V coprocessor, with a main frequency of 108MHz, 64KB Flash, and 32KB SRAM.

The Unihiker includes various onboard components such as a Home button, A/B buttons, and a 2.8-inch touch-enabled color screen with a resolution of 240x320. The device also features a capacitive silicon microphone, a PT0603 phototransistor light sensor, a passive buzzer, and a blue LED. Additionally, it has an ICM20689 six-axis sensor, which includes a three-axis accelerometer and a three-axis gyroscope.

In terms of interfaces, the Unihiker offers multiple connectivity options. It has a USB Type-C interface for connecting the CPU to a PC for programming or powering the main board. There is also a USB Type-A interface for connecting external USB devices. Moreover, the board includes a microSD card slot for expanding storage, a 3Pin I/O supporting three 10-bit PWM and two 12-bit ADC channels, an independent 4Pin I2C interface, and 19 independent I/O golden fingers compatible with micro:bit, supporting various communication protocols and functions.

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

1.3 Running YOLOv8 Object Detection on the Unihiker

In this article, we will use the Unihiker, developed by DFRobot, to run YOLOv8 and attempt to accelerate it by converting it to the ONNX format.

Deploying YOLOv8 on the Unihiker has significant practical and educational implications:

1. Portability and Deployment Flexibility: The Unihiker's compact form factor makes it easy to embed in space-constrained devices for portable object detection deployment. Compared to large computers, the Unihiker is more suitable for on-site and mobile scenarios.

2. Cost-Effectiveness: The Unihiker is relatively low-cost, making it suitable for budget-constrained projects and educational purposes. Running YOLOv8 on the Unihiker allows for low-cost object detection application development and experimentation.

3. Learning and Experimentation Platform: The Unihiker offers a rich set of interfaces and onboard components, making it an ideal platform for learning and experimentation. By running YOLOv8 on the Unihiker, students and developers can gain a deeper understanding of the integration of embedded systems and artificial intelligence, and learn to apply optimization and acceleration algorithms in resource-constrained environments.

4. Technical Challenges and Innovation: Running YOLOv8 on the resource-limited Unihiker requires overcoming challenges related to computational performance and memory limitations. This provides developers with an opportunity to explore and innovate by trying various optimization techniques, such as model compression, quantization, and hardware acceleration.

2. Preparation: Environment Setup for Running YOLOv8

To successfully run YOLOv8 on the Unihiker, we will use the library provided by Ultralytics for deployment. First, we need to ensure that the Python environment on the Unihiker meets the requirements for YOLOv8, specifically that the Python version is upgraded to 3.8 or higher. We recommend using MiniConda for version management, as it allows for easy switching and management of different Python environments.

The general steps are as follows:

1. Install MiniConda: First, download and install MiniConda on the Unihiker. MiniConda is a lightweight Python distribution designed to simplify the management of Python environments and package installations.

2. Create a New Environment: Use MiniConda to create a new virtual environment with Python 3.8 or higher. This ensures compatibility by isolating the YOLOv8 deployment from the system's default Python environment.

3. Activate the Environment: Activate the newly created virtual environment to make it the current working environment.

4. Install the Ultralytics Library: In the activated virtual environment, use the pip command to install the official YOLO library provided by Ultralytics. This will download and install all necessary dependencies and components, allowing us to run YOLOv8 smoothly.

Following these steps, we can successfully deploy YOLOv8 on the Unihiker, leveraging its powerful object detection capabilities. This method ensures efficient operation of YOLOv8 and facilitates environment management and version control, providing a stable foundation for subsequent development and experimentation. Additionally, using MiniConda for version management allows us to flexibly meet different project requirements for Python environments, enhancing development efficiency.

Here are the detailed steps:

Step 1: Check the Current Python Version

In the terminal, input:

Copy Code
python --version

The terminal should display:

Python 3.7.3

Since Ultralytics does not support lower Python versions, we need to upgrade Python. We choose to use MiniConda for version management and upgrading.

Note: Do not use Anaconda, as it may cause errors on the Unihiker.

Step 2: Download MiniConda

In the terminal, input:

Copy Code
wget https://github.com/conda-forge/miniforge/releases/latest/download/Miniforge3-Linux-aarch64.sh

After downloading, the terminal should display:

Saved “Miniforge3-Linux-aarch64.sh” [74300552/74300552])

Step 3: Install MiniConda

In the terminal, input:

Copy Code
sudo bash Miniforge3-Linux-aarch64.sh

Follow the prompts to press the ENTER key or type yes as needed. Finally, the terminal should display:

Added mamba to /root/.bashrc

==> For changes to take effect, close and re-open your current shell. <==

Thank you for installing Miniforge3!

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

In the terminal, input:

Copy Code
source ~/.bashrc

When the installation is complete, input:

Copy Code
conda

Terminal display

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

Step 4: Activate Conda

In the terminal, input:

Copy Code
conda activate

You should see the terminal display:

root@unihiker:

Change to

(base) root@unihiker:~

You have successfully activated conda

Step 5: Create a YOLO Environment in Conda

Name the environment yolo and select Python version 3.11. In the terminal, input:

Copy Code
conda create -n yolo python=3.11

During the process, the terminal will display:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

Input y to proceed. After setting up the environment, the terminal will display:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

Step 6: Activate the yolo environment

In the terminal, input:

Copy Code
conda activate yolo

You should see the terminal display:

root@unihiker:

Change to

(base) root@unihiker:~

You have successfully activated conda

Step 7: Install utralytics

In the terminal, input:

Copy Code
pip install ultralytics

After completion, the terminal displays:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

Step 8: Install Pillow

In the terminal, input:

Copy Code
pip install pillow

If installed, the terminal displays:

Requirement already satisfied: pillow in /root/miniforge3/envs/yolo/lib/python3.11/site-packages (10.3.0)

Step 9: Install OpenCV

In the terminal, input:

Copy Code
pip install opencv-python

If installed, the terminal displays:

Requirement already satisfied: opencv-python in /root/miniforge3/envs/yolo/lib/python3.11/site-packages (4.9.0.80)

Requirement already satisfied: numpy>=1.21.2 in /root/miniforge3/envs/yolo/lib/python3.11/site-packages (from opencv-python) (1.26.4)

3. Quick Start: Running Native YOLOv8

The YOLOv8 object detection model comes in five variants, all trained on the COCO dataset. The suffixes and corresponding model performance are as follows:

n: Nano (ultra-lightweight)

s: Small

m: Medium

l: Large

x: Extra Large

Each model variant offers a balance between performance and computational requirements, allowing you to choose the one that best fits your specific needs and available resources.

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

Due to the limited performance of the Unihiker, we will only use the native YOLOv8n for image object detection tasks. YOLOv8n is the lightest model in the YOLOv8 series, capable of performing object detection tasks with lower computational resources and faster speed while maintaining accuracy, making it very suitable for resource-constrained application scenarios.

Below are the specific steps:

Step 1: Create and Enter the yolo Directory

In the terminal, input:

Copy Code
mkdir yolo
cd yolo

Step 2: Create a Python File

Create a file named quick_start.py

Sample code:

CODE

Copy Code
Python
from ultralytics import YOLO 
# Load a pretrained YOLO model (recommended for training) 
model = YOLO("yolov8n.pt") 
# Perform object detection on an image using the model
 results = model("https://ultralytics.com/images/bus.jpg") 
# Save results to disk 
results[0].save(filename=f"result_bus.jpg")

Step 3: Ensure the YOLO Environment is Activated

In the terminal, input:

Copy Code
conda activate yolo

You should see the terminal display:

(yolo) root@unihiker:~/yolo#

Step 4: Run the Python Script

In the terminal, input:

Copy Code
python quick_start.py

You should see the terminal display:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

Using the native YOLOv8n model for inference on a single image takes approximately 27 seconds, which is relatively slow. At this point, several new files have appeared in our directory:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

You can see that Ultralytics automatically downloaded yolov8n.pt, which is the weight file for YOLOv8n. It also downloaded the image bus.jpg, which is the picture we prepared for YOLO inference, as shown below:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

Finally model was inferred, storing the results as result_bus.jpg:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

4. Optimization: Converting to ONNX Format

When running the native YOLOv8n, the speed is very slow, so we need to convert its format to accelerate its performance. This section describes how to convert yolov8n.pt to ONNX format to speed up execution. Below are the detailed steps:

Step 1: Move to the yolo directory created in the previous section

In the terminal, input:

cd yolo

Step 2: Create a Python file named export_onnx.py, with the following code:

CODE

Copy Code
Python 
from ultralytics import YOLO
# Load a model 
model = YOLO("yolov8n.pt") 
# load an official model 
# Export the model 
model.export(format="onnx")

Step 3: Ensure the YOLO environment is activated

In the terminal, input:

Copy Code
conda activate yolo

You should see the terminal display change to:

(yolo) root@unihiker:~/yolo#

Step 4: Run the python script you wrote

In the terminal, input:

Copy Code
python export_onnx.py

You should see the terminal display:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

As you can see, to convert formats, you need to install the ONNX library, which Ultralytics does automatically. Finally, the converted file is automatically saved as yolov8n.onnx:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

Step 5: Write the files that run the onnx model

Create the predict_onnx.py file and write the following code:

CODE

Copy Code
Python 
from ultralytics import YOLO
# Load the exported NCNN model 
onnx_model = YOLO("yolov8n.onnx", task = 'detect')
# Run inference
results = onnx_model("https://ultralytics.com/images/bus.jpg") 
# Save results to disk
results[0].save(filename=f"result_bus_onnx.jpg")

Step 6: Run inference code

In the terminal, input:

Copy Code
python predict_onnx.py

You should see the terminal display:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

Prediction results are generated in the directory:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

As you can see, object detection with the onnx model takes about 20 seconds, which is 7 seconds faster than the native model.

5. Further optimization: Reduce the size of the input image

It can be seen that the current inference speed is still slow.

If you want to increase the speed of inference, you can reduce the size of the input image. When exporting the ONNX model, we can set the parameter imgsz to specify the size of the input image. If the size of the input image is uncertain, we can also set the dynamic parameter to True. In this case, the exported ONNX model can accept any size of image input for inference. The specific steps are as follows:

Step 1: Move to the yolo directory created in the previous section

In the terminal, input:

cd yolo

Step 2: Create a Python file called export_onnx.py with the following code

CODE

Copy Code
Python 
from ultralytics import YOLO 
# Load a model
model = YOLO("yolov8n.pt") # load an official model 
# Export the model 
model.export(format="onnx", dynamic = True)

Step 3: Confirm the yolo environment is activated

In the terminal, input:

Copy Code
conda activate yolo

You should see the terminal display: (yolo) root@unihiker:~/yolo#

Step 4: Run the python script

In the terminal, input:

Copy Code
python export_onnx.py

You should see the terminal display:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

As you can see, to convert formats, you need to install the ONNX library, which Ultralytics does automatically. Finally, the converted file is automatically saved as yolov8n.onnx:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

Step 5: Write the files that run the onnx model

Create the predict_onnx.py file and write the following code:

CODE

Copy Code
Python 
from ultralytics import YOLO 
import cv2 
# Load the exported NCNN model 
onnx_model = YOLO("yolov8n.onnx", task = 'detect') 
image = cv2.imread('bus.jpg') 
print(image.shape) 
# Run inference 
print('original') 
results = onnx_model("bus.jpg") 
results[0].save(filename='bus_640.jpg') 
print(448) 
results = onnx_model("bus.jpg", imgsz = 448) 
results[0].save(filename='bus_448.jpg') 
print(320) 
results = onnx_model("bus.jpg", imgsz = 320) 
results[0].save(filename='bus_320.jpg') 
print(256) 
results = onnx_model("bus.jpg", imgsz = 256) 
results[0].save(filename='bus_256.jpg') 
print(128) 
results = onnx_model("bus.jpg", imgsz = 128) 
results[0].save(filename='bus_128.jpg') 
print(64) 
results = onnx_model("bus.jpg", imgsz = 64) 
results[0].save(filename='bus_64.jpg')

In this code, we test the operation of the raw size image, the 448 size image, the 320 size image, the 256 size image, the 128 size image, and the 64 size image.

Step 6: Run inference code

In the terminal, input:

Copy Code
python predict_onnx.py

You should see the terminal display:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

The size of the original image is 1080*810, and the maximum predicted size of the original yolov8n is 640, which takes about 22 seconds. The results are as follows:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

If the input size is 448, it takes about 3.5 seconds. The results are as follows:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

If the input size is 320, it takes about 2.2 seconds. The results are as follows:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

If the input size is 256, it takes about 0.8 seconds. The results are as follows:

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

When the input size is 128, it takes about 0.4 seconds.

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

If the input size is 64, it takes about 0.1 seconds.

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

It can be summarized as follows:

Notice: the performance was tested on bus.jpg. Maybe you need more tests if you have your own dataset.

Image of How to Run YOLOv8 Object Detection on Unihiker Single Board Computer

Conclusion

As you can see, you can run yolov8n with simple code using the UNIHIKER.

If you use the UNIHIKER for image object detection, you can consider using a 448 resolution input. In this case, the processing time of an image is about 3.5 seconds, and the performance is excellent.

If the UNIHIKER is used for fast detection or video detection, limited to the computing power of the line board, it is recommended to use 128 resolution input; in this case, the processing time of an image is about 0.4 seconds.

Want to explore more projects, share your creations, or connect with like-minded enthusiasts? Visit the UNIHIKER official website for the latest updates, tutorials, and resources. Don’t forget to join the UNIHIKER Discord community to exchange ideas, get support, and collaborate on exciting new projects.

🎮 Join UNIHIKER Discord: https://discord.gg/PVAWBMPwsk

Happy coding! 😊

Número de parte del fabricante DFR0706-EN
UNIHIKER IOT PROGRAMMING SBC
DFRobot
$85.00
Ver más Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.