AI Bunny is a cute, educational, interactive companion in a 3D-printed bunny enclosure. It listens, speaks, responds, teaches—practicing language, storytelling, educational games, answering questions. This DIY device brings edge AI to life for kids and grownups.
Huskylens AI Vision Sensor can be used in the FIRST Tech Challenge Game. In this article, we will show how to use Huskylens AI Camera to identify April Tag. Tag Recognition function can detect tags, and learn, recognize, track specified tags. These tags are called April Tags.
This tutorial is ideal for students, hobbyists, or educators who want to integrate precise distance sensing into projects such as robotics, automation, obstacle detection, or smart measuring tools.
This project is to connect an external USB camera on UNIHIKER and use the camera to recognize the object, find the square object in the frame and frame it out.
This project is to connect an external USB camera on UNIHIKER and use the camera to recognize the hands and draw keypoints on it.
The UNIHIKER-based Yolo license plate recognizer uses a USB camera and YOLO model for fast, accurate recognition, enabling smart vehicle monitoring, efficiency, and security.
The UNIHIKER K10 is now fully compatible with major programming platforms.
As Internet of Things (IoT) applications continue to evolve, developers using the ESP32 series often face challenges such as congested 2.4GHz bands, data transmission bottlenecks, and inefficient multi-device collaboration.
When working on the UNIHIKER K10 AI vision recognition project, we often need to recognize our own face or point the camera in a different direction. However, since the K10's camera is fixed on the board, this can be difficult. To solve this, we can use a 24-pin FPC Extension Board and an FPC cable.
Have you ever wanted to run YOLOv8 on a compact, affordable device? This tutorial is your gateway to running YOLOv8, the state-of-the-art object detection model, on the Unihiker single-board computer. Designed for Python enthusiasts and embedded systems developers.