Maker.io main logo

Build a 6-DOF Arduino Robotic Arm from Scratch

469

2026-02-04 | By Rinme Tom

License: General Public License Robot Kits Arduino

📌 Overview

Robotic manipulators are essential in both industrial automation and hobby robotics. This step-by-step project shows you how to build an Arduino Robotic Arm with a 6-degree-of-freedom (6-DOF) robotic arm driven by servo motors and controlled by an Arduino microcontroller. You’ll learn mechanical assembly, wiring, Arduino programming, and real-time control through an interactive interface — ideal for makers, students, and robotics enthusiasts.

Arduino Robotic Arm

🧰 Parts & Tools You’ll Need

Below is a curated list of essential components available from DigiKey (or part examples if an exact match doesn’t exist). These parts form the backbone of your robotic arm.

Diy Robotic Arm

🛠️ Core Electronics

🔌 Actuators

  • Hobby servo motors (at least 6) — each joint uses one servo for motion (base rotation, shoulder, elbow, wrist pitch, wrist rotation, gripper)

  • Servo horns & mounting brackets — for attaching servos to printed or metal parts

🔧 Mechanical & Assembly

  • 3D-printed arm parts or metal bracket kit (base, links, wrist mounts, gripper) — essential structure

  • Screws, nuts & bolts — mounting hardware

  • Screwdrivers, small pliers — assembly tools

Circuit Diagram

💻 Software

  • Arduino IDE (for uploading control firmware)

  • Web browser with Web Serial API support (Chrome, Edge) for interactive controls

Tip: You may also choose a full metal 6-DOF arm kit from your inventory to simplify mechanical assembly.

3d printing process

🧩 Step-by-Step Assembly

1️⃣ 3D Print or Source Mechanical Parts

Print or obtain arm segments: base, shoulder link, elbow link, wrist modules, and gripper. Make sure the pieces fit snugly around servo mounts and rotate freely.

2️⃣ Mounting the Motors

  1. Insert one servo into each joint housing (base, shoulder, elbow, wrist tilt, wrist rotation, gripper).

  2. Use servo horns to attach the output shaft to the arm linkages.

  3. Ensure neutral (90°) alignment for all servos before tightening screws.

A good neutral position ensures smoother motion and fewer wiring issues during testing.

3️⃣ Wiring and Power

Servos can draw more current than the Arduino’s onboard regulator can safely provide — always use an external 5 V supply for servos and share a common ground with the Arduino.

  1. Connect all servo power (red) and ground (black) lines to the external 5 V supply.

  2. Connect all servo signal (PWM) wires to PWM-capable pins on the Arduino.

  3. Connect the ground of the external supply to the Arduino ground.

Hardware Set up

👨‍💻 Arduino Firmware

Below is a simplified version of the Arduino sketch that initializes servos and sets them to a neutral pose:

Copy Code
#include <Servo.h>

Servo baseServo, shoulderServo, elbowServo, wristRotServo, wristTiltServo, gripperServo;

void setup() {
  baseServo.attach(3);
  shoulderServo.attach(5);
  elbowServo.attach(6);
  wristRotServo.attach(9);
  wristTiltServo.attach(10);
  gripperServo.attach(11);

  // Set neutral positions
  baseServo.write(90);
  shoulderServo.write(90);
  elbowServo.write(90);
  wristRotServo.write(90);
  wristTiltServo.write(90);
  gripperServo.write(90);
}

void loop() {
  // Placeholder: Real application will read commands (serial/web) to move servos
}

📎 Save this as robotic_arm.ino and upload using Arduino IDE.

🖥️ Interactive Web Control Interface

You can build a simple web interface using HTML/JavaScript that uses the Web Serial API to send servo position commands to your Arduino in real time.
This allows slider-controlled motion for each servo — great for testing and demos.

Key features your interface can include:
✔ Individual servo sliders
✔ “Home” position button
✔ Saved movement presets
✔ Live feedback display

Dashboard

🛠️ Testing & Troubleshooting

Before running full motion sequences:

➤ Ensure all servos are powered correctly and not overheating.
➤ Test each joint individually via simple Arduino sketches.
➤ If servos jitter or reset, check your power supply rating — most issues stem from low current delivery.

🧠 What You’ll Learn

🔹 Servo control using Arduino PWM
🔹 Multi-axis mechanical movement
🔹 Real-time control via web interface
🔹 Power distribution and wiring best practices
🔹 Practical robotics fundamentals

📈 Expand Your Build

Once your arm is functional, here are ways to take it further:

  • Add Bluetooth or Wi-Fi control — link to a mobile app

  • Camera integration for basic vision tasks

  • Inverse kinematics support for smooth motion planning

Número de parte del fabricante T050000
TINKERKIT BRACCIO (US.EU.UK.AU P
Arduino
$305.88
Ver más Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.