Maker.io main logo

Robotics Education: Robot Tour Part 1

735

2024-01-08 | By Antonio Velasco

As the students working on the Detector Building Project have been speeding along, the Robot Tour students have been watching along to pick up some coding skills and get familiar with Arduino. Finally, with some dedicated build time, they've been able to make some significant progress of their own, which will be documented in this blog!

For context on the projects that we're working on, check out the first installment of the blog here! In short, I'm teaching some Pearl City High School students (located in Hawaii!) about embedded systems by coaching them for robotics events they'll compete in for the Science Olympiad. The other project is an ORP (or Redox probe) that will measure conductivity and eventually PPM/concentration. This project will be on creating a rover that can traverse a certain course and earn points based on its navigation time and if it can reach some special areas! The name of the event we're working on for this project is Robot Tour!

Getting Started

Of course, the first thing to do with any coding project is to get on the grind with getting familiar with...code! On the first day, we did a little overview of our plan, we reviewed the basics involving syntax, loops, and the basic functions that students need to know. As we haven't had a build day yet for the Robot Tour project, the students on this event have just been piggybacking on the coding worktime with the Detector Building (the other event) students to get familiar with libraries and more.

With that, today the first thing that we did was start up the Arduino IDE and test out all of our components to make sure that they work before we put everything together. This included the servo motors, ultrasonic sensor, the Arduino shield, and a couple more misc. components. They all ended up working fine, so we immediately got to work on the build!

Parallax's All-In-One Kit!

For this part, we used a Parallax kit that included everything.

Robotics Education: Robot Tour Part 1

If you're interested in nabbing one for yourself or your students, I've linked it below. It comes with battery holders, a Parallax Arduino shield, multiple circuit components, wheels, motors, and more. Namely, it doesn't come with an Arduino R3 (the specific Arduino that it is compatible with) nor the USB-A to USB-B cable, so ensure that you have those ahead of time. It also doesn't come with any sensors, so be sure to get that on the side as well. However, outside of that, the kit is all-inclusive and perfect to get started with.

Robotics Education: Robot Tour Part 1

The Parallax website has an entire tutorial that guides the students through some basic circuitry and building the rover from the ground up. This was great news to me as it meant that I had a crutch to rely on when teaching the content, and also a step-by-step guide on using the kit. We covered the first two chapters with ease and got through all the initial testing and set-up.

Now, it was time to build.

Assembly

The students got to work on assembling the robot utilizing the instructions on the website through Chapter 3.

Robotics Education: Robot Tour Part 1

The instructions were very easy to follow, and the students only required minor guidance here and there to ensure that they were utilizing the right part or when they didn’t know how something worked. Of course, we all agreed that the most satisfying part of any shield build was sandwiching the shield to the Arduino Uno R3.

Robotics Education: Robot Tour Part 1

Just super cool how everything lines up!

In no time, we were almost done hooking everything up.

Robotics Education: Robot Tour Part 1

The hardest part ended up being threading some of the wires through, but we got it done and, in less than an hour since we started assembling the robot, we were done!

Robotics Education: Robot Tour Part 1

The entire process was stress-free, and although we forgot the AA batteries, we were able to get some code and power in directly through the USB-A to USB-B adaptor, testing the rover by itself for the first time.

Next-Steps

Needless to say, the first order of business is getting some AA batteries to have the rover move without a wired attachment. The students have also got some homework: start some test code for a basic obstacle course. In the next blog, I'll talk more about the course and the coding process since that'll end up being more of an intensive process. We also have plans to add an ultrasonic sensor and some extra components that'll make the rover competitive.

Robotics Education: Robot Tour Part 1

For now, though, we've made some excellent progress, and I'm excited to see what comes next!

Check out the other Robotics Education Projects below!

Robotics Education: The Basics

Detector Building Part 1

Detector Building Part 2

Número de parte del fabricante 130-35000
KIT ROBOTICS ARDUINO SHIELD
Parallax Inc.
$227.71
Ver más Details
Número de parte del fabricante A000066
ARDUINO UNO R3 ATMEGA328P BOARD
Arduino
$27.60
Ver más Details
Número de parte del fabricante 3942
ULT SEN TX/RX 40KHZ 5V
Adafruit Industries LLC
Número de parte del fabricante LR6XWA/BXU
BATTERY ALKALINE 1.5V AA
Panasonic Energy
Número de parte del fabricante 321010008
CABLE A PLUG TO B PLUG 4.92'
Seeed Technology Co., Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.