Maker.io main logo

Introduction to Zephyr Part 3: Kconfig Tutorial

2,281

2025-03-20 | By ShawnHymel

Microcontrollers ESP32

In the previous parts of our “Introduction to Zephyr” series, we looked at setting up a basic Zephyr application and using CMake to manage our build. This time, we’ll dive into another core component of the Zephyr build system: Kconfig.

Kconfig is a configuration system originally developed for the Linux kernel. It provides a powerful and flexible way to enable, disable, or parameterize components and features of a large and complex system like Zephyr. By leveraging Kconfig, we can control which libraries, drivers, and functionalities are included in the final firmware image, all without hard coding these decisions directly into our source code.

In this tutorial, we’ll:

  1. Introduce Kconfig and the menuconfig interface.
  2. Show how to enable and configure a random number generator using Zephyr’s Kconfig symbols.
  3. Walk through enabling pseudo-random number generation.
  4. Demonstrate how to create your own Kconfig symbol in a custom Zephyr module.

Along the way, we’ll continue building on our Docker-based development environment and ESP32 platform. By the end, you’ll have a working application that prints random numbers to the console and a solid understanding of how to manage Zephyr configurations using Kconfig and menuconfig.

All example code and solutions for this series can be found in this repository: https://github.com/ShawnHymel/introduction-to-zephyr/

Why Kconfig?

Zephyr supports a huge range of hardware platforms, drivers, middleware, and OS features. Not every application needs every feature, so Kconfig helps developers customize their firmware images to only include what’s necessary. Instead of editing code files directly, Kconfig lets you specify options—like enabling a particular driver or selecting a pseudo-random number generator—through configuration symbols.

These symbols are stored in .config files generated during the build process. You can edit them interactively using menuconfig (a text-based user interface), guiconfig (a graphical user interface) or by placing desired configuration symbols in a prj.conf file at the project root. Each symbol can be turned on or off (y or n), or given a numeric/string value, all controlled by Kconfig’s logic.

You can read more about how Zephyr uses the Kconfig system here: https://docs.zephyrproject.org/latest/build/kconfig/menuconfig.html

Setting up the Random Number Generator Example

To start, we’ll create a new application directory named 03_kconfig_demo that generates random numbers using Zephyr’s random API. The random API can produce pseudo-random numbers or connect to a true hardware entropy source if available (for example, the ESP32 has a hardware RNG).

Note that the code for this tutorial can be found here: https://github.com/ShawnHymel/introduction-to-zephyr/tree/main/workspace/apps/03_demo_kconfig

Prerequisites:

Inside the container (or your development environment), create the new application directory and the necessary files:

Directory structure:

Copy Code
workspace/apps/03_kconfig_demo/
├─ CMakeLists.txt
├─ prj.conf
└─ src/
   └─ main.c
main.c

We’ll write a simple loop that prints a random number every second:

Copy Code
#include <zephyr/random/random.h>

// Settings
static const int32_t sleep_time_ms = 1000;

int main(void)
{
    uint32_t rnd;
    double rnd_float;

    // Do forever
    while (1) {

        // Print random number
        rnd = sys_rand32_get();
        rnd_float = (double)rnd / (UINT32_MAX + 1.0);
        printk("Random value: %.3f\r\n", rnd_float);

        // Sleep
        k_msleep(sleep_time_ms);
    }

    return 0;
}

CMakeLists.txt

Our CMakeLists.txt is straightforward, similar to previous examples:

Copy Code
cmake_minimum_required(VERSION 3.20.0)

set(ZEPHYR_EXTRA_MODULES "${CMAKE_SOURCE_DIR}/../../modules/say_hello")

find_package(Zephyr REQUIRED HINTS $ENV{ZEPHYR_BASE})
project(random)

target_sources(app PRIVATE src/main.c)

prj.conf

For now, leave prj.conf empty. Zephyr requires it to exist even if it has no content. Later, we might add Kconfig symbols here if needed:

Attempting to Build and Running into Kconfig Issues

Let’s try to build this application:

Copy Code
west build -p always -b esp32s3_devkitc/esp32s3/procpu

You might see an error like:

Copy Code
undefined reference to `z_impl_sys_rand_get'
collect2: error: ld returned 1 exit status

This indicates that even though we included the correct headers and called sys_rand32_get(), the corresponding random number generator library isn’t actually built into our firmware. Why? Because we haven’t told Kconfig to enable the appropriate symbols.

In Zephyr, including a header file doesn’t automatically link its implementation. Many drivers, subsystems, and services are gated behind Kconfig symbols that must be enabled. Let’s fix that using menuconfig.

Using menuconfig to Explore Kconfig Options

menuconfig provides an interactive, terminal-based menu for browsing and setting Kconfig symbols. To run it, invoke:

Copy Code
west build -p always -b esp32s3_devkitc/esp32s3/procpu -t menuconfig

This brings up a text-based UI with menus you can navigate using arrow keys and Enter. Key tips:

  • Press / to search for symbols.
  • Press ? for help on a selected symbol.
  • Press Space to toggle a symbol ([ ] means off, [X] means on).
  • Search for “random” by pressing / and typing “^random” (menuconfig supports regex, and ‘^’ means to search at the beginning of the string). You’ll see various symbols and menus related to random number generation. Navigate to the "Random Number Generators" menu. Here, you’ll see options for pseudo-random and entropy-based random number generation.

    Introduction to Zephyr Part 3: Kconfig Tutorial

    The pseudo-random number generator (PRNG) typically uses a system timer or other software-based approach for speed but is not truly random. It’s often good enough for basic scenarios. For full entropy (true randomness), you’d rely on hardware RNG or the entropy driver—if your MCU and board support it.

    The ESP32-S3 has a hardware RNG, but we’ll use the simple pseudo-random generator for this demo. Search for and enable Allow non-random number generator. This should automatically select the System timer as your Random generator source.

    Introduction to Zephyr Part 3: Kconfig Tutorial

    Return to the main menu and exit (or press ‘q’), saving your configuration.

    This process updates the build’s .config file (in build/zephyr/.config). After enabling the pseudo-random number generator, rebuild (note the lack of the -p pristine tag):

    Copy Code
    west build -b esp32s3_devkitc/esp32s3/procp

    Now, the application should link properly and build without error.

    If you run and flash the firmware onto your ESP32-S3 (using esptool as we did in previous episodes), you should see a stream of random values printed out every second.

    Introduction to Zephyr Part 3: Kconfig Tutorial

    Understanding the Generated .config

    Every time you run west build, Zephyr’s build system merges configuration fragments from various places: the board’s default configuration, the SOC’s defaults, the drivers, and your prj.conf (and any extra conf files you specify). The result is a unified .config file in build/zephyr/.config.

    You can open this file after running menuconfig and saving changes. Search for CONFIG_RANDOM to see what got enabled.

    Remember that .config is generated at build time and will be overwritten if you run west build -p always (which forces a pristine build). To preserve your manual menuconfig changes, avoid -p always. Each time you run menuconfig, Kconfig stores the previous settings in .conf.old. You can use diff to see what changed between the two menuconfig runs:

    Copy Code
    diff build/zephyr/.config.old build/zephyr/.config

    You can also use Zephyr’s diffconfig tool to view the difference between the previous menuconfig runs:

    Copy Code
    python $ZEPHYR_BASE/scripts/kconfig/diffconfig build/zephyr/.config.old build/zephyr/.config

    You can copy these differences to your prj.conf file to save the Kconfig settings between builds (even if you delete the build/ directory or run with -p always). Remember that Kconfig settings are not permanent unless you write them into prj.conf or a board-specific conf file. Relying solely on menuconfig for persistent configuration can lead to changes being overwritten after a pristine build.

    Managing Board-Specific and Overlay Configuration Files

    What if your application runs on multiple boards, but only some boards have a particular hardware RNG? You might not want to enable certain symbols globally in prj.conf.

    Zephyr supports specifying additional configuration fragments via EXTRA_CONF_FILE or CONF_FILE. For example, you could place board-specific Kconfig settings in a separate file:

    Copy Code
    workspace/apps/03_demo_kconfig/boards/
    └─ esp32s3_devkitc.conf

    This file could contain hardware-specific symbols for ESP32-S3. Then build with:

    Copy Code
    west build -p always -b esp32s3_devkitc/esp32s3/procpu -- -DEXTRA_CONF_FILE=boards/esp32s3_devkitc.conf

    This approach keeps your main prj.conf clean and board-agnostic, while allowing you to add board-specific configuration without editing .config directly.

    Creating Custom Kconfig Symbols in a Zephyr Module

    So far, we’ve only toggled existing Kconfig symbols. Zephyr also lets you define your own symbols for custom modules. Let’s create a simple module that prints “Hello!” when enabled.

    Module Structure

    In your workspace, create an out-of-tree Zephyr module with the following structure:

    Copy Code
    workspace/modules/say_hello/
    ├─ zephyr/
    │  └─ module.yaml
    ├─ say_hello.h
    ├─ say_hello.c
    ├─ Kconfig
    └─ CMakeLists.txt
    say_hello.h:
    Copy Code
    #ifndef SAY_HELLO_H_
    #define SAY_HELLO_H_
    
    // Public function declaration
    void say_hello(void);
    
    #endif /* SAY_HELLO_H_ */
    
    say_hello.c:
    
    Copy Code
    #include <zephyr/kernel.h>
    
    #include "say_hello.h"
    
    void say_hello(void) {
        printk("Hello!\r\n");
    }
    

    Kconfig (for your module):

    Copy Code
    # Create a new option in menuconfig
    config SAY_HELLO
        bool "Basic print test to console"
        default n   # Set the library to be disabled by default
        depends on PRINTK   # Make it dependent on PRINTK
        help
            Adds say_hello() function to print a basic message to the console.

    This defines a new Kconfig symbol SAY_HELLO which the user can enable or disable from menuconfig.

    CMakeLists.txt (in modules/say_hello):

    Copy Code
    # Check if SAY_HELLO is set in Kconfig
    if(CONFIG_SAY_HELLO)
    
        # Add your source file directory
        zephyr_include_directories(.)
    
        # Add the source file you want to compile
        zephyr_library_sources(say_hello.c)
    
    endif()

    This CMake logic ensures that say_hello.c is only compiled and linked if CONFIG_SAY_HELLO is set.

    module.yaml

    We also need a module.yaml file so Zephyr knows this directory is a module:

    Copy Code
    name: say_hello
    build:
      cmake: .
      kconfig: Kconfig

    Integrating the Module into the Application

    Back in your main application (03_kconfig_demo), update CMakeLists.txt to tell Zephyr about the extra module:

    Copy Code
    cmake_minimum_required(VERSION 3.20.0)
    
    set(ZEPHYR_EXTRA_MODULES "${CMAKE_SOURCE_DIR}/../../modules/say_hello")
    
    find_package(Zephyr REQUIRED HINTS $ENV{ZEPHYR_BASE})
    project(random)
    
    target_sources(app PRIVATE src/main.c)
    
    Using the say_hello Module in src/main.c
    
    Copy Code
    #include <zephyr/random/random.h>
    
    #ifdef CONFIG_SAY_HELLO
    #include "say_hello.h"
    #endif
    
    // Settings
    static const int32_t sleep_time_ms = 1000;
    
    int main(void)
    {
        uint32_t rnd;
        double rnd_float;
    
        // Do forever
        while (1) {
    
            // Print random number
            rnd = sys_rand32_get();
            rnd_float = (double)rnd / (UINT32_MAX + 1.0);
            printk("Random value: %.3f\r\n", rnd_float);
    
    #ifdef CONFIG_SAY_HELLO
            say_hello();
    #endif
    
            // Sleep
            k_msleep(sleep_time_ms);
        }
    
        return 0;
    }
     

    If CONFIG_SAY_HELLO is y, it prints “Hello!” after each random number. If not, those function calls will be left out of the build, keeping the firmware smaller.

    Enable SAY_HELLO by adding to boards/esp32s3_devkitc.conf:

    Copy Code
    CONFIG_SAY_HELLO=y

    Build again with:

    Copy Code
    west build -p always -b esp32s3_devkitc/esp32s3/procpu -- -DEXTRA_CONF_FILE=boards/esp32s3_devkitc.conf

    After flashing, you should see random values and “Hello!” printed every loop.

    If you disable CONFIG_SAY_HELLO, the module’s code won’t be included, and you won’t see the greeting.

    Challenge: Printing Floats

    Now, let’s go a step further and convert the random 32-bit integer into a floating-point number between 0.0 and 1.0. Modify src/main.c:

    Copy Code
    #include <zephyr/random/random.h>
    
    // Settings
    static const int32_t sleep_time_ms = 1000;
    
    int main(void)
    {
    	uint32_t rnd;
    	double rnd_float;
    
    // Do forever
    while (1) {
    
                    // Print random number
    		rnd = sys_rand32_get();
    		rnd_float = (double)rnd / (UINT32_MAX + 1.0);
    		printk("Random number: %.3f\r\n", rnd_float);
    
    		// Sleep
    		k_msleep(sleep_time_ms);
    	}
    
    	return 0;
    }
    

    Potential Problem: Many embedded builds disable floating-point formatting by default to save space. You may see something like "*float*" printed to the console instead of your actual number. In that case, you’ll need to enable floating-point support in Zephyr’s menuconfig or switch to a standard library like Newlib with floating-point support enabled.

    To do this, open menuconfig again:

    Copy Code
    west build -p always -b esp32s3_devkitc/esp32s3/procpu -t menuconfig -- -DEXTRA_CONF_FILE=boards/esp32s3_devkitc.conf

    Search for picolibc or newlib and explore enabling floating-point formatting. Some configurations require turning on certain CONFIG_NEWLIB_LIBC_FLOAT_PRINTF or CONFIG_PICOLIBC_IO_FLOAT options. This part is left as a challenge—try enabling these symbols and see if you can print floating-point numbers successfully!

    You can find my solution here: https://github.com/ShawnHymel/introduction-to-zephyr/tree/main/workspace/apps/03_solution_kconfig_float

    Going Further:

    In this post, we explored how to use Kconfig and menuconfig within Zephyr to configure subsystems like random number generators. If you’d like to dive more into Kconfig, I recommend the following resources:

    With a solid grasp of CMake, Kconfig, and the fundamental building blocks of Zephyr, you’re well on your way to developing more advanced embedded applications.

    Número de parte del fabricante ESP32-S3-DEVKITC-1-N32R8V
    ESP32-S3-WROOM-2-N32R8V DEV BRD
    Espressif Systems
    More Info
    Ver más Details
    Número de parte del fabricante 3533
    GRAPHIC DISPLAY TFT RGB 0.96"
    Adafruit Industries LLC
    Número de parte del fabricante 1782
    MCP9808 TEMP I2C BREAKOUT BRD
    Adafruit Industries LLC
    Número de parte del fabricante 3386P-1-103TLF
    TRIMMER 10K OHM 0.5W PC PIN TOP
    Bourns Inc.
    Número de parte del fabricante 1825910-6
    SWITCH TACTILE SPST-NO 0.05A 24V
    TE Connectivity ALCOSWITCH Switches
    Número de parte del fabricante CF14JT220R
    RES 220 OHM 5% 1/4W AXIAL
    Stackpole Electronics Inc
    Número de parte del fabricante LTL-4224
    LED RED CLEAR T-1 3/4 T/H
    Lite-On Inc.
    Número de parte del fabricante 14284
    JUMPER M/M 4" 26AWG 30PCS
    SparkFun Electronics
    Número de parte del fabricante FIT0096
    BREADBRD TERM STRIP 3.20X2.00"
    DFRobot
    Número de parte del fabricante DH-20M50055
    USB AM TO USB MICRO, USB 2.0 - 1
    Cvilux USA
    Add all DigiKey Parts to Cart
    Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.