Maker.io main logo

TensorFlow Lite for Microcontrollers Kit Quickstart

313

2019-08-15 | By Adafruit Industries

License: See Original Project Programmers

Courtesy of Adafruit

Guide by Lady Ada

Get going quickly with your TensorFlow Lite kit!

Overview

Machine learning has come to the 'edge' - small microcontrollers that can run a very miniature version of TensorFlow Lite to do ML computations.

But you don't need super complex hardware to start developing your own TensorFlow models! We've curated a simple kit to dip your toes into machine learning waters.

 

Kit includes:

The kit uses our PyBadge as your edge processor. It's a compact board - it's credit card sized. It's powered by our favorite chip, the ATSAMD51, with 512KB of flash and 192KB of RAM. We add 2 MB of QSPI flash for file storage, handy for TensorFlow Lite files, images, fonts, sounds, or other assets.

You can plug in a microphone into the ports at the bottom, to add microphone input for micro speech recognition. Our Arduino library has some demos you can get started with to recognize various word pairs like "yes/no", "up/down" and "cat/dog". TensorFlow Lite for microcontrollers is very cutting-edge so expect to see a lot of development happening in this area, with lots of code and process changes.

Parts required

You can get everything you need minus tools in this kit:

Or as individual parts:

Assembly

Step 1 - Solder Headers onto Microphone

You'll need to plug into your microphone, so visit this guide for step by step instructions on soldering the headers on

Image-1-78480-640

Step 2 - Connect JST PH Cable to Microphone

Connect Red to VCC, Black to GND and White to OUT

Image-2-78481-640

Step 3 - Cut and solder the 3V selection jumper on the back of the PyBadge or PyGamer

On the back of your board, find the STEMMA cable voltage selection jumper. Cut the trace from Vcc to 5V

Image-3-78483-340

Then solder in the Vcc to 3V pads

Image-4-78484-340

Step 4 - Plug in Microphone into D2

Image-5-78488-640

Software Setup

We're going to be using the popular Arduino IDE to compile and load code. Start by following the PyBadge setup guide to

Once that's all done, also install the TFLite Micro Speech library

Image-6-78490-740

Try loading the JSON demo version of the code

Image-7-78491-540

Select from the Tools menu

  • Board: Adafruit PyBadge M4 Express

  • CPU Speed: 200 MHz

  • Optimize: Fastest

  • USB Stack: TinyUSB

  • Port: Correct Serial/COM port

Image-8-78493-540

And compile upload to the PyBadge

After its done uploading, you should see a new disk drive on your computer called CIRCUITPY (or similar) it will be 8 MB large

Image-9-78494-540

Unzip this folder and drag the tflite_config.json and yesno.tflite files to the disk drive

yesnodemo.zip

Image-10-78497-640

Eject the disk drive via the operating system (Eject or move it to the trash on MacOS)

Image-11-78498-540

Press Reset on the back of the board to restart

You'll get a boot screen telling you what model it loaded (thats the tflite file)

Image-12-78501-340

Press the A button to record up to 1.5 seconds of audio, the first neopixel will light up red to let you know

Try saying "yes"

Image-13-78500-340

Or "no"

Image-14-78499-340

You can also get a silence output if nothing is heard at all

Image-15-78502-340

Número de parte del fabricante 1063
EVAL BOARD FOR MAX4466
Adafruit Industries LLC
USB TO 2.1MM MALE BARREL JACK CA
Número de parte del fabricante 2697
USB TO 2.1MM MALE BARREL JACK CA
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.