Maker.io main logo

Robotic AI Bear using ChatGPT

413

2023-05-30 | By Adafruit Industries

License: See Original Project 3D Printing CNC Accessories Raspberry Pi SBC

Courtesy of Adafruit

Guide by M. LeBlanc-Williams

Overview

The Peek-A-Boo Teddy Bear by GUND is an affordable robotic bear ‎that plays pre-recorded sounds. It has a motorized mouth to ‎simulate talking and motorized arms that can lift a blanket to hide ‎its face.‎

 

This guide will show you how to enhance the bear to make it do ‎more than just play 'peek-a-boo' by tying it to OpenAI's ChatGPT API. ‎Now you can speak to the toy and ask it questions, have it tell you ‎stories, and more! Voice recognition is used to generate the prompts ‎and then text-to-speech plays back the response.‎

We do this by replacing the electronics inside with a Raspberry Pi 4, ‎an Adafruit Motor HAT, and a couple of options for playing audio such ‎as the MAX98357 I2S Amp and a Mini USB Speaker. The Raspberry Pi 4 ‎will be running a custom Python script that interacts with multiple ‎APIs including two from OpenAI and one from Azure. ‎

It takes inspiration from some iconic bear characters including a ‎popular toy in the 1980s called Teddy Ruxpin that would tell stories ‎while making prerecorded robotic gestures and movements. This ‎project was also inspired by the toy bear from the movie A.I., which ‎was advanced robotic companion designed to provide love and ‎comfort to a child.‎

This project combines the best of both worlds to create a robotic ‎bear that not only tells stories, jokes, and poems, but also interacts ‎with you using natural language processing powered by ChatGPT. ‎This technology allows the bear to respond to questions and engage ‎in conversations.‎

By the end of this guide, you will have learned how to upgrade your ‎own robotic bear with ChatGPT integration, gaining hands-on ‎experience with robotics, programming, and artificial intelligence.‎

Parts

This project has a few options depending on how compact versus ‎how easy you would like the project. Here are the parts you will need ‎for either build.‎

The first thing you will need is a Raspberry Pi 4. This project will likely ‎also work on a Raspberry Pi 3, but it has not been tested.‎

You will also need a motor HAT. The reason for the HAT over the ‎bonnet is because more soldering points are available.‎

You will need this set of nylon screws and standoffs for the project.‎

Easier Build Option

Compact Build Option

Optional Parts

These parts are optional but enhance the project.‎

Circuit Diagram

diagram_1

Required Wiring

The HAT Motor Power will come from a USB cable that will be ‎plugged into the battery pack.‎

  • Green Arms Motor Wire to HAT M1 left side (1st terminal ‎position)

  • Orange Arms Motor Wire to HAT M1 right side (2nd terminal ‎position)

  • Yellow Mouth Motor Wire to HAT M2 left side (4th terminal ‎position)

  • White Mouth Motor Wire to HAT M2 right side (5th terminal ‎position)

  • Foot Button wire 1 to HAT GPIO #16

  • Foot Button wire 2 to HAT Gnd

  • HAT Motor Power + to External USB +5V

  • HAT Motor Power - to External USB Gnd

Compact Build Additional Wiring

For the speaker wires, the order doesn't matter. Since it only has a ‎single speaker.‎

  • MAX98357 Vin to HAT 3V

  • MAX98357 Gnd to HAT Gnd

  • MAX98357 LRC to HAT GPIO #19

  • MAX98357 BCLK to HAT GPIO #18

  • MAX98357 DIN to HAT GPIO #21

  • ‎100K Resistor to MAX98357 Gain

  • Other side of 100K Resistor to MAX98357 Vin

  • Speaker Wires to MAX98357 Speaker Output

3D Printing‎

parts_2

This project will be assembled with just a few 3D printed parts, ‎described below. The parts are available in either the STL (older) or ‎‎3MF (newer) format. Most slicers support both. You'll need to print ‎multiples of some parts:‎

Main Case

  • ‎1 x Case Top.stl

  • ‎1 x Case Bottom.stl

Speaker Retainers

If you're using the 4mm 0.25W speaker from inside the bear:‎

  • ‎2 x 4mm Thick Speaker Retainer.stl

If you're using an upgraded Adafruit 2mm 0.5W speaker:‎

  • ‎2 x 2mm Thick Speaker Retainer.stl

Download STL Files

Download 3MF Files

Download CAD Source

Slicer Settings

The specific setting values aren't that important with this case. ‎However, here's the settings used to print the case for this guide.‎

For the larger case parts:

  • ‎20% infill

  • Supports on build plate enabled

  • ‎0.2mm Layer Height‎

For the small speaker retainers:

  • ‎20% infill

  • ‎0.2mm Layer Height‎

  • No Supports

Parts Details

Case Bottom

The Raspberry Pi and Motor HAT will be housed here.‎

bottom_3

Case Top

The speaker and MAX98357 will be attached here.‎

top_4

‎4mm Thick Speaker Retainer

These retainers are for the 4mm thick speaker that you can harvest ‎from inside the bear.‎

speaker_5

‎2mm Thick Speaker Retainer‎

These are for holding the thinner 2mm 0.5W Adafruit speaker ‎upgrade.‎

retainer_6

Modifying the Bear

To be able to make use of the bear, you will need to disassemble it ‎and remove the circuitry so that it can be connected to the ‎Raspberry Pi. Some of the tools you will need include a couple of ‎sizes of Phillips-head and Flathead screwdrivers, some isopropyl ‎alcohol, and flush cutters or a soldering iron.‎

Some screws will be reused. Be sure to keep those in a place where ‎you can find them later.‎

Disassembly

As you disassemble the bear, be sure to carefully set aside the ‎screws and electronics as some of this will be re-used in the final ‎circuit.‎

Isopropyl Alcohol is very good at removing hot glue.‎

Start by removing the bear from the packaging.‎

start_7

Turn the bear over and open the flap covering the battery ‎compartment. You may want to remove the battery cover and ‎batteries so you can use them for something else. They won't be ‎used in this project.‎

turn_8

Remove the 4 screws and set them aside. Then remove the cover. ‎You may need to pry it a bit.‎

remove_9

The fabric around the electronics housing should now be free to pull ‎away. Go ahead and pull the housing out of the bear.‎

fabric_10

To expose the housing, first carefully push the cloth around the ‎housing up so that the bottom half inch of the housing is exposed. ‎Then push it up the rest of the way.‎

expose_11

The housing is attached further up with a bunch of hot glue. ‎Applying some isopropyl alcohol (or IPA) to the glue with a cotton ‎swab or something similar will cause the glue to become brittle and ‎less adhesive. The higher the concentration of IPA, the better it ‎works. Don't forget to remove the glue on the lower white wires.‎

attached_12

There are 4 more screws holding the housing together. Remove ‎those screws and set them aside.‎

screws_13

Once the two halves of the housing are taken apart, you will have ‎access to the electronics and wiring.‎

housing_14

On the circuit board are connections to the power, mouth motor, ‎arms motor, foot button, and speaker. Remove everything except the ‎power wires because they won't be needed. If you are doing the ‎easier build option or upgrading the speaker, you won't need the ‎built-in speaker either. You can either use flush cutters or remove ‎the glue and desolder each wire.‎

board_15

Preparing the Motor Wires

In order to connect the motor wires to the Adafruit Motor HAT, we ‎recommend extending the thin wires with thicker jumper wires and ‎a nice connector on the end.‎

If you don't mind the wires being short on the short side, you may ‎want to try wire ferrules. These have the advantage of not being as ‎deep and you don't risk melting the polyfill stuffing inside the bear. ‎However, the wire gauge is a bit small and it's tricky to get the ‎ferrules to stay on properly.‎

You could also combine the two methods and extend the wires with ‎thicker ones and replace the long black connectors with the shorter ‎ferrules.‎

Be very careful while using heat near the bear! It's easy to ‎accidentally melt the fur or the polyfill stuffing! If you aren't very ‎confident with your skills, you could temporarily line the fur with ‎aluminum foil to act as a heat shield.‎

With the 6" wires, by cutting in half, you can have 2 useable parts. If ‎you would like longer wires, you can just cut off 1 end.‎

wires_16

You'll want to cut, strip, and tin 4 wires to match the motor wires. ‎You will also want to cut 4 pieces of heat shrink tubing. Place the ‎heat shrink on the wires now so you don't forget later.‎

wires_17

Strip and tin the wires inside the bear. Very carefully solder the wire ‎extensions to the motor wires sticking out. You may want to ‎temporarily remove some of the stuffing to give you more room to ‎work and place some aluminum foil around the area you are ‎working.‎

strip_18

Now slide the heat shrink tubing up and heat it. I used a hot air ‎soldering station set at 120° Celsius, which seemed to be just hot ‎enough to shrink it. You could also use electrical tape to insulate if ‎you aren't comfortable with heat shrink.‎

slide_19

Preparing the Foot Button

If you would like to make it so the foot button can be disconnected, ‎you can attach the JST SM Plug cable to it and the receptacle to the ‎Pi.‎

If you are not using this connector, just strip and tin the pair of white ‎wires coming out of the bear with a small knot in the end without ‎shortening the wires.‎

The foot button wires and JST cables are quite long, so it's helpful to ‎trim them down a bit.‎

foot_20

foot_21

Place some heat shrink tubing on the foot button wires. Since the ‎wires are already separated, it makes things a lot easier.‎

place_22

Strip, tin, and solder the harness to the foot button wires. The specific ‎wire doesn't matter since pushing the button connects them ‎together.‎

harness_23

Slide the heat shrink tubing over the soldered wires and heat it up. ‎Since the wiring isn't as short as the motor wires, this is much easier.‎

slide_24

That’s it. You’ll connect the receptacle on the Wiring page.

connect_25

Preparing the Speaker

If you are reusing the speaker and you would like to use the terminal ‎connector on the MAX98357, you will want to replace the wires on ‎the speaker with ones similar to the motor. Otherwise, you can just ‎strip and tin the existing wires.‎

Prepare two more wires and desolder the ones that come with the ‎speaker.‎

prepare_26

Solder the new wires onto the speaker.‎

solder_27

That's it! The bear is all prepared for adding the new electronics.‎

DC and Stepper Motor HAT ‎Assembly

Solder on Headers and Terminal ‎Block

Before we can motorin' there's a little soldering to be done. This step ‎will attach the 2x20 socket header so that we can plug this HAT into ‎a Raspberry Pi, and the terminal blocks so you can attach external ‎power and motors.‎

Start by plugging the 2x20 header into a Raspberry Pi, this will keep ‎the header stable while you solder. Make sure the Pi is powered ‎down!‎

start_28

Place the HAT on top so that the short pins of the 2x20 header line ‎up with the pads on the HAT.‎

hat_29

And Solder!‎

Heat up your iron and solder in one header connection on the right.‎

Once it is soldered, put down the solder and reheat the solder point ‎with your iron while straightening the HAT so it isn't leaning down.

‎‎(For tips on soldering, be sure to check out our Guide to Excellent ‎Soldering).‎

solder_30

solder_31

Solder one point on the opposite side of the connector.‎

point_32

Solder each of the connections for the top row.‎

row_33

row_34

row_35

Flip the board around and solder all the connections for the other ‎half of the 2x20 header.‎

flip_36

flip_37

flip_38

flip_39

Check over your work so far, make sure each solder point is shiny, ‎and isn't bridged or dull or cracked.‎

check_40

Now grab the 3.5mm-spaced terminal blocks. These will let you ‎quickly connect up your motor and power supply using only a ‎screwdriver.‎

You will have 3 x 2-pin terminal blocks and 2 x 3-pin terminal blocks.‎

Slide each of the 3-pin terminal blocks into a 2-pin to create two 5-‎pin blocks.‎

slide_41

Slide the terminal blocks along the edge of the HAT, so that the ‎‎'mouth' of each block is facing out.‎

You can use scotch or other plain tape to keep the terminal blocks ‎flat against the PCB while you solder.‎

slide_42

Flip over the board and solder in all of the terminal block pins.‎

flip_43

flip_44

flip_45

Check over your work so far, make sure each solder point is shiny, ‎and isn't bridged or dull or cracked.‎

You’re done! You can now move onto the software side.‎

side_46

Wiring

The wiring for the new electronics going into the bear is fairly ‎straightforward. Make sure you have assembled the Adafruit DC and ‎Stepper Motor Hat first.‎

USB Cable Modification Option

To power the motors, you are going to use 5V directly from the USB ‎Power Bank. While it could be powered from the Pi, the output isn't ‎as high, and the motors are noisy which may be heard through the ‎speakers.‎

For the more compact build option, you will shorten the wiring with ‎the following procedure.‎

Start with the USB to 2.1mm adapter cable.‎

cable_47

Cut the cable with about 6 inches of wire length from the USB plug ‎and strip the ends.‎

cut_48

For a better connection, crimp some wire ferrules to the ends.‎

crimp_49

The side with the white stripes is the negative side.‎

side_50

USB Cable Adapter Option

For the easier build option, you can create a little adapter for the USB ‎cable. This method is less compact, but non-destructive.‎

For this you will need:‎‎

  • 1 x USB to 2.1mm adapter cable‎

  • 1 x Female DC Power Adapter‎‎

  • 2 x Jumper Wires‎‎

option_51

Install the jumper wires in the female DC power adapter. It's a good ‎idea to use different colors so it's easier to tell which side is positive ‎and which side is negative.‎

install_52

Just plug the cable into the DC power adapter and you’re done.‎

plug_53

Foot Button Connection

You will want to connect the other half of the JST SM connection pair ‎to the Motor HAT. If you are soldering the white wires directly to the ‎HAT, you should have already prepared them in the Modifying the ‎Bear step.‎

Prepare the receptacle half of the connection by stripping and ‎tinning the wires.‎

prepare_54

Solder the wires on the GPIO #16 and one of the GND pads on the ‎DC Motor HAT.‎

motor_55

motor_56

MAX98357 I2S Amplifier

Because the project is using a 3W amplifier with a 0.25W or 0.5W ‎speaker, it's a good idea to reduce the gain as much as possible ‎because too much can actually heat the speaker coil to the point of ‎melting the speaker cone. This can be accomplished by connecting ‎a 100K resistor between Gain and Vin.‎

Prepare a 4-inch wire by cutting and stripping it. You can just use ‎one of the jumper wires with both ends cut off if you don't have extra ‎wire. You will also need a 100K resistor and the MAX98357 with only ‎the terminal soldered on. Optionally, you could just solder the ‎speaker directly to the MAX98357 instead of using the terminal.‎

amplifier_57

Start by soldering the wire to the Vin pin on the MAX98357.‎

start_58

Next, take the resistor and fold the leads down at a 90-degree angle ‎so that they are parallel to each other.‎

About 5mm further down from the resistor, add a 90-degree bend in ‎the leads keeping them parallel. Cut one side of the resistor so that ‎the cut side touches the underside of the Vin wire, and the ‎remaining lead can be soldered to Gain pin.‎

resistor_59

resistor_60

resistor_61

resistor_62

Prepare four more wires so that they are about the same length as ‎the first wire.‎

wires_63

Solder these wires to the LRC, BCLK, DIN, and GND pins of the ‎MAX98357.‎

pins_64

Solder the remaining connections according to the Circuit ‎Diagram page of this guide.‎

That's it! Everything should now be ready for assembly.‎

assembly_65

Raspberry Pi Setup

Install Raspberry Pi OS 64-bit Lite

For the bear, you will need the 64-bit version of the latest Raspberry ‎Pi OS Lite because the OpenAI libraries will only install on that ‎version. Since the project uses a voice interface, a desktop isn't ‎required. You can refer to the CircuitPython on Linux and Raspberry ‎Pi guide for more help setting it up.‎

Once you have everything set up, you will need to open a terminal ‎and install Blinka. Refer to the Installing CircuitPython Libraries on ‎Raspberry Pi page to quickly get up and running.‎

If you are planning on using HDMI audio, you may want to skip the ‎Audio setup sections below since they will remove this option.‎

Audio System and Drivers

Before you can configure the audio devices, you will need to install ‎some additional audio libraries:‎

Copy Code
sudo apt install libpulse-dev pulseaudio apulse

 

Sometimes these installations create default incompatible ‎configuration files that cause errors. These configuration files are not ‎necessary for the audio system to run. Run the following to remove ‎any existing sound configuration files:‎

Copy Code
rm ~/.asoundrc
sudo rm /etc/asound.conf

I2S Audio Setup for Compact Build Option

If you installed the MAX98357, you would need to install some ‎software to use it. Follow the Raspberry Pi Setup instructions from ‎the Adafruit MAX98357 guide.‎

Afterwards follow the Raspberry Pi Test procedure to make sure sound ‎is playing.‎

USB Audio Selection for Easier Build Option

If you went with the easier build option, most likely it will just work ‎without any changes. If not, you can tell the system which audio ‎device to use by typing:‎‎

Copy Code
sudo raspi-config

 

Select System Options→Audio. Make sure USB Audio is selected and ‎then tab over to Ok to select it. After that, you can exit to the ‎command line and that's it.‎

select_66

The volume can be adjusted by running:‎

Copy Code
alsamixer

You can just adjust the Master Volume or if you want to adjust for ‎the speaker only, you can press F6 and choose UACDemoV1.0 from ‎the device list.‎

volume_67

Install Required Libraries

You will need to have a few libraries installed before the script will ‎run on your computer. Start with some prerequisite libraries:‎

Copy Code
sudo apt install python3-pyaudio build-essential libssl-dev libasound2 wget
pip3 install SpeechRecognition

Next install the MotorKit CircuitPython library:‎‎

Copy Code
pip3 install adafruit-circuitpython-motorkit

Next install the OpenAI library:‎‎

Copy Code
pip3 install --upgrade openai

Finally Install the Azure Speech Services library:‎

Copy Code
pip3 install --upgrade azure-cognitiveservices-speech

Create an Account with OpenAI

The OpenAI platform is managed by OpenAI and changes at their ‎discretion, and so the details may be slightly different from what is ‎documented here.‎

In your web browser, visit https://platform.openai.com/‎

Click the "sign up" link. Then, you can use your e-mail to sign up, or ‎an existing Google or Microsoft account.‎

OpenAI may require additional steps such as e-mail or phone ‎verification before you can log in to your account.‎

opeen_68

Once you have completed the verification process and logged in, you ‎will next create an API key. Use the menu in the far upper right ‎corner (probably labeled "Personal") and then select "View API Keys".‎

view_68a

Then, create a fresh API key by clicking "Create new secret key".‎

key_69

Add this secret key to /etc/environment. From the command line, you ‎can open it in your favorite editor and add.‎

OPENAI_API_KEY=”sk-b6…kP5”

You will need to reboot before it will be loaded into your ‎environment variables.‎‎

secret_70

At the time of writing, OpenAI provides a free credit with new ‎accounts. After the free credit is used or expires, you'll need to enter ‎a credit card in your billing information to keep using the service.‎

Using the project tends to cost a few cents per session at most, and ‎it's easy to limit your monthly bill to a pre-set amount such as $8.00.‎

To set a hard usage limit per month, visit the "Usage Limits" section ‎of the OpenAI website.‎

set_71a

set_71

Create an Account with Azure

The Azure platform is managed by Microsoft and changes at their ‎discretion, and so the details may be slightly different from what is ‎documented here.‎

In your web browser, visit https://azure.microsoft.com/‎

Click the Free account link at the top, then click the Start ‎free button. Then, you can use your e-mail to sign up, or sign into an ‎existing Microsoft account.‎

Microsoft may require additional steps such as e-mail verification ‎before you can log in to your account.‎

platform_72

platform_73

Once you have completed the verification process and are logged in, ‎go to the Speech Services section under AI + Machine Learning to ‎create a Speech Service resource.‎

You will likely need to create a new Resource group. For the Instance ‎Details, create a unique name. You can just choose a name you like ‎and add some random numbers to the end. For Pricing Tier, there's ‎only one choice since it's a free account.‎

Click Review and Create at the bottom.‎

process_74

Review your settings and click Create.‎

create_75

Once it is created, click the Go to resource Button.‎

resource_76

Under overview, click the copy button on Key 1 to copy it to your ‎clipboard. You can click the Show Keys button as well if you want to ‎view it.‎

Add this secret key and the region to /etc/environment. From the ‎command line, you can open it in your favorite editor and add:‎

SPEECH_KEY="4f1d...02a9" SPEECH_REGION="eastus"‎

You will need to reboot before it will be loaded into your ‎environment variables.‎

variables_77

Using a Different Voice

Azure Speech Services includes a number of different voices. In their ‎Voice Gallery, you can listen to the different voices and get the Voice ‎Name to change in your code.‎

Click the Go to speech Studio button.‎

button_78

Under Text-to-speech, click Voice Gallery.‎

under_79

You can listen to the different voices. Once you find one that you are ‎happy with, select Sample code and change to Python.‎

Look for the value of speech_config. speech_synthesis_voice_name

It should be something like en-US-GuyNeural. You can change this ‎in your code later.‎

code_80

Code the Bear

This is the code that will run on the bear. Since the API keys are ‎stored in your environment variables, there's no need to modify the ‎code.‎

‎Download Project Bundle‎

Copy Code
# SPDX-FileCopyrightText: 2023 Melissa LeBlanc-Williams for Adafruit Industries
#
# SPDX-License-Identifier: MIT

import threading
import os
import sys

from datetime import datetime, timedelta
from queue import Queue
import time
import random
from tempfile import NamedTemporaryFile

import azure.cognitiveservices.speech as speechsdk
import speech_recognition as sr
import openai

import board
import digitalio
from adafruit_motorkit import MotorKit

# ChatGPT Parameters
SYSTEM_ROLE = (
    "You are a helpful voice assistant in the form of a talking teddy bear"
    " that answers questions and gives information"
)
CHATGPT_MODEL = "gpt-3.5-turbo"
WHISPER_MODEL = "whisper-1"

# Azure Parameters
AZURE_SPEECH_VOICE = "en-GB-OliverNeural"
DEVICE_ID = None

# Speech Recognition Parameters
ENERGY_THRESHOLD = 1000  # Energy level for mic to detect
PHRASE_TIMEOUT = 3.0  # Space between recordings for sepating phrases
RECORD_TIMEOUT = 30

# Motor Parameters
ARM_MOVEMENT_TIME = 0.5
BASE_MOUTH_DURATION = 0.2  # A higher number means slower mouth movement
SPEECH_VARIANCE = 0.1  # Higher allows more mouth movement variance.
                       # It pauses for BASE_MOUTH_DURATION ± SPEECH_VARIANCE
MOTOR_DUTY_CYCLE = 1.0  # Lower provides less power to the motors

# Import keys from environment variables
openai.api_key = os.environ.get("OPENAI_API_KEY")
speech_key = os.environ.get("SPEECH_KEY")
service_region = os.environ.get("SPEECH_REGION")

if openai.api_key is None or speech_key is None or service_region is None:
    print(
        "Please set the OPENAI_API_KEY, SPEECH_KEY, and SPEECH_REGION environment variables first."
    )
    sys.exit(1)

speech_config = speechsdk.SpeechConfig(subscription=speech_key, region=service_region)
speech_config.speech_synthesis_voice_name = AZURE_SPEECH_VOICE


def sendchat(prompt):
    completion = openai.ChatCompletion.create(
        model=CHATGPT_MODEL,
        messages=[
            {"role": "system", "content": SYSTEM_ROLE},
            {"role": "user", "content": prompt},
        ],
    )
    # Send the heard text to ChatGPT and return the result
    return completion.choices[0].message.content


def transcribe(wav_data):
    # Read the transcription.
    print("Transcribing...")
    attempts = 0
    while attempts < 3:
        try:
            with NamedTemporaryFile(suffix=".wav") as temp_file:
                result = openai.Audio.translate_raw(
                    WHISPER_MODEL, wav_data, temp_file.name
                )
                return result["text"].strip()
        except (openai.error.ServiceUnavailableError, openai.error.APIError):
            time.sleep(3)
        attempts += 1
    return "I wasn't able to understand you. Please repeat that."


class Listener:
    def __init__(self):
        self.listener_handle = None
        self.recognizer = sr.Recognizer()
        self.recognizer.energy_threshold = ENERGY_THRESHOLD
        self.recognizer.dynamic_energy_threshold = False
        self.recognizer.pause_threshold = 1
        self.last_sample = bytes()
        self.phrase_time = datetime.utcnow()
        self.phrase_timeout = PHRASE_TIMEOUT
        self.phrase_complete = False
        # Thread safe Queue for passing data from the threaded recording callback.
        self.data_queue = Queue()
        self.mic_dev_index = None

    def listen(self):
        if not self.listener_handle:
            with sr.Microphone() as source:
                print(source.stream)
                self.recognizer.adjust_for_ambient_noise(source)
                audio = self.recognizer.listen(source, timeout=RECORD_TIMEOUT)
            data = audio.get_raw_data()
            self.data_queue.put(data)

    def record_callback(self, _, audio: sr.AudioData) -> None:
        # Grab the raw bytes and push it into the thread safe queue.
        data = audio.get_raw_data()
        self.data_queue.put(data)

    def speech_waiting(self):
        return not self.data_queue.empty()

    def get_speech(self):
        if self.speech_waiting():
            return self.data_queue.get()
        return None

    def get_audio_data(self):
        now = datetime.utcnow()
        if self.speech_waiting():
            self.phrase_complete = False
            if self.phrase_time and now - self.phrase_time > timedelta(
                seconds=self.phrase_timeout
            ):
                self.last_sample = bytes()
                self.phrase_complete = True
            self.phrase_time = now

            # Concatenate our current audio data with the latest audio data.
            while self.speech_waiting():
                data = self.get_speech()
                self.last_sample += data

            # Use AudioData to convert the raw data to wav data.
            with sr.Microphone() as source:
                audio_data = sr.AudioData(
                    self.last_sample, source.SAMPLE_RATE, source.SAMPLE_WIDTH
                )
            return audio_data

        return None


class Bear:
    def __init__(self, azure_speech_config):
        kit = MotorKit(i2c=board.I2C())
        self._arms_motor = kit.motor1
        self._mouth_motor = kit.motor2

        # Setup Foot Button
        self._foot_button = digitalio.DigitalInOut(board.D16)
        self._foot_button.direction = digitalio.Direction.INPUT
        self._foot_button.pull = digitalio.Pull.UP

        self.do_mouth_movement = False
        self._mouth_thread = threading.Thread(target=self.move_mouth, daemon=True)
        self._mouth_thread.start()
        if DEVICE_ID is None:
            audio_config = speechsdk.audio.AudioOutputConfig(use_default_speaker=True)
        else:
            audio_config = speechsdk.audio.AudioOutputConfig(device_name=DEVICE_ID)
        self._speech_synthesizer = speechsdk.SpeechSynthesizer(
            speech_config=azure_speech_config, audio_config=audio_config
        )

        self._speech_synthesizer.synthesizing.connect(self.start_moving_mouth)
        self._speech_synthesizer.synthesis_completed.connect(self.stop_moving_mouth)

    def start_moving_mouth(self, _event):
        self.do_mouth_movement = True

    def stop_moving_mouth(self, _event):
        self.do_mouth_movement = False

    def deinit(self):
        self.do_mouth_movement = False
        self._mouth_thread.join()
        self._arms_motor.throttle = None
        self._mouth_motor.throttle = None
        self._speech_synthesizer.synthesis_started.disconnect_all()
        self._speech_synthesizer.synthesis_completed.disconnect_all()

    def _move_arms_motor(self, dir_up=True):
        direction = -1 if dir_up else 1
        self._arms_motor.throttle = MOTOR_DUTY_CYCLE * direction
        time.sleep(ARM_MOVEMENT_TIME)
        # Remove Power from the motor to avoid overheating
        self._arms_motor.throttle = None

    def _move_mouth_motor(self, dir_open=True):
        duration = (
            BASE_MOUTH_DURATION
            + random.random() * SPEECH_VARIANCE
            - (SPEECH_VARIANCE / 2)
        )
        # Only power the motor while opening and let the spring close it
        self._mouth_motor.throttle = MOTOR_DUTY_CYCLE if dir_open else None
        time.sleep(duration)
        # Remove Power from the motor and let close to avoid overheating
        self._mouth_motor.throttle = None

    def foot_pressed(self):
        return not self._foot_button.value

    def move_mouth(self):
        print("Starting mouth movement thread")
        while True:
            if self.do_mouth_movement:
                self._move_mouth_motor(dir_open=True)
                self._move_mouth_motor(dir_open=False)

    def move_arms(self, hide=True):
        self._move_arms_motor(dir_up=hide)

    def speak(self, text):
        result = self._speech_synthesizer.speak_text_async(text).get()

        # Check result
        if result.reason == speechsdk.ResultReason.SynthesizingAudioCompleted:
            print("Speech synthesized for text [{}]".format(text))
        elif result.reason == speechsdk.ResultReason.Canceled:
            cancellation_details = result.cancellation_details
            print("Speech synthesis canceled: {}".format(cancellation_details.reason))
            if cancellation_details.reason == speechsdk.CancellationReason.Error:
                print("Error details: {}".format(cancellation_details.error_details))


def main():
    listener = Listener()
    bear = Bear(speech_config)

    transcription = [""]
    bear.speak(
        "Hello there! Just give my left foot a squeeze if you would like to get my attention."
    )
    while True:
        try:
            # If button is pressed, start listening
            if bear.foot_pressed():
                bear.speak("How may I help you?")
                listener.listen()

            # Pull raw recorded audio from the queue.
            if listener.speech_waiting():
                audio_data = listener.get_audio_data()
                bear.speak("Let me think about that")
                bear.move_arms(hide=True)
                text = transcribe(audio_data.get_wav_data())

                if text:
                    if listener.phrase_complete:
                        transcription.append(text)
                        print(f"Phrase Complete. Sent '{text}' to ChatGPT.")
                        chat_response = sendchat(text)
                        transcription.append(f"> {chat_response}")
                        print("Got response from ChatGPT. Beginning speech synthesis.")
                        bear.move_arms(hide=False)
                        bear.speak(chat_response)
                    else:
                        print("Partial Phrase...")
                        transcription[-1] = text

                os.system("clear")
                for line in transcription:
                    print(line)
                print("", end="", flush=True)
                time.sleep(0.25)
        except KeyboardInterrupt:
            break
    bear.deinit()


if __name__ == "__main__":
    main()

‎View on GitHub

Downloading the Code

To download the code onto your Pi, just run the following to ‎download:‎

Copy Code
cd ~
wget https://raw.githubusercontent.com/adafruit/Adafruit_Learning_System_Guides/main/ChatGPT_Bear/assistant.py

How the Python Code Works

This is an overview about how the code works. It's mostly a ‎combination of code to interface between:

  • Azure Speech Services API

  • OpenAI ChatGPT API

  • OpenAI Whisper API

  • SpeechRecognition Library

  • CircuitPython Motor Library

The code uses threading and events in order to be able to move the ‎mouth motors at the same time the audio output from the Azure ‎Speech Services is playing.‎

Parameters

The code starts out with a number of parameters that can be altered. ‎Here are the main parameters that you might want to change:

  • The SYSTEM_ROLE parameter is a description to ChatGPT about ‎how it should act

  • The CHATGPT_MODEL and WHISPER_MODEL parameters can be updated ‎as newer versions of the API become available

  • The AZURE_SPEECH_VOICE is the voice name that can be altered to ‎change how the bear sounds. See the Create an Account with ‎Azure page for more details on selecting a different voice in ‎Azure Speech Services

  • The RECORD_TIMEOUT is the amount of time in seconds that the ‎bear will listen after pushing the button on the foot

  • The DEVICE_ID is for specifying the ID of a particular Audio ‎Output Device. See the Troubleshooting section on ‎the Usage page of this guide to find the right value. Leaving it ‎set to None will try and use the system default device

The remaining parameters have already been tuned pretty well, but ‎you are welcome to experiment with them.‎

‎Download File‎

Copy Code
# ChatGPT Parameters
SYSTEM_ROLE = (
    "You are a helpful voice assistant in the form of a talking teddy bear"
    " that answers questions and gives information"
)
CHATGPT_MODEL = "gpt-3.5-turbo"
WHISPER_MODEL = "whisper-1"

# Azure Parameters
AZURE_SPEECH_VOICE = "en-GB-OliverNeural"
DEVICE_ID = None

# Speech Recognition Parameters
ENERGY_THRESHOLD = 1000  # Energy level for mic to detect
PHRASE_TIMEOUT = 3.0  # Space between recordings for sepating phrases
RECORD_TIMEOUT = 30

# Motor Parameters
ARM_MOVEMENT_TIME = 0.5
BASE_MOUTH_DURATION = 0.2  # A higher number means slower mouth movement
SPEECH_VARIANCE = 0.1  # Higher allows more mouth movement variance.
                       # It pauses for BASE_MOUTH_DURATION ± SPEECH_VARIANCE
MOTOR_DUTY_CYCLE = 1.0  # Lower provides less power to the motors

Initialization

Grab the API parameters from the environment variables and create ‎the speech configuration.‎

Download File

Copy Code
openai.api_key = os.environ.get("OPENAI_API_KEY")
speech_key = os.environ.get("SPEECH_KEY")
service_region = os.environ.get("SPEECH_REGION")

speech_config = speechsdk.SpeechConfig(subscription=speech_key, region=service_region)
speech_config.speech_synthesis_voice_name = AZURE_SPEECH_VOICE

OpenAI API Interface Helpers

The sendchat and transcribe functions are for packaging and sending ‎data to the ChatGPT and Whisper APIs respectively.‎

‎Download File‎

Copy Code
def sendchat(prompt):
    completion = openai.ChatCompletion.create(
        model=CHATGPT_MODEL,
        messages=[
            {"role": "system", "content": SYSTEM_ROLE},
            {"role": "user", "content": prompt},
        ],
    )
    # Send the heard text to ChatGPT and return the result
    return completion.choices[0].message.content


def transcribe(wav_data):
    # Read the transcription.
    print("Transcribing...")
    attempts = 0
    while attempts < 3:
        try:
            with NamedTemporaryFile(suffix=".wav") as temp_file:
                result = openai.Audio.translate_raw(
                    WHISPER_MODEL, wav_data, temp_file.name
                )
                return result["text"].strip()
        except (openai.error.ServiceUnavailableError, openai.error.APIError):
            time.sleep(3)
        attempts += 1
    return "I wasn't able to understand you. Please repeat that."

The Listener Class

The Listener class interfaces with the SpeechRecognition library to ‎handle listening for speech and returning the prepared audio data.‎

‎Download File‎

Copy Code
class Listener:
    def __init__(self):
        self.listener_handle = None
        self.recognizer = sr.Recognizer()
        self.recognizer.energy_threshold = ENERGY_THRESHOLD
        self.recognizer.dynamic_energy_threshold = False
        self.recognizer.pause_threshold = 1
        self.last_sample = bytes()
        self.phrase_time = datetime.utcnow()
        self.phrase_timeout = PHRASE_TIMEOUT
        self.phrase_complete = False
        # Thread safe Queue for passing data from the threaded recording callback.
        self.data_queue = Queue()
        self.mic_dev_index = None

    def listen(self):
        if not self.listener_handle:
            with sr.Microphone() as source:
                print(source.stream)
                self.recognizer.adjust_for_ambient_noise(source)
                audio = self.recognizer.listen(source, timeout=RECORD_TIMEOUT)
            data = audio.get_raw_data()
            self.data_queue.put(data)

    def record_callback(self, _, audio: sr.AudioData) -> None:
        # Grab the raw bytes and push it into the thread safe queue.
        data = audio.get_raw_data()
        self.data_queue.put(data)

    def speech_waiting(self):
        return not self.data_queue.empty()

    def get_speech(self):
        if self.speech_waiting():
            return self.data_queue.get()
        return None

    def get_audio_data(self):
        now = datetime.utcnow()
        if self.speech_waiting():
            self.phrase_complete = False
            if self.phrase_time and now - self.phrase_time > timedelta(
                seconds=self.phrase_timeout
            ):
                self.last_sample = bytes()
                self.phrase_complete = True
            self.phrase_time = now

            # Concatenate our current audio data with the latest audio data.
            while self.speech_waiting():
                data = self.get_speech()
                self.last_sample += data

            # Use AudioData to convert the raw data to wav data.
            with sr.Microphone() as source:
                audio_data = sr.AudioData(
                    self.last_sample, source.SAMPLE_RATE, source.SAMPLE_WIDTH
                )
            return audio_data

        return None

The Bear Class

The Bear class initializes and sets up the motors and button. It ‎handles the timing of the motors and the speech synthesis.‎

One interesting function inside of this class is the move_mouth function ‎which is threaded. It is in a constant loop and will constantly move ‎the mouth while the do_mouth_movement variable is true. This makes ‎turning the mouth movement on and off very easy.‎

In the initialization, there are also a couple of events that are ‎triggered by the Azure Speech Services API to time the mouth ‎movement to the speech much better. The way these events are set ‎up is by using the connect function and passing in the function that ‎will be called when triggered.‎‎

Download File‎

Copy Code
class Bear:
    def __init__(self, azure_speech_config):
        kit = MotorKit(i2c=board.I2C())
        self._arms_motor = kit.motor1
        self._mouth_motor = kit.motor2

        # Setup Foot Button
        self._foot_button = digitalio.DigitalInOut(board.D16)
        self._foot_button.direction = digitalio.Direction.INPUT
        self._foot_button.pull = digitalio.Pull.UP

        self.do_mouth_movement = False
        self._mouth_thread = threading.Thread(target=self.move_mouth, daemon=True)
        self._mouth_thread.start()
        if DEVICE_ID is None:
            audio_config = speechsdk.audio.AudioOutputConfig(use_default_speaker=True)
        else:
            audio_config = speechsdk.audio.AudioOutputConfig(device_name=DEVICE_ID)
        self._speech_synthesizer = speechsdk.SpeechSynthesizer(
            speech_config=azure_speech_config, audio_config=audio_config
        )

        self._speech_synthesizer.synthesizing.connect(self.start_moving_mouth)
        self._speech_synthesizer.synthesis_completed.connect(self.stop_moving_mouth)

    def start_moving_mouth(self, _event):
        self.do_mouth_movement = True

    def stop_moving_mouth(self, _event):
        self.do_mouth_movement = False

    def deinit(self):
        self.do_mouth_movement = False
        self._mouth_thread.join()
        self._arms_motor.throttle = None
        self._mouth_motor.throttle = None
        self._speech_synthesizer.synthesis_started.disconnect_all()
        self._speech_synthesizer.synthesis_completed.disconnect_all()

    def _move_arms_motor(self, dir_up=True):
        direction = -1 if dir_up else 1
        self._arms_motor.throttle = MOTOR_DUTY_CYCLE * direction
        time.sleep(ARM_MOVEMENT_TIME)
        # Remove Power from the motor to avoid overheating
        self._arms_motor.throttle = None

    def _move_mouth_motor(self, dir_open=True):
        duration = (
            BASE_MOUTH_DURATION
            + random.random() * SPEECH_VARIANCE
            - (SPEECH_VARIANCE / 2)
        )
        # Only power the motor while opening and let the spring close it
        self._mouth_motor.throttle = MOTOR_DUTY_CYCLE if dir_open else None
        time.sleep(duration)
        # Remove Power from the motor and let close to avoid overheating
        self._mouth_motor.throttle = None

    def foot_pressed(self):
        return not self._foot_button.value

    def move_mouth(self):
        print("Starting mouth movement thread")
        while True:
            if self.do_mouth_movement:
                self._move_mouth_motor(dir_open=True)
                self._move_mouth_motor(dir_open=False)

    def move_arms(self, hide=True):
        self._move_arms_motor(dir_up=hide)

    def speak(self, text):
        result = self._speech_synthesizer.speak_text_async(text).get()

        # Check result
        if result.reason == speechsdk.ResultReason.SynthesizingAudioCompleted:
            print("Speech synthesized for text [{}]".format(text))
        elif result.reason == speechsdk.ResultReason.Canceled:
            cancellation_details = result.cancellation_details
            print("Speech synthesis canceled: {}".format(cancellation_details.reason))
            if cancellation_details.reason == speechsdk.CancellationReason.Error:
                print("Error details: {}".format(cancellation_details.error_details))

The Main Function Loop

The main function starts off by setting up instances of ‎the Bear and Listener classes. It also sets up a transcript that it ‎maintains throughout interactions. This allows for you to see what is ‎being heard and what the bear is returning in a text format.‎

The Main Loop waits to the foot to be presses. Once pressed, it ‎listens for up to 30 seconds or until it determines a phase has been ‎spoken. Once it has a phrase, it is processed, and the bear moves ‎and responds appropriately.‎

Once you exit the main loop, a few things are deinitialized in order to ‎free up resources and hardware so that the bear isn't drawing excess ‎power.‎

Download File‎

Copy Code
def main():
    listener = Listener()
    bear = Bear(speech_config)

    transcription = [""]
    bear.speak(
        "Hello there! Just give my left foot a squeeze if you would like to get my attention."
    )
    while True:
        try:
            # If button is pressed, start listening
            if bear.foot_pressed():
                bear.speak("How may I help you?")
                listener.listen()

            # Pull raw recorded audio from the queue.
            if listener.speech_waiting():
                audio_data = listener.get_audio_data()
                bear.speak("Let me think about that")
                bear.move_arms(hide=True)
                text = transcribe(audio_data.get_wav_data())

                if text:
                    if listener.phrase_complete:
                        transcription.append(text)
                        print(f"Phrase Complete. Sent '{text}' to ChatGPT.")
                        chat_response = sendchat(text)
                        transcription.append(f"> {chat_response}")
                        print("Got response from ChatGPT. Beginning speech synthesis.")
                        bear.move_arms(hide=False)
                        bear.speak(chat_response)
                    else:
                        print("Partial Phrase...")
                        transcription[-1] = text

                os.system("clear")
                for line in transcription:
                    print(line)
                print("", end="", flush=True)
                time.sleep(0.25)
        except KeyboardInterrupt:
            break
    bear.deinit()

Assembly

hacks_Case_Assembly_Disassembly

Assembly Tool

The headers are much easier to install in the deep case by using a ‎tool. If you have a 5mm Hex Nut Driver, then go ahead and use that. ‎If not, you can make a tool out of a couple of extra nylon threaded ‎standoffs. This tool works by having two standoffs with more friction ‎extend into a third standoff that is being installed.‎

This tool just uses 2 of the 12mm threaded standoffs.

tool_82

Start by completely screwing one post into another until you feel ‎some resistance.‎

start_83

Continue tightening about an additional 1/6 turn until and line up ‎the flat edges. Don't over-tighten or the plastic could break off. The ‎idea is to have more friction between these two standoffs than you ‎will have with the standoff you are installing.‎

tight_84

To use, just thread the standoff that you are installing onto the ‎threads of the tool you assembled. Just use a minimal amount of ‎friction since you want it to come off of the tool when it's installed.‎

thread_85

Screw the standoff into a nut. When it is tight enough, just hold it in ‎place with a finger or flathead screwdriver and unscrew the tool ‎from the installed standoff.‎

standoff_86

Case Bottom

Make sure to remove any supports. A small flathead screwdriver or ‎so small needle-nosed pliers should work well.‎

case_87

For the bottom, you'll need this hardware:‎

  • The Case Bottom

  • ‎4 x 12mm nylon M2.5 standoffs‎

  • ‎4 x nylon M2.5 nuts‎

bottom_88

Insert the Raspberry Pi 4 in the bottom case. Make sure you don't ‎have a MicroSD card inserted! You'll want to have the A/V ports go ‎in first before pushing the other side down so that it is sitting flat.‎

insert_89

Place a nut into the hex insert on the bottom of the case.‎

nut_90

Install a standoff through the Pi and into the nut you inserted using a ‎tool.‎

install_91

Install standoffs into the remaining corners.‎

corners_92

Place the motor HAT onto the Pi. You can use the upper left side of ‎the case (the corner furthest away from any ports) to easily align the ‎GPIO headers.‎

headers_93

Case Top

Speaker and amp installation is only required if you are doing the ‎compact build option.‎

For the top, you'll need this hardware:

  • The Case Top

  • ‎2 x Speaker Retainers of the appropriate size

  • ‎4 x 8mm screws you set aside from disassembling the bear‎

hardware_94

Place the speaker into the speaker holder.‎

speaker_95

Install the speaker retainers on each side of the speaker using the ‎screws from the bear.‎

install_96

The wires are a bit of a tight fit, so it's easier to install them in the ‎MAX98357 terminal first. Place the wires in the appropriate terminal ‎so that they have enough length once installed.‎

wires_97

Once installed, you may need to bend the wires a little to the sides to ‎give them enough room to fit.‎

once_98

Install the MAX98357 using 2 more screws from the bear.‎

screws_99

Final Case Assembly

Place the wiring for the foot in the slot in the case.‎

foot_100

Tie a knot in the wiring close to the case, just on the outside.‎

tie_101

Now lift up the wire and place it so the knot so it is on the inside. This ‎will act as a strain relief.‎

lift_102

This is a good time to install the wiring for the motor power. On the ‎USB cable, the negative wire is the side with the white stripes. Be ‎sure to install correctly to avoid any damage.

time_103

If you built an adapter, just use the jumper wires instead.‎

adapter_104

Install the lid by placing it directly over the case bottom and ‎lowering it. If the strain relief knot is in the way, you can push it in ‎temporarily while placing the lid. It may take a little bit of adjusting if ‎some of the wires are in the way.‎

lid_105

You will need four 10mm nylon screws to attach the lid.‎

nylon_106

Install the screws into the top. Only turn just enough that it feels a ‎little snug. It's very easy to overturn the screws and break them.‎

top_107

You may also want to loosen the appropriate screws for the motor ‎wire terminals. However, those can be installed after the case is ‎assembled.‎

loosen_108

When you connect the wires from the bear, the wire order is ‎important. Install the wires to the M2 and M2 terminals as shown in ‎the photo.‎

connector_109

USB Speaker

If you went with the easier install option, just plug the speaker into ‎one of the USB ports of the Raspberry Pi. We'll show you how to ‎configure it later.‎

speaker_110

USB Microphone

Be sure to install the USB microphone.‎

microphone_111

If you would like to be able to control where the sound is picked up, you could use a simple USB extension cable.‎

microphone_112

Power Connections

To power the Raspberry Pi and motors, you'll want the USB power ‎bank along with a short USB cable. If you don't have any extras, you ‎can use the USB cable that came with the power bank.‎

power_113

Connect the USB cable between one port of the power Bank and the ‎Raspberry Pi.‎

Connect the other USB cable for motor power to the other port.‎

If the power bank turns on automatically, you can force it back off by ‎double-pressing the power button.‎

power_114

Final Bear Assembly

Remove as much stuffing as you need. Depending on the build ‎options you decided on, you may need to remove a little or a lot of ‎the stuffing from the bear.‎

stuffing_115

If you used the external speaker, place it inside the head. Keep ‎taking out stuffing as needed. The fit is a bit tight.‎

If you placed your microphone on an extension, you will want to ‎place this in the head at the same time. Try and keep it as close to ‎the surface as possible, so the stuffing doesn't muffle the sound too ‎much.‎

Replace some of the stuffing back into the head afterwards until if ‎feels like it is held in place and the head looks normal. ‎

stuffing_116

Place any excessively long cords into the bear next. Keep the USB ‎plugs that go into the battery accessible.‎

place_117

Place the enclosure into the bear next. There's a small hole so you ‎can see the status lights. Having that face down lets you easily know ‎if the Pi is powered up or not. Continue adding stuffing but leave ‎room for the battery.‎

enclosure_118

Place the battery in. Add some more stuffing. Add just enough so ‎the body looks natural. Remember, you will need to remove the ‎battery pack to charge it or turn it off and on.‎

Be careful of the plugs sticking out of the Pi. It's easy to accidentally ‎break off connectors with everything jammed in so tight.‎

plugs_119

Finally close the flap using the Velcro under the tail.‎

flap_120

Check how well the bear sits. You may need to shift things around a ‎bit or add or remove stuffing if it doesn't look right.‎

Keep in mind, the speaker in the head can make it a bit top heavy, ‎which can cause it to fall over when the arms move. Try and keep ‎most of the weight a bit lower if possible.‎

head_121

Usage

hacks_Main_Image_Tighter

When you are ready to use the bear, open the flap on the bottom ‎and just give it a final check to make sure the battery is charged, and ‎you have all of the cables connected. Make sure the battery and Pi ‎are powered on.‎

Connect to the bear over Wi-Fi using SSH. Once you are logged in, ‎type the following:‎

Copy Code
cd ~
python3 assistant.py

The bear should start talking and prompt you to squeeze its foot. ‎Squeeze the foot and then ask it a question or request something.‎

Here are a few examples of requests to try:‎

  • Tell me a joke

  • Tell me a story about a robotic bear

  • Tell me a poem about video game characters

  • Tell me about CircuitPython

When you are finished. Just press Control+C a couple of times. ‎Because of the multi-threading, sometimes it takes a moment to ‎stop.‎

Troubleshooting

No Keys

Make sure you have specified your API keys before running the script. ‎It should let you know if it wasn't able to find those values. If you set ‎the values in /etc/environ, then you must reboot before the values ‎will be loaded. If you would like to see a list of your environment ‎variables, run the following command:‎

Copy Code
printenv

You should see a list of variables specific to your setup.‎

No Audio

If you hear no sound when you run the script, it could be caused by a ‎few things. To begin with, run through the tests specific to the way ‎you set up device.‎

You can also try running the following command to test the audio:‎

Copy Code
speaker-test

If you have verified that sound comes through with speaker-test, you ‎may need to set the DEVICE_ID. To determine the Device ID, just run ‎the following command:‎

Copy Code
aplay -L | grep plughw:

You should get a list of IDs. that begin with plughw like this:‎

code_123

For instance, if you have the USB Speaker, you should see a device ‎like plughw:CARD=UACDemoV10,DEV=0. Set the DEVICE_ID variable ‎to that value and it should use that.‎

Download File

Copy Code
DEVICE_ID = "plughw:CARD=UACDemoV10,DEV=0"
Número de parte del fabricante 2348
DC STEP MTR HAT FOR RASPBERRY PI
Adafruit Industries LLC
$22.50
Ver más Details
Número de parte del fabricante 3006
EVAL BOARD FOR MAX98357A
Adafruit Industries LLC
Número de parte del fabricante 3369
MINI EXTERNAL USB STEREO SPEAKER
Adafruit Industries LLC
$12.50
Ver más Details
Número de parte del fabricante 3299
BLACK NYLON SCREW AND STAND-OFF
Adafruit Industries LLC
$16.95
Ver más Details
BREADBOARD-FRIENDLY PCB MOUNT MI
Número de parte del fabricante 1898
BREADBOARD-FRIENDLY PCB MOUNT MI
Adafruit Industries LLC
Número de parte del fabricante 1957
JUMPER WIRE M TO M 6" 28AWG
Adafruit Industries LLC
Número de parte del fabricante 368
ADAPT TERM BL 2POS TO 2.1MM JCK
Adafruit Industries LLC
Número de parte del fabricante CFR-25JB-52-100R
RES 100 OHM 5% 1/4W AXIAL
YAGEO
Número de parte del fabricante 3083
ALUM HEAT SINK FOR RASPBERRY PI
Adafruit Industries LLC
Número de parte del fabricante 2880
2-PIN JST SM PLUG + RECEPTACLE C
Adafruit Industries LLC
Número de parte del fabricante 5131
WIRE FERRULE KIT - 800 PIECES
Adafruit Industries LLC
$17.95
Ver más Details
Número de parte del fabricante 4055
CBL USB2.0 A RCPT TO A PLG 0.98'
Adafruit Industries LLC
Número de parte del fabricante SC0194(9)
SBC 1.5GHZ 4 CORE 4GB PI 4 MOD B
Raspberry Pi
$100.00
Ver más Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.