Maker.io main logo

Make a Magic 6-Ball Randomiser with Dice Project Kit and Value Acrylic

255

2025-02-20 | By Kitronik Maker

License: See Original Project Laser Cutters

Courtesy of Kitronik

Guide by Kitronik Maker

Forget the Magic 8 Ball, the new Kitronik Magic 6 Ball is where it’s at! Using the Kitronik Dice ‎Project Kit and some Value Acrylic, you too can create a fun randomiser with life advice. ‎Download the dxf zip file and follow, our in-house animator/designer, Kev's instructions.‎

This is a great hands-on activity for the classroom, combining practical electronics and ‎design. As with all electronic kits that form a part of a larger design, studying the electronics ‎is optional. Great outcomes can be obtained by just soldering together the kit and ‎designing a custom enclosure to house it.

covers_1

What you’ll need:‎

label_2

Step 1 - Get Soldering:

Start by soldering the dice kit together, making sure that the LEDs and switch sit higher than ‎the IC Socket and they are all the same distance off the board. You will need to use the legs ‎that have been cut off the resistors to extend the legs on the switch.‎

solder_3

Step 2 - Download and Laser:‎

You can download our free dxf file for the Magic 6 Ball right here.‎

dxf_4

Here’s our guide to engraving it and cutting. We have suggested engraving the main base ‎with the words Magic 6 Ball purely as a guide when it comes to gluing the white letters, but ‎this is optional as it can take a while depending on how deep you want the engrave.‎

Get cutting your green, black, and white Kitronik Value Acrylic!‎

acrylic_5

Step 3 - Stick Around:‎

Using super glue, get sticking all your cut elements together…‎

‎‎Step 4 - Lights…‎

When everything is dry and fully stuck, insert the Panel Mount LED clips into the four corner ‎holes and push the fully soldered kit into place…‎

lights_6

Step 5 - Should I eat this Cake?‎

Ask a question and push the Dice Kit button. The dice lights correspond to the engraved ‎answers around the edge of the 6 Ball.‎

Good luck…‎

step5_7

Download the Vol 3 PDF!‎‎ ‎

©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof ‎without Kitronik’s prior written consent.

Número de parte del fabricante 2109
DICE PROJECT KIT
Kitronik Ltd.
Número de parte del fabricante 4749
BLACK LED DIFFUSION ACRYLIC PANE
Adafruit Industries LLC
Número de parte del fabricante SSH-LX5091
HOLDER LED PANEL 5MM BLACK NYLON
Lumex Opto/Components Inc.
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.