Maker.io main logo

Introduction to FPGA Part 8 - Memory and Block RAM

1,771

2021-12-27 | By ShawnHymel

License: Attribution

A field-programmable gate array (FPGA) is a reconfigurable integrated circuit (IC) that lets you implement a wide range of custom digital circuits. Throughout the series, we will examine how an FPGA works as well as demonstrate the basic building blocks of implementing digital circuits using the Verilog hardware description language (HDL).

Storing large amounts of data can be difficult in FPGAs if you use just logic cells. Each cell (usually) contains one look-up table (LUT) and a D flip-flop. Storing data in the D flip-flops (e.g. 1 bit of information) would quickly consume all of your logic cells. Some synthesis tools will allocate LUTs to be used as memory if the data requirements are low enough. This is known as “distributed” random access memory (RAM).

However, most FPGAs offer other types of memory alongside their reprogrammable fabric. Most commonly, you’ll see chunks of memory called “block RAM” that you can allocate to store data. Unless specified in code, the synthesis tool will determine (based on your data requirements) if distributed RAM or block RAM is used for your design.

In the previous tutorial, we demonstrated how to write Verilog testbenches and simulate designs using Icarus Verilog. This time, we show how to allocate block RAM in the iCE40 and read/write data to/from it. We also show how to initialize values in the RAM from a text file.

Video

If you have not done so, please watch the following video, which explains the concepts required to complete the challenge. It also demonstrates a working version of the challenge:

 

Required Hardware

For this challenge, you will need the following hardware:

Hardware Connections

The PMOD connector at the end of the iCEstick has the following pinout:

iCEstick PMOD connector pinout

A full pinout of the iCEstick can be found here.

Connect 4 pushbuttons to the iCEstick as follows. Note that you do not need pull-up resistors on the buttons. We will use the internal pull-up resistors available in the FPGA.

iCEstick connections to buttons Fritzing diagram

Resources

The following datasheets and guides might be helpful as you tackle the challenges:

Challenge

Your challenge is to create a simple LED sequencer. You should configure your 4 pushbuttons as follows:

  • RST: reset button (globally reset all counters, state machines, etc.)

  • SET: set button that records the value on VAL[1:0] into a memory location and then increments the memory pointer

  • PTN[0]: first bit of the value/pattern

  • PTN[1]: second bit of the value/pattern

The idea is that you can record a simple sequence (up to 8 values) in block RAM. You do this by holding down VAL[1:0] to create a number (e.g. binary 00, 01, 10, or 11) and then pressing the SET button. When the SET button is pressed, the 2-bit binary value is stored in memory and the memory address pointer is increased by one. You repeat the process, holding down a new 2-bit binary number.

You continue doing this until you’ve filled up the sequencer memory with 8 values. At the same time, the sequencer is continuously cycling through the memory, reading each value and displaying it on 2 of the LEDs.

So, if you enter the sequence 0, 1, 0, 1, 2, 3, 2, 1, on the next full loop, the sequencer would display the following binary values on the LEDs: 00, 01, 00, 01, 10, 11, 10, 01.

Hint: you will likely need to use many of the concepts and modules you wrote from previous videos/challenges! This includes a clock divider and a button debounce module. You will also likely want to make these designs modular and instantiate them in a top-level design. Finally, I highly recommend simulating your design to make sure everything works.

Solution

Spoilers below! I highly encourage you to try the challenge on your own before comparing your answer to mine. Note that my solution may not be the only way to solve the challenge.

The code for this project is too large to paste onto this page in its entirety. As a result, you can find all of the Verilog modules, physical constraint file, memory initialization text file, and testbench/simulation files in this repository.

In this project, I use the clock-divider, debouncer, and memory Verilog modules written in this and previous episodes/challenges. I also create a top-level design (named sequencer-top.v) that brings together these modules and provides some glue logic:

sequencer-top.v

Copy Code
// Top-level design for sequencer
// 
// Inputs:
//      clk         - 12 MHz clock
//      rst_btn     - pushbutton (RESET)
//      set_btn     - pushbutton (SET value at next memory address)
//      ptn_0_btn   - pushbutton (PATTERN[0] for sequence)
//      ptn_1_btn   - pushbutton (PATTERN[1] for sequence)
// 
// Outputs:
//      led[1:0]    - LEDs
// 
// Push RESET to set everything to 0. Hold PATTERN[0] and/or PATTERN[1] and 
// press SET to record value in memory. Continue doing this for up to 8 memory
// locations. Sequence will play on LEDs and loop forever.
//
// Date: November 15, 2021
// Author: Shawn Hymel
// License: 0BSD

// Top-level design for the sequencer
module sequencer_top #(

    // Parameters
    parameter   DEBOUNCE_COUNTS = 480000 - 1,   // Counts for debounce wait
    parameter   STEP_COUNTS = 6000000 - 1,      // Clock cycles between steps
    parameter   NUM_STEPS = 8                   // Number of steps

) (

    // Inputs
    input               clk,
    input               rst_btn,
    input               set_btn,
    input               ptn_0_btn,
    input               ptn_1_btn,
    
    // Outputs
    output  reg [1:0]   led,
    output      [2:0]   unused_led
);
    
    // Internal signals
    wire            rst;
    wire            set;
    wire            set_d;
    wire    [1:0]   ptn;
    wire            div_clk;
    wire    [1:0]   r_data;
    
    // Storage elements (initialize some values)
    reg             w_en = 0;
    reg             r_en = 1'b1;    // Always high!
    reg     [2:0]   w_addr = 0;
    reg     [2:0]   r_addr;
    reg     [1:0]   w_data;
    reg     [2:0]   step_counter;
    reg     [2:0]   mem_ptr = 0;
    
    // Turn off unused LEDs
    assign unused_led = 3'b000;
    
    // Invert active-low buttons
    assign rst = ~rst_btn;
    assign set = ~set_btn;
    assign ptn[0] = ~ptn_0_btn;
    assign ptn[1] = ~ptn_1_btn;
    
    // Clock divider
    clock_divider #(
        .COUNT_WIDTH(24), 
        .MAX_COUNT(STEP_COUNTS)
    ) div (
        .clk(clk),
        .rst(rst),
        .out(div_clk)
    );
    
    // Button debouncer for set buttons
    debouncer #(
        .COUNT_WIDTH(24),
        .MAX_CLK_COUNT(DEBOUNCE_COUNTS)
    ) set_debouncer (
        .clk(clk),
        .rst(rst),
        .in(set),
        .out(set_d)
    );
    
    // Memory unit
    memory #(   
        .MEM_WIDTH(2), 
        .MEM_DEPTH(NUM_STEPS), 
        .INIT_FILE("mem_init.txt")
    ) mem (
        .clk(clk),
        .w_en(w_en),
        .r_en(r_en),
        .w_addr(w_addr),
        .r_addr(r_addr),
        .w_data(w_data),
        .r_data(r_data)
    );
    
    // Read from memory each divided clock cycle
    always @ (posedge div_clk or posedge rst) begin
        if (rst == 1'b1) begin
            led <= 0;
            r_addr <= 0;
            step_counter <= 0;
        end else begin
            r_addr <= step_counter;
            step_counter <= step_counter + 1;
            led <= r_data;
        end
    end
    
    // Register write data as soon as debounced set signal goes high
    always @ (posedge set_d) begin
        w_data <= ptn;
    end
    
    // Handle writing pattern to memory
    always @ (posedge clk or posedge rst) begin
    
        // Reset memory address pointer and write enable signal
        if (rst == 1'b1) begin
            mem_ptr <= 0;
            w_en <= 1'b0;
            
        // Set write enable high and increment memory pointer
        end else if (set_d == 1'b1) begin
            w_addr <= mem_ptr;
            w_en <= 1'b1;
            mem_ptr <= mem_ptr + 1;
        
        // Reset write enable signal
        end else begin
            w_en <= 1'b0;
        end
    end
    
endmodule

In this design, we invert the button signals and instantiate the clock divider, debouncer, and memory modules. Note that we instantiate the memory module to use block RAM that is 2 bits wide and 8 elements deep.

Next, we read from memory on each divided clock cycle:

Copy Code
    // Read from memory each divided clock cycle
    always @ (posedge div_clk or posedge rst) begin
        if (rst == 1'b1) begin
            led <= 0;
            r_addr <= 0;
            step_counter <= 0;
        end else begin
            r_addr <= step_counter;
            step_counter <= step_counter + 1;
            led <= r_data;
        end
    end

The value in memory is clocked/registered to the output LEDs. The step_counter (i.e. the read memory address pointer) is also increased by one. Because step_counter is only 3 bits wide, it will automatically wrap from 0x7 to 0x0, so we don’t need additional logic to prevent the pointer from exceeding the memory address space.

In parallel, the value on the pattern buttons (ptn[1:0]) is registered so that it can be written to memory on the next (non-divided) clock cycle (even if you let go of the ptn buttons after pressing the set button).

Copy Code
    // Register write data as soon as debounced set signal goes high
    always @ (posedge set_d) begin
        w_data <= ptn;
    end

Finally, we handle writing the pattern to memory:

Copy Code
    // Handle writing pattern to memory
    always @ (posedge clk or posedge rst) begin
    
        // Reset memory address pointer and write enable signal
        if (rst == 1'b1) begin
            mem_ptr <= 0;
            w_en <= 1'b0;
            
        // Set write enable high and increment memory pointer
        end else if (set_d == 1'b1) begin
            w_addr <= mem_ptr;
            w_en <= 1'b1;
            mem_ptr <= mem_ptr + 1;
        
        // Reset write enable signal
        end else begin
            w_en <= 1'b0;
        end
    end

Whenever the debounced set signal (a single pulse) is seen, the write enable (w_en) line is pulsed for a clock cycle while the pattern is present on the write data (w_data) bus. Note that the pointer for the write address (w_addr) is set from a separate mem_ptr value, which is also incremented.

Save all of these files in a single folder. Initialize the project with apio, verify, and run simulation:

Copy Code
apio init -b icestick
apio verify
apio sim

You should see GTKWave open with the simulated design. Zoom out, and make sure that the pattern is stored in memory. Note that the initialization memory file has the pattern stored as: 0, 0, 0, 0, 1, 1, 1, 1. So, you should see: 3, 3, 0, 0, 1, 1, 1, 1 after the pattern has been set from the simulated buttons.

Simulated sequencer in GTKWave

Now, enter the following to upload the design to your FPGA:

Copy Code
apio build
apio upload

Try entering new patterns on the buttons and see if the sequencer replays them!

Testing the LED sequencer

Recommended Reading

The following content might be helpful if you would like to dig deeper:

Número de parte del fabricante ICE40HX1K-STICK-EVN
BOARD EVAL FPGA ICESTICK
Lattice Semiconductor Corporation
$158.75
Ver más Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.