Maker.io main logo

CLUE Text Telephone Transmitter

98

2024-10-18 | By Adafruit Industries

License: See Original Project Amplifiers Bluetooth / BLE Sound

Courtesy of Adafruit

Guide by John Park

Overview

 

The TTY machine (a.k.a., Teletype/textphone/Minicom) is a ‎communications device similar to a teleprinter that is used to send ‎text messages over the public switched telephone network.‎

The TTY was developed in the 1960s to assist deaf and hard-of-‎hearing users in communicating over the telephone system. It ‎consists of a keyboard, display, and acoustic coupler for a phone ‎handset (some also included a small continuous roll printer or ‎interface for external printers). The TTY converts typed characters to ‎audio signals which can be sent over the phone system to TTY ‎machine on the receiving end, where those audio signals would be ‎converted back to text for display.‎

The TTY was supplanted in the 1990s by modern services such as ‎instant messaging on computers and texting on phones (as well as ‎video calls and video relay services for sign language use) but the ‎technology is interesting to study, and in fact still works on some ‎phone exchanges.‎

In this guide we'll take a look at how the TTY uses audio tones to ‎communicate and build our own transmitter with a CLUE capable of ‎sending messages to a TTY machine, both in standalone mode and ‎in Bluetooth LE mode with messages being sent from iOS or Android.‎

 

 

Parts

Huge thanks to Tod Kurt and Jan Goolsbey for their insights into ‎implementing a frequency shift keyed communications protocol and ‎to Jeff Epler and Carter Nelson for helping make the code efficient ‎and effective.‎

TTY Fundamentals

‎5-Bit Encoding

TTY machines send and receive audio signals (usually over the ‎phone line) which are encoded and decoded as text. They feature a ‎small typing keyboard, display, phone handset acoustic coupling ‎modem, and often a small printer or printer port.‎

TTY machines typically use a 5-bit character encoding protocol based ‎on Baudot code that was developed in 1870 for telegraph ‎transmission of the Roman alphabet, numbers, and symbols.‎

The chirping you'll hear when typing a letter on a TTY machine are ‎‎1400Hz and 1800Hz tones being shifted in 5-bit sets to represent the ‎full character, number, and symbol set. You can see the frequencies ‎of the letter A visualized here -- we'll take a closer look at the specific ‎meaning below.‎

encoding_1

encoding_2

The protocol is defined in this specification document. Here are ‎some relevant selections:‎

A.1 Mode of operation

ANNEX A

‎5-bit operational mode

The 5-bit mode is defined in ANSI TIA/EIA-825 (2000), A Frequency ‎Shift Keyed Modem for use on the Public Switched Telephone ‎Network.

The communication channel is half-duplex with no channel ‎turnaround. Carrier is transmitted 150 ms before the first character is ‎transmitted. The receiver shall be disabled for 300 ms when a ‎character is transmitted to mitigate false detection of echoes (in ‎non-V.18 devices, the carrier may remain for up to 1 s after the last ‎character to provide this same function). ‎

A.2 Modulation

The modulation is frequency shift-keyed modulation (i.e. no carrier is ‎present when a character is not being transmitted) using 1400 Hz ‎‎(±5%) for a binary 1 and 1800 Hz (±5%) for a binary 0. A bit duration of ‎either 20 or 22.00 ± 0.40 ms is used providing either a nominal data ‎signaling rate of 50 or 45.45 bits/s respectively. ‎

Looking at our captured audio from the letter A, here's what we see:‎

audio_3

  • A bit is 20ms in duration

  • The lower frequency 1400Hz tone is used both as the carrier ‎tone and to represent a binary 1

  • The higher frequency 1800Hz tone is used to represent binary 0

  • Letter A (see full chart below) has a binary 5-bit encoding ‎of 00011

  • ‎5-bit character codes are sent with in order of least signifigant ‎bit (so "right-to-left"), which means the A bits are transmitted ‎as 11000

  • The start bit is a binary 0 sent for 1 bit time, while the stop bit is ‎a binary 1 sent for at least 1.5-bit time

Put all of that together and we get this:‎

carrier (for 150ms) + 0 + 11000 + 1 (for 40ms)‎‎ ‎

Play the file below to hear the A audio looped five times.‎

tty_5

One other important feature of the TTY 5-bit code is the ‎implementation of character sets. With 5 bits we can only encode 32 ‎characters, however there are two mode character codes reserved ‎‎(sort of like a shift or control key) for switching the decoder between ‎‎"letters" and "figures".‎

When the LTRS mode character (11111) is sent, all characters that ‎follow are decoded as their alphabet letter version. When the FIGS ‎mode character (11011) is sent, all characters that follow are decoded ‎as their numerical or symbol variant.‎

In practice:‎

  • ‎11111 + 01101 would decode as F

  • ‎11011 + 01101 would decode as !‎

The mode character should be sent right before any shift to the other ‎mode, or every 72 characters even if you are staying in one mode.‎

You'll notice these mode swaps when typing on a TTY machine ‎because some keystrokes will suddenly sound twice as long as the ‎mode character is sent right before the letter or figure character.‎

Now, let’s implement this in CircuitPython to send tones over a ‎speaker and into the TTY system.‎

CircuitPython on CLUE

CircuitPython is a derivative of MicroPython designed to simplify ‎experimentation and education on low-cost microcontrollers. It ‎makes it easier than ever to get prototyping by requiring no upfront ‎desktop software downloads. Simply copy and edit files on ‎the CIRCUITPY flash drive to iterate.‎

The following instructions will show you how to install CircuitPython. ‎If you've already installed CircuitPython but are looking to update it ‎or reinstall it, the same steps work for that as well!‎

Set up CircuitPython Quick Start!‎

Follow this quick step-by-step for super-fast Python power :)‎

Download the latest version of CircuitPython for CLUE from ‎circuitpython.org

Click the link above to download the latest version of ‎CircuitPython for the CLUE.‎

Download and save it to your desktop (or wherever is handy).‎

click_6

Plug your CLUE into your computer using a known-good USB cable.‎

A lot of people end up using charge-only USB cables and it is very ‎frustrating! So, make sure you have a USB cable you know is good ‎for data sync.‎

Double-click the Reset button on the top (magenta arrow) on your ‎board, and you will see the NeoPixel RGB LED (green arrow) turn ‎green. If it turns red, check the USB cable, try another USB port, ‎etc. Note: The little red LED next to the USB connector will pulse red. ‎That's ok!‎

If double-clicking doesn't work the first time, try again. Sometimes it ‎can take a few tries to get the rhythm right!‎

board_7

You will see a new disk drive appear called CLUEBOOT.‎

Drag the adafruit-circuitpython-clue-etc.uf2 file to CLUEBOOT.‎

drive_8

drive_9

The LED will flash. Then, the CLUEBOOT drive will disappear, and a ‎new disk drive called CIRCUITPY will appear.‎

If this is the first time, you're installing CircuitPython or you're doing ‎a completely fresh install after erasing the filesystem, you will have ‎two files - boot_out.txt, and code.py, and one folder - lib on ‎your CIRCUITPY drive.‎

If CircuitPython was already installed, the files present before ‎reloading CircuitPython should still be present on ‎your CIRCUITPY drive. Loading CircuitPython will not create new ‎files if there was already a CircuitPython filesystem present.‎

That's it, you're done! :)‎

drive_10

Assemble the Transmitter

assemble_11

To get a nice, clear audio output from the CLUE, we'll add an ‎amplifier/speaker breakout board. The STEMMA Speaker board plus ‎JST-to-alligator clips cable makes it easy.‎

Hook Up

Plug the JST 3-pin cable into the STEMMA Speaker board. It is keyed ‎to only go in one way.‎

Now, connect the three alligator clips to the CLUE board from the ‎back side. Make these connections:‎

  • white to pin #0

  • red to pin 3V

  • black to pin GND

hookup_12

hookup_13

hookup_14

If you are sending audio TTY transmissions over a phone line to a TTY ‎machine on the other end of the line, you'll simply hold the STEMMA ‎speaker to the mouthpiece of your phone handset.‎

To test on a local machine (and see the text show up on the ‎supremely awesome vacuum fluorescent display!) you can hold the ‎speaker to the mic input coupler, or more permanently attach it with ‎rubber bands as shown below.‎

Wrap two rubber bands around the mouthpiece coupler on the TTY ‎machine.‎

Place the STEMMA speaker directly over the coupler stalk.‎

Criss cross the rubber bands over the STEMMA speaker board to hold ‎it snugly in place (the fewer unwanted mechanical vibrations the ‎better).‎

You may also use a single rubber band to hold the CLUE board onto ‎the battery cover as shown.‎

wrap_15

wrap_16

wrap_17

wrap_18

wrap_19

Power

Most TTY machines can be powered from batteries or a DC 9V wall ‎adapter.‎

You can choose to power your CLUE from USB power or a battery, ‎such as a LiPo or a small 3x AAA battery pack.‎

power_20

Code the TTY Transmitter

 

 

Text Editor

Adafruit recommends using the Mu editor for editing your ‎CircuitPython code. You can get more info in this guide.‎

Alternatively, you can use any text editor that saves files.‎

Installing Project Code

To use with CircuitPython, you need to first install a few libraries, into ‎the lib folder on your CIRCUITPY drive. Then you need to ‎update code.py with the example script.‎

Thankfully, we can do this in one go. In the example below, click ‎the Download Project Bundle button below to download the ‎necessary libraries and the code.py file in a zip file. Extract the ‎contents of the zip file, open the ‎directory Baudot_TTY/baudot_tty/ and then click on the directory ‎that matches the version of CircuitPython you're using and copy the ‎contents of that directory to your CIRCUITPY drive.‎

Your CIRCUITPY drive should now look similar to the following ‎image:‎

drive_21

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2020 John Park for Adafruit Industries
#
# SPDX-License-Identifier: MIT

### Baudot TTY Message Transmitter

### The 5-bit mode is defined in ANSI TIA/EIA-825 (2000)
### "A Frequency Shift Keyed Modem for use on the Public Switched Telephone Network"

import time
import math
import array
import board
from audiocore import RawSample
import audiopwmio

# constants for sine wave generation
SIN_LENGTH = 100  # more is less choppy
SIN_AMPLITUDE = 2 ** 12  # 0 (min) to 32768 (max)  8192 is nice
SIN_OFFSET = 32767.5  # for 16bit range, (2**16 - 1) / 2
DELTA_PI = 2 * math.pi / SIN_LENGTH  # happy little constant

sine_wave = [
    int(SIN_OFFSET + SIN_AMPLITUDE * math.sin(DELTA_PI * i)) for i in range(SIN_LENGTH)
]
tones = (
    RawSample(array.array("H", sine_wave), sample_rate=1800 * SIN_LENGTH),  # Bit 0
    RawSample(array.array("H", sine_wave), sample_rate=1400 * SIN_LENGTH),  # Bit 1
)

bit_0 = tones[0]
bit_1 = tones[1]
carrier = tones[1]


char_pause = 0.1  # pause time between chars, set to 0 for fastest rate possible

dac = audiopwmio.PWMAudioOut(
    board.A2
)  # the CLUE edge connector marked "#0" to STEMMA speaker
# The CLUE's on-board speaker works OK, not great, just crank amplitude to full before trying.
# dac = audiopwmio.PWMAudioOut(board.SPEAKER)


LTRS = (
    "\b",
    "E",
    "\n",
    "A",
    " ",
    "S",
    "I",
    "U",
    "\r",
    "D",
    "R",
    "J",
    "N",
    "F",
    "C",
    "K",
    "T",
    "Z",
    "L",
    "W",
    "H",
    "Y",
    "P",
    "Q",
    "O",
    "B",
    "G",
    "FIGS",
    "M",
    "X",
    "V",
    "LTRS",
)

FIGS = (
    "\b",
    "3",
    "\n",
    "-",
    " ",
    "-",
    "8",
    "7",
    "\r",
    "$",
    "4",
    "'",
    ",",
    "!",
    ":",
    "(",
    "5",
    '"',
    ")",
    "2",
    "=",
    "6",
    "0",
    "1",
    "9",
    "?",
    "+",
    "FIGS",
    ".",
    "/",
    ";",
    "LTRS",
)

char_count = 0
current_mode = LTRS

#  The 5-bit Baudot text telephone (TTY) mode is a Frequency Shift Keyed modem
#  for use on the Public Switched Telephone network.
#
#   Definitions:
#       Carrier tone is a 1400Hz tone.
#       Binary 0 is an 1800Hz tone.
#       Binary 1 is a 1400Hz tone.
#       Bit duration is 20ms.

#       Two modes exist: Letters, aka LTRS, for alphabet characters
#       and Figures aka FIGS for numbers and symbols. These modes are switched by
#       sending the appropriate 5-bit LTRS or FIGS character.
#
#   Character transmission sequence:
#       Carrier tone transmits for 150ms before each character.
#       Start bit is a binary 0 (sounded for one bit duration of 20ms).
#       5-bit character code can be a combination of binary 0s and binary 1s.
#       Stop bit is a binary 1 with a minimum duration of 1-1/2 bits (30ms)
#
#


def baudot_bit(pitch=bit_1, duration=0.022):  # spec says 20ms, but adjusted as needed
    dac.play(pitch, loop=True)
    time.sleep(duration)
    # dac.stop()


def baudot_carrier(duration=0.15):  # Carrier tone is transmitted for 150 ms before the
    # first character is transmitted
    baudot_bit(carrier, duration)
    dac.stop()


def baudot_start():
    baudot_bit(bit_0)


def baudot_stop():
    baudot_bit(bit_1, 0.04)  # minimum duration is 30ms
    dac.stop()


def send_character(value):
    baudot_carrier()  # send carrier tone
    baudot_start()  # send start bit tone
    for i in range(5):  # send each bit of the character
        bit = (value >> i) & 0x01  # bit shift and bit mask to get value of each bit
        baudot_bit(tones[bit])  # send each bit, either 0 or 1, of a character
    baudot_stop()  # send stop bit
    baudot_carrier()  # not to spec, but works better to extend carrier


def send_message(text):
    global char_count, current_mode  # pylint: disable=global-statement
    for char in text:
        if char not in LTRS and char not in FIGS:  # just skip unknown characters
            print("Unknown character:", char)
            continue

        if char not in current_mode:  # switch mode
            if current_mode == LTRS:
                print("Switching mode to FIGS")
                current_mode = FIGS
                send_character(current_mode.index("FIGS"))
            elif current_mode == FIGS:
                print("Switching mode to LTRS")
                current_mode = LTRS
                send_character(current_mode.index("LTRS"))
        # Send char mode at beginning of message and every 72 characters
        if char_count >= 72 or char_count == 0:
            print("Resending mode")
            if current_mode == LTRS:
                send_character(current_mode.index("LTRS"))
            elif current_mode == FIGS:
                send_character(current_mode.index("FIGS"))
            # reset counter
            char_count = 0
        print(char)
        send_character(current_mode.index(char))
        time.sleep(char_pause)
        # increment counter
        char_count += 1


while True:
    send_message("\nADAFRUIT 1234567890 -$!+='()/:;?,. ")
    time.sleep(2)
    send_message("\nWELCOME TO JOHN PARK'S WORKSHOP!")
    time.sleep(3)
    send_message("\nWOULD YOU LIKE TO PLAY A GAME?")
    time.sleep(5)

    # here's an example of sending a character
    # send_character(current_mode.index("A"))
    # time.sleep(char_pause)

 

‎View on GitHub

Here's how the code works:‎

Libraries

First, we'll import the necessary libraries, including the audiocore ‎RawSample and audiopwmio that allow us to create a play tones ‎over the analog output pin.‎

Download File

Copy Code
import time
import math
import array
import board
from audiocore import RawSample
import audiopwmio

 

Sine Waves

Next, we'll create some constants and code to generate a couple of ‎sine wave tables, one at 1400Hz and the other at 1800Hz.‎

Download File

Copy Code
SIN_LENGTH = 100  # more is less choppy
SIN_AMPLITUDE = 2 ** 12  # 0 (min) to 32768 (max)  8192 is nice
SIN_OFFSET = 32767.5  # for 16bit range, (2**16 - 1) / 2
DELTA_PI = 2 * math.pi / SIN_LENGTH  # happy little constant

sine_wave = [
    int(SIN_OFFSET + SIN_AMPLITUDE * math.sin(DELTA_PI * i)) for i in range(SIN_LENGTH)
]
tones = (
    RawSample(array.array("H", sine_wave), sample_rate=1800 * SIN_LENGTH),  # Bit 0
    RawSample(array.array("H", sine_wave), sample_rate=1400 * SIN_LENGTH),  # Bit 1
)

 

Lists

We'll create a pair of lists called LTRS and FIGS that contain the full ‎character sets we'll be able to send.‎

We'll also set the current_mode to LTRS for purposes of sending the ‎mode code and switching between the modes.‎

Baudot Functions

A series of functions are used to create the different uses of the sine ‎waves for carrier tone, binary 0 bit, binary 1 bit, start bit, and stop bit.‎

Download File

Copy Code
def baudot_bit(pitch=bit_1, duration=0.022):  # spec says 20ms, but adjusted as needed
    dac.play(pitch, loop=True)
    time.sleep(duration)
    # dac.stop()


def baudot_carrier(duration=0.15):  # Carrier tone is transmitted for 150 ms before the
    # first character is transmitted
    baudot_bit(carrier, duration)
    dac.stop()


def baudot_start():
    baudot_bit(bit_0)


def baudot_stop():
    baudot_bit(bit_1, 0.04)  # minimum duration is 30ms
    dac.stop()

 

Send Character

The send_character() function bundles up the parts into a proper TTY ‎compliant message including the carrier tone, start bit, 5-bit ‎character, stop bit, and carrier tone again. It receives a value ‎argument of a 5-bit binary code from the LTRS or FIGS list and ‎marches through this from LSB first, using bit shifting and bit ‎masking to grab each relevant bit and convert it to the proper tone.‎

Download File

Copy Code
def send_character(value):
    baudot_carrier()  # send carrier tone
    baudot_start()  # send start bit tone
    for i in range(5):  # send each bit of the character
        bit = (value >> i) & 0x01  # bit shift and bit mask to get value of each bit
        baudot_bit(tones[bit])  # send each bit, either 0 or 1, of a character
    baudot_stop()  # send stop bit
    baudot_carrier()  # not to spec, but works better to extend carrier

 

Send Message

The send_message() function is a convenience function for bundling up ‎a whole message string and then one at a time converting the ‎characters to proper send_character() commands.‎

This includes testing each character to see if it is a LTRS or FIGS list ‎item, and then sending the proper mode character if needed. It also ‎follows the spec and sends the relevant mode character after every ‎‎72 characters.‎

Download File

Copy Code
def send_message(text):
    global char_count, current_mode  # pylint: disable=global-statement
    for char in text:
        if char not in LTRS and char not in FIGS:  # just skip unknown characters
            print("Unknown character:", char)
            continue

        if char not in current_mode:  # switch mode
            if current_mode == LTRS:
                print("Switching mode to FIGS")
                current_mode = FIGS
                send_character(current_mode.index("FIGS"))
            elif current_mode == FIGS:
                print("Switching mode to LTRS")
                current_mode = LTRS
                send_character(current_mode.index("LTRS"))
        # Send char mode at beginning of message and every 72 characters
        if char_count >= 72 or char_count == 0:
            print("Resending mode")
            if current_mode == LTRS:
                send_character(current_mode.index("LTRS"))
            elif current_mode == FIGS:
                send_character(current_mode.index("FIGS"))
            # reset counter
            char_count = 0
        print(char)
        send_character(current_mode.index(char))
        time.sleep(char_pause)
        # increment counter
        char_count += 1

 

Main Loop

The main loop of the program sends whatever messages are ‎specified. In these demos the \n carriage return is used to add a ‎break between messages. There is also a commented sample of ‎sending a single character.‎

Download File

Copy Code
while True:
    send_message("\nADAFRUIT 1234567890 -$!+='()/:;?,. ")
    time.sleep(2)
    send_message("\nWELCOME TO JOHN PARK'S WORKSHOP!")
    time.sleep(3)
    send_message("\nWOULD YOU LIKE TO PLAY A GAME?")
    time.sleep(5)

    # here's an example of sending a character
    # send_character(current_mode.index("A"))
    # time.sleep(char_pause)

 

Code the BLE TTY Transmitter

 

 

After trying the simple example on the previous page, you can ‎switch to this code to try out Bluetooth LE functionality using the ‎Adafruit Bluefruit LE Connect app on your iOS or Android device.‎

See this guide to get the app installed and set up.‎

Installing Project Code

To use with CircuitPython, you need to first install a few libraries, into ‎the lib folder on your CIRCUITPY drive. Then you need to ‎update code.py with the example script.‎

Thankfully, we can do this in one go. In the example below, click ‎the Download Project Bundle button below to download the ‎necessary libraries and the code.py file in a zip file. Extract the ‎contents of the zip file, open the ‎directory Baudot_tty/baudot_tty_ble/ and then click on the ‎directory that matches the version of CircuitPython you're using and ‎copy the contents of that directory to your CIRCUITPY drive.‎

Your CIRCUITPY drive should now look similar to the following ‎image:‎

cir_22

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2020 John Park for Adafruit Industries
#
# SPDX-License-Identifier: MIT

### Baudot TTY Message Transmitter
### Bluefruit Connect UART mode to send messages to CLUE for audio
### tramsission to TTY machine.

### The 5-bit mode is defined in ANSI TIA/EIA-825 (2000)
### "A Frequency Shift Keyed Modem for use on the Public Switched Telephone Network"

import time
import math
import array
import board
import audiopwmio
from audiocore import RawSample
from adafruit_ble import BLERadio
from adafruit_ble.advertising.standard import ProvideServicesAdvertisement
from adafruit_ble.services.nordic import UARTService

# BLE radio setup
ble = BLERadio()
uart_server = UARTService()
advertisement = ProvideServicesAdvertisement(uart_server)
ble._adapter.name = "TTY_MACHINE"  # pylint: disable=protected-access

# constants for sine wave generation
SIN_LENGTH = 100  # more is less choppy
SIN_AMPLITUDE = 2 ** 12  # 0 (min) to 32768 (max)  8192 is nice
SIN_OFFSET = 32767.5  # for 16bit range, (2**16 - 1) / 2
DELTA_PI = 2 * math.pi / SIN_LENGTH  # happy little constant

sine_wave = [
    int(SIN_OFFSET + SIN_AMPLITUDE * math.sin(DELTA_PI * i)) for i in range(SIN_LENGTH)
]
tones = (
    RawSample(array.array("H", sine_wave), sample_rate=1800 * SIN_LENGTH),  # Bit 0
    RawSample(array.array("H", sine_wave), sample_rate=1400 * SIN_LENGTH),  # Bit 1
)

bit_0 = tones[0]
bit_1 = tones[1]
carrier = tones[1]


char_pause = 0.0  # pause time between chars, set to 0 for fastest rate possible

dac = audiopwmio.PWMAudioOut(
    board.A2
)  # the CLUE edge connector marked "#0" to STEMMA speaker
# The CLUE's on-board speaker works OK, not great, just crank amplitude to full before trying.
# dac = audiopwmio.PWMAudioOut(board.SPEAKER)


LTRS = (
    "\b",
    "E",
    "\n",
    "A",
    " ",
    "S",
    "I",
    "U",
    "\r",
    "D",
    "R",
    "J",
    "N",
    "F",
    "C",
    "K",
    "T",
    "Z",
    "L",
    "W",
    "H",
    "Y",
    "P",
    "Q",
    "O",
    "B",
    "G",
    "FIGS",
    "M",
    "X",
    "V",
    "LTRS",
)

FIGS = (
    "\b",
    "3",
    "\n",
    "-",
    " ",
    "-",
    "8",
    "7",
    "\r",
    "$",
    "4",
    "'",
    ",",
    "!",
    ":",
    "(",
    "5",
    '"',
    ")",
    "2",
    "=",
    "6",
    "0",
    "1",
    "9",
    "?",
    "+",
    "FIGS",
    ".",
    "/",
    ";",
    "LTRS",
)

char_count = 0
current_mode = LTRS

#  The 5-bit Baudot text telephone (TTY) mode is a Frequency Shift Keyed modem
#  for use on the Public Switched Telephone network.
#
#   Definitions:
#       Carrier tone is a 1400Hz tone.
#       Binary 0 is an 1800Hz tone.
#       Binary 1 is a 1400Hz tone.
#       Bit duration is 20ms.
#
#       Two modes exist: Letters, aka LTRS, for alphabet characters
#       and Figures aka FIGS for numbers and symbols. These modes are switched by
#       sending the appropriate 5-bit LTRS or FIGS character.
#
#   Character transmission sequence:
#       Carrier tone transmits for 150ms before each character.
#       Start bit is a binary 0 (sounded for one bit duration of 20ms).
#       5-bit character code can be a combination of binary 0s and binary 1s.
#       Stop bit is a binary 1 with a minimum duration of 1-1/2 bits (30ms)


def baudot_bit(pitch=bit_1, duration=0.022):  # spec says 20ms, but adjusted as needed
    dac.play(pitch, loop=True)
    time.sleep(duration)
    # dac.stop()


def baudot_carrier(duration=0.15):
    # Carrier is transmitted 150 ms before first character is sent
    baudot_bit(carrier, duration)
    dac.stop()


def baudot_start():
    baudot_bit(bit_0)


def baudot_stop():
    baudot_bit(bit_1, 0.04)  # minimum duration is 30ms
    dac.stop()


def send_character(value):
    baudot_carrier()  # send carrier tone
    baudot_start()  # send start bit tone
    for i in range(5):  # send each bit of the character
        bit = (value >> i) & 0x01  # bit shift and bit mask to get value of each bit
        baudot_bit(tones[bit])  # send each bit, either 0 or 1, of a character
    baudot_stop()  # send stop bit
    baudot_carrier()  # not to spec, but works better to extend carrier


def send_message(text):
    global char_count, current_mode  # pylint: disable=global-statement
    for char in text:
        if char not in LTRS and char not in FIGS:  # just skip unknown characters
            print("Unknown character:", char)
            continue

        if char not in current_mode:  # switch mode
            if current_mode == LTRS:
                print("Switching mode to FIGS")
                current_mode = FIGS
                send_character(current_mode.index("FIGS"))
            elif current_mode == FIGS:
                print("Switching mode to LTRS")
                current_mode = LTRS
                send_character(current_mode.index("LTRS"))
        # Send char mode at beginning of message and every 72 characters
        if char_count >= 72 or char_count == 0:
            print("Resending mode")
            if current_mode == LTRS:
                send_character(current_mode.index("LTRS"))
            elif current_mode == FIGS:
                send_character(current_mode.index("FIGS"))
            # reset counter
            char_count = 0
        print(char)
        send_character(current_mode.index(char))
        time.sleep(char_pause)
        # increment counter
        char_count += 1


while True:
    print("WAITING...")
    send_message("\nWAITING...\n")
    ble.start_advertising(advertisement)
    while not ble.connected:
        pass

    # Connected
    ble.stop_advertising()
    print("CONNECTED")
    send_message("\nCONNECTED\n")

    # Loop and read packets
    while ble.connected:
        if uart_server.in_waiting:
            raw_bytes = uart_server.read(uart_server.in_waiting)
            textmsg = raw_bytes.decode().strip()
            print("received text =", textmsg)
            send_message("\n")
            send_message(textmsg.upper())

    # Disconnected
    print("DISCONNECTED")
    send_message("\nDISCONNECTED\n")

 

View on GitHub

Once you've copied the code.py code file to your CLUE, you can ‎connect from the Bluefruit app to the CLUE device named TTY ‎Machine and then use the UART function to send messages to the ‎CLUE.‎

The letters will be received by the CLUE and then sent as audio to ‎the TTY machine!‎

Code the TTY GUI

 

 

This version of the code adds in a simple GUI for selecting a phrase ‎with the A button and sending it with the B button.‎

version_23

Installing Project Code

To use with CircuitPython, you need to first install a few libraries, into ‎the lib folder on your CIRCUITPY drive. Then you need to ‎update code.py with the example script.‎

Thankfully, we can do this in one go. In the example below, click ‎the Download Project Bundle button below to download the ‎necessary libraries and the code.py file in a zip file. Extract the ‎contents of the zip file, open the ‎directory Baudot_TTY/baudot_tty_gui/ and then click on the ‎directory that matches the version of CircuitPython you're using and ‎copy the contents of that directory to your CIRCUITPY drive.‎

Your CIRCUITPY drive should now look similar to the following ‎image:‎

circ_24

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2020 John Park for Adafruit Industries
#
# SPDX-License-Identifier: MIT

### Baudot TTY Message Transmitter with CLUE GUI
### Pick from four phrases to send from the CLUE screen with buttons

### The 5-bit mode is defined in ANSI TIA/EIA-825 (2000)
### "A Frequency Shift Keyed Modem for use on the Public Switched Telephone Network"

import time
import math
import array
import board
from audiocore import RawSample
import audiopwmio
import displayio
from adafruit_display_shapes.circle import Circle
from adafruit_clue import clue
from adafruit_display_text import label
import terminalio

# Enter your messages here no more than 34 characters including spaces per line
messages = [
    "HELLO FROM ADAFRUIT INDUSTRIES",
    "12345678910 -$!+='()/:;?",
    "WOULD YOU LIKE TO PLAY A GAME?",
    "WELCOME TO JOHN PARK'S WORKSHOP",
]


clue.display.brightness = 1.0
screen = displayio.Group()

VFD_GREEN = 0x00FFD2
VFD_BG = 0x000505

# setup screen
# BG
color_bitmap = displayio.Bitmap(240, 240, 1)
color_palette = displayio.Palette(1)
color_palette[0] = VFD_BG
bg_sprite = displayio.TileGrid(color_bitmap, x=0, y=0, pixel_shader=color_palette)
screen.append(bg_sprite)

# title
title_label = label.Label(
    terminalio.FONT, text="TTY CLUE", scale=4, color=VFD_GREEN
)
title_label.x = 20
title_label.y = 16
screen.append(title_label)

# footer
footer_label = label.Label(
    terminalio.FONT, text="<PICK         SEND>", scale=2, color=VFD_GREEN
)
footer_label.x = 4
footer_label.y = 220
screen.append(footer_label)

# message configs
messages_config = [
    (0, messages[0], VFD_GREEN, 2, 60),
    (1, messages[1], VFD_GREEN, 2, 90),
    (2, messages[2], VFD_GREEN, 2, 120),
    (3, messages[3], VFD_GREEN, 2, 150),
]

messages_labels = {}  # dictionary of configured messages_labels

message_group = displayio.Group(scale=1)

for message_config in messages_config:
    (name, textline, color, x, y) = message_config  # unpack tuple into five var names
    message_label = label.Label(terminalio.FONT, text=textline, color=color)
    message_label.x = x
    message_label.y = y
    messages_labels[name] = message_label
    message_group.append(message_label)
screen.append(message_group)

# selection dot
dot_y = [52, 82, 112, 142]
dot = Circle(220, 60, 8, outline=VFD_GREEN, fill=VFD_BG)
screen.append(dot)

clue.display.root_group = screen

# constants for sine wave generation
SIN_LENGTH = 100  # more is less choppy
SIN_AMPLITUDE = 2 ** 12  # 0 (min) to 32768 (max)  8192 is nice
SIN_OFFSET = 32767.5  # for 16bit range, (2**16 - 1) / 2
DELTA_PI = 2 * math.pi / SIN_LENGTH  # happy little constant

sine_wave = [
    int(SIN_OFFSET + SIN_AMPLITUDE * math.sin(DELTA_PI * i)) for i in range(SIN_LENGTH)
]
tones = (
    RawSample(array.array("H", sine_wave), sample_rate=1800 * SIN_LENGTH),  # Bit 0
    RawSample(array.array("H", sine_wave), sample_rate=1400 * SIN_LENGTH),  # Bit 1
)

bit_0 = tones[0]
bit_1 = tones[1]
carrier = tones[1]


char_pause = 0.1  # pause time between chars, set to 0 for fastest rate possible

dac = audiopwmio.PWMAudioOut(
    board.A2
)  # the CLUE edge connector marked "#0" to STEMMA speaker
# The CLUE's on-board speaker works OK, not great, just crank amplitude to full before trying.
# dac = audiopwmio.PWMAudioOut(board.SPEAKER)


LTRS = (
    "\b",
    "E",
    "\n",
    "A",
    " ",
    "S",
    "I",
    "U",
    "\r",
    "D",
    "R",
    "J",
    "N",
    "F",
    "C",
    "K",
    "T",
    "Z",
    "L",
    "W",
    "H",
    "Y",
    "P",
    "Q",
    "O",
    "B",
    "G",
    "FIGS",
    "M",
    "X",
    "V",
    "LTRS",
)

FIGS = (
    "\b",
    "3",
    "\n",
    "-",
    " ",
    "-",
    "8",
    "7",
    "\r",
    "$",
    "4",
    "'",
    ",",
    "!",
    ":",
    "(",
    "5",
    '"',
    ")",
    "2",
    "=",
    "6",
    "0",
    "1",
    "9",
    "?",
    "+",
    "FIGS",
    ".",
    "/",
    ";",
    "LTRS",
)

char_count = 0
current_mode = LTRS

#  The 5-bit Baudot text telephone (TTY) mode is a Frequency Shift Keyed modem
#  for use on the Public Switched Telephone network.
#
#   Definitions:
#       Carrier tone is a 1400Hz tone.
#       Binary 0 is an 1800Hz tone.
#       Binary 1 is a 1400Hz tone.
#       Bit duration is 20ms.

#       Two modes exist: Letters, aka LTRS, for alphabet characters
#       and Figures aka FIGS for numbers and symbols. These modes are switched by
#       sending the appropriate 5-bit LTRS or FIGS character.
#
#   Character transmission sequence:
#       Carrier tone transmits for 150ms before each character.
#       Start bit is a binary 0 (sounded for one bit duration of 20ms).
#       5-bit character code can be a combination of binary 0s and binary 1s.
#       Stop bit is a binary 1 with a minimum duration of 1-1/2 bits (30ms)
#
#


def baudot_bit(pitch=bit_1, duration=0.022):  # spec says 20ms, but adjusted as needed
    dac.play(pitch, loop=True)
    time.sleep(duration)
    # dac.stop()


def baudot_carrier(duration=0.15):  # Carrier tone is transmitted for 150 ms before the
    # first character is transmitted
    baudot_bit(carrier, duration)
    dac.stop()


def baudot_start():
    baudot_bit(bit_0)


def baudot_stop():
    baudot_bit(bit_1, 0.04)  # minimum duration is 30ms
    dac.stop()


def send_character(value):
    baudot_carrier()  # send carrier tone
    baudot_start()  # send start bit tone
    for i in range(5):  # send each bit of the character
        bit = (value >> i) & 0x01  # bit shift and bit mask to get value of each bit
        baudot_bit(tones[bit])  # send each bit, either 0 or 1, of a character
    baudot_stop()  # send stop bit
    baudot_carrier()  # not to spec, but works better to extend carrier


def send_message(text):
    global char_count, current_mode  # pylint: disable=global-statement
    for char in text:
        if char not in LTRS and char not in FIGS:  # just skip unknown characters
            print("Unknown character:", char)
            continue

        if char not in current_mode:  # switch mode
            if current_mode == LTRS:
                print("Switching mode to FIGS")
                current_mode = FIGS
                send_character(current_mode.index("FIGS"))
            elif current_mode == FIGS:
                print("Switching mode to LTRS")
                current_mode = LTRS
                send_character(current_mode.index("LTRS"))
        # Send char mode at beginning of message and every 72 characters
        if char_count >= 72 or char_count == 0:
            print("Resending mode")
            if current_mode == LTRS:
                send_character(current_mode.index("LTRS"))
            elif current_mode == FIGS:
                send_character(current_mode.index("FIGS"))
            # reset counter
            char_count = 0
        print(char)
        send_character(current_mode.index(char))
        time.sleep(char_pause)
        # increment counter
        char_count += 1


message_pick = 0

while True:
    if clue.button_a:
        message_pick = (message_pick + 1) % 4  # loop through the lines
        dot.y = dot_y[message_pick]
        time.sleep(0.4)  # debounce

    if clue.button_b:
        dot.fill = VFD_GREEN
        send_message(messages[message_pick])
        dot.fill = VFD_BG

View on GitHub

Número de parte del fabricante 4500
CLUE NRF52840 EXPRESS
Adafruit Industries LLC
$44.95
Ver más Details
Número de parte del fabricante 3885
STEMMA SPEAKER & AUDIO AMPLIFIER
Adafruit Industries LLC
Número de parte del fabricante 592
CABLE A PLUG TO MCR B PLUG 3'
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.