Maker.io main logo

Adafruit Bonsai Buckaroo

76

2024-04-12 | By Adafruit Industries

License: See Original Project micro:bit

Courtesy of Adafruit

Guide by Kattni Rembor

Overview

boards_1

We can’t wait for spring to arrive, and we’re looking forward to caring ‎for some plants! We designed this little add-on ‎for micro:bit or CLUE boards – bolt it on with 5 screws to get a ‎buzzer/beeper, motor driver, and breakouts for connecting a soil ‎sensor (two alligator clips + nails work just fine). Simple, but effective!

boards_2

  • 8mm Buzzer/Speaker on pin P0 - have your plant kit beep ‎when it wants watering, or have it sing a song when it’s nice ‎and happy.
  • ‎3V Motor control (on/off) on pin P2 - connect to a water pump ‎to automatically water dry plants
  • Alligator clip pads for pin P1, 3V and GND - connect to two ‎alligator clips and nails to measure soil resistance

boards_3

Works with micro:bit in Arduino, MicroPython or MakeCode. For ‎CLUE, you can use CircuitPython or Arduino.

plant_4

Pinouts

bonsai_5

The Bonsai Buckaroo is designed to add a speaker, motor terminal, ‎and pins for connecting a soil sensor to your micro:bit or CLUE board. ‎Let's take a look!‎

Along the top are the mount points. The Bonsai Buckaroo ships with ‎screws for attaching to your micro:bit or CLUE.‎

mount_6

On the left side is the speaker. Use it to have your plant kit beep ‎when it wants watering, or have it sing a song when it's nice and ‎happy.‎

speaker_7

On the right is the 3V Motor control (on/off) on pin P2. Connect to a ‎water pump to automatically water dry plants. The 3V connector ‎‎(typically the red wire) goes into the part of the controller terminal ‎towards the top, and the ground (typically the black wire) goes to the ‎part of the controller terminal towards the bottom (by the 3V MOTOR ‎label). However, for our pumps, it does not really matter which way ‎you put the wires in.

control_8

In the center are the Alligator clip pads for pin P1, 3V and GND. ‎Connect to two alligator clips and nails to measure soil resistance as ‎shown on the next pages.‎

clip_9

Watermelon

We'll tell you about it later.‎

water_10

CLUE and CircuitPython Usage

clue_11

It's easy to use the Adafruit Bonsai Buckaroo with CircuitPython. This ‎example uses the Adafruit CircuitPython CLUE library to display soil ‎moisture level and the status of the pump motor on the CLUE ‎display. Connect your Bonsai Buckaroo to your CLUE and connect ‎the motor and plant to the Bonsai Buckaroo, and you're on your way ‎to automatic plant care. Let's take a look!‎

Wiring up your Bonsai Buckaroo

For this project, you'll need a Bonsai Buckaroo, a CLUE, a water ‎pump, some tubing, alligator clips, and two nails (or something else ‎conductive will work too!). It's super simple to connect them up.‎

  • Mount the Bonsai Buckaroo to the CLUE using the included ‎mounting hardware.
  • Connect the red wire of the water pump to the top of the ‎motor controller terminal.
  • Connect the black wire of the water pump to the bottom of ‎the motor controller terminal.
  • Connect an alligator clip to the 3V pad on the Bonsai ‎Buckaroo.
  • Connect an alligator clip to the PIN#1 pad of the Bonsai ‎Buckaroo.
  • Connect the other end of the alligator clip wires to nails stuck ‎into the soil of your plant.
  • Connect the tubing to the water pump.
  • Place the other end of the tubing in the soil of the plant.

wiring_12

Wire the Pump Driver Terminal

The Bonsai Buckaroo terminal connectors are spring-loaded press-fit ‎connectors. Push down on one tab to separate the internal ‎connector a bit and then push in the wire. Release the pressure on ‎the tab and the terminal will grip the wire.‎

Repeat for the second terminal.‎

sensors_bonsaiwiring

The image at the top of the page shows the CLUE connected to a AA ‎battery pack. If you find that battery pack isn't lasting long enough ‎for your needs, consider using a larger battery, or using a USB cable ‎plugged into the wall to provide longer usage.‎

Installing CircuitPython Libraries

The Adafruit CircuitPython CLUE library requires a number of other ‎libraries to work. Please follow the instructions on the CLUE ‎CircuitPython Libraries page to ensure you have all the necessary ‎libraries installed.‎

Before continuing, ensure that your lib folder looks like the one in ‎the CLUE guide Libraries page!‎

Bonsai Buckaroo Plant Care ‎Helper

Save the following as code.py on your CIRCUITPY drive.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2020 Kattni Rembor for Adafruit Industries
#
# SPDX-License-Identifier: MIT

import time
import board
import digitalio
import analogio
from adafruit_clue import clue

# Turn off the NeoPixel
clue.pixel.fill(0)

# Motor setup
motor = digitalio.DigitalInOut(board.P2)
motor.direction = digitalio.Direction.OUTPUT

# Soil sense setup
analog = analogio.AnalogIn(board.P1)

def read_and_average(analog_in, times, wait):
analog_sum = 0
for _ in range(times):
analog_sum += analog_in.value
time.sleep(wait)
return analog_sum / times

clue_display = clue.simple_text_display(title=" CLUE Plant", title_scale=1, text_scale=3)
clue_display.show()

while True:
# Take 100 readings and average them
analog_value = read_and_average(analog, 100, 0.01)
# Calculate a percentage (analog_value ranges from 0 to 65535)
percentage = analog_value / 65535 * 100
# Display the percentage
clue_display[0].text = "Soil: {} %".format(int(percentage))
# Print the values to the serial console
print((analog_value, percentage))

if percentage < 50:
motor.value = True
clue_display[1].text = "Motor ON"
clue_display[1].color = (0, 255, 0)
time.sleep(0.5)

# always turn off quickly
motor.value = False
clue_display[1].text = "Motor OFF"
clue_display[1].color = (255, 0, 0)

View on GitHub

helper_14

Let's take a look at the code.‎

First, we import all the necessary libraries, and turn off the NeoPixel ‎on the back of the board.‎

Next, we set up the motor on Pin 2, and setup Pin 1 as an analog pin.‎

Then we have a helper function designed to read an analog pin, and ‎take a number of readings over a given period of time.‎

The last thing we do before the loop is set up to display text on the ‎CLUE display using the CLUE library, with the title "CLUE Plant".‎

Inside the loop, we first use the helper function to take 100 readings ‎and average them. Then we use that average to calculate a ‎percentage, and display that percentage. We also print the average ‎and percentage to the serial console.‎

If the percentage is less than 50, we turn on the motor and display ‎‎"Motor ON" in green, and then pause for 0.5 seconds.‎

Otherwise, we turn the motor off and display "Motor OFF" in red.‎

That's all there is to automated plant care using CircuitPython, the ‎Bonsai Buckaroo, and CLUE!‎

micro:bit and MakeCode Usage

micro_15

This example uses the Bonsai Buckaroo, the micro:bit, and Microsoft ‎MakeCode to create an automatic plant care system.‎

If you are new to Microsoft MakeCode, Adafruit has an excellent ‎getting started tutorial at https://learn.adafruit.com/makecode.‎

This project requires:‎

  • Bonsai Buckaroo
  • micro:bit
  • water pump
  • two alligator clips and two nails (or other conductive materials ‎work as well)‎

Wire up the parts the same way as the previous page, substituting ‎the micro:bit for the CLUE.‎

The following is a short program. It reads the value from Pin 1, plots a ‎graph on the micro:bit, and displays the soil moisture value when ‎pressing button A. If the moisture level drops below 50%, it turns on ‎the motor for 0.5 seconds, and then turns it off.‎

Open the Bonsai Buckaroo Plant Care program in MakeCode

Your MakeCode screen should have the following MakeCode ‎program loaded.‎

makecode_16

The program starts off with a little song. Then it begins checking the ‎analog reading on Pin 1, and plots a bar graph on the LED array of ‎the values. If you press button A, the LED array shows the actual ‎reading.‎

If the reading drops below 500 (50%), it plays a tone, turns on the ‎motor for 0.5 seconds, and turns it off. This repeats until the reading ‎rises above 500.‎

That's all there is to plant care with Bonsai Buckaroo, micro:bit and ‎MakeCode!‎

program_17

Downloads

Files

Schematic

schematic_18

Fab Print

fabprint_19

Número de parte del fabricante 4534
BONSAI BUCKAROO PLANT CARE HELPE
Adafruit Industries LLC
Número de parte del fabricante 4100
SMALL ALLIGATOR CLIP TEST LEAD (
Adafruit Industries LLC
Número de parte del fabricante 4500
CLUE NRF52840 EXPRESS
Adafruit Industries LLC
$44.95
Ver más Details
Número de parte del fabricante MICRO:BIT SINGLE
BBC MICRO-BIT V2 SBC BOARD ONLY
Micro:bit
$24.49
Ver más Details
Número de parte del fabricante 4546
SUBMERSIBLE 3VDC HORIZONTAL PUMP
Adafruit Industries LLC
Número de parte del fabricante 4547
SUBMERSIBLE 3VDC VERTICAL PUMP
Adafruit Industries LLC
Número de parte del fabricante 4545
TUBING PVC 6MM ID X 1 METER
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.