Maker.io main logo

Arduino-Powered Rat Diorama: Electronics and Taxidermy

89

2024-08-16 | By bekathwia

License: See Original Project Arduino

 

Electronics and Taxidermy! That’s what’s on the menu for this diorama project collaboration ‎between Emily Graslie and me. In this project, we will build a plywood diorama box and fill it with ‎cityscape features like a brick wall with a dryer vent and LED lighting. Oh, and rat taxidermy. ‎You’d be surprised how much overlap in tools there can be. Check out how many of the tools we ‎needed are carried by DigiKey!‎

‎[DK list https://www.digikey.com/en/mylists/list/7XKTVCR5D6 ]‎‎

becky-stern-emily-graslie-rat-diorama-build-24

becky-stern-emily-graslie-rat-diorama-build-26

Recycled Vape Steam Feature

For this project, I was squarely in charge of any electronic elements going into our diorama. We ‎brainstormed a steam feature, so I got to work on that first.‎

To turn an old disposable, vape into a mini fog machine, I hooked it up to an air pump using bits ‎of silicone tubing. These things are activated by negative air pressure from the user inhaling ‎through it, so the pump can do the same thing. ‎

I picked up some flavorless 0% nicotine e-juice and used it to refill the spent vapes I got from a ‎friend. I drilled out the mouthpiece to make the tubing fit and used silicone adhesive for an ‎airtight seal. ‎

Note that even though these things were “empty” - they still stunk. So, I wrote a simple Arduino ‎program to activate the pump for a few seconds every minute, simulating a human user, with the ‎exit tube out the window to flush out the stinky vape juice left in the sponge. ‎

I soldered wires onto the pump to make the connections more permanent. This setup was the ‎first thing I mounted to my control board - a piece of plywood I set upright in my vise with a plan ‎to install it inside the diorama later. I used bits of nylon strapping and some screws to secure the ‎pump to the wood.‎

The relative positioning of the vape device and the pump matters because of the condensation ‎that forms in the tube, and the vape works best upright, so I wanted to figure out a way to mount ‎it (and a few backups) just below the pump. I could have used more strapping, but I wanted to ‎make them easily removable for refilling, so I 3D printed a little holder and mounted it and a ‎power strip to the board as well.‎

I figured out that one of my vapes could operate while charging, so I kept it plugged in. Usually, ‎they can’t charge and run at the same time, and the others in this set certainly don’t.‎

 becky-stern-emily-graslie-rat-diorama-build-00

becky-stern-emily-graslie-rat-diorama-build-21

becky-stern-emily-graslie-rat-diorama-build-25

becky-stern-emily-graslie-rat-diorama-build-12

Making the Flashlight

I wanted to try to make my rat hold a tiny flashlight, so I modeled one in Tinkercad, my favorite ‎free 3D modeling software, and printed it out in grey PLA filament on my 3D printer. A single ‎‎5mm LED fits inside, and the wires come out of a hole in the handle.‎

The wires from the flashlight, the air pump transistor circuit, and the LED strip all converge on ‎the control board, where an Arduino Uno and solderless breadboard host all the connections. ‎

becky-stern-emily-graslie-rat-diorama-build-23

becky-stern-emily-graslie-rat-diorama-build-27

Control Board Refinement

Once everything was working, I made a new, more permanent circuit using a Solderful ‎breadboard. I made ID tags for each one with my label maker. ‎

In the days and weeks leading up to this build, I couldn’t help but start collecting some authentic ‎city trash for our diorama. I also shellacked some pizza crust in case we want to depict our ‎taxidermy rats having a snack.‎

becky-stern-emily-graslie-rat-diorama-build-19

Preparing Specimens

We loaded up the van with the in-progress parts and drove to Emily’s place in Chicago. There we ‎built the plywood box that will contain the diorama, then we spent the next day at the Peggy ‎Notebaert Nature Museum learning how to prepare the rat specimens for taxidermy. This was an ‎entirely new experience for me. Emily’s friend and fellow YouTuber Rob Scallon also joined us ‎at the museum, where Rob Kelsey taught us to skin and flesh out our rats. ‎

Go over to Emily’s channel to watch the full gory process.

becky-stern-emily-graslie-rat-diorama-build-15

becky-stern-emily-graslie-rat-diorama-build-29

becky-stern-emily-graslie-rat-diorama-build-30

becky-stern-emily-graslie-rat-diorama-build-03

becky-stern-emily-graslie-rat-diorama-build-04

becky-stern-emily-graslie-rat-diorama-build-05

Diorama - Faux Bricks

Our diorama centerpiece is the corner of a brick building, so I carved bricks from some foam ‎insulation and then textured them with a piece of aluminum foil, which is a trick I picked up from ‎Nerdforge. When I wanted to make a double-height block for the concrete footer, I used air-dry ‎clay to fill in the gaps. Emily painted the bricks. ‎

becky-stern-emily-graslie-rat-diorama-build-02

becky-stern-emily-graslie-rat-diorama-build-08

becky-stern-emily-graslie-rat-diorama-build-09

becky-stern-emily-graslie-rat-diorama-build-10

Diorama - Plywood Box

The plywood box needed to have an opening at the back for installing the electronics, and its ‎floor needed to be elevated from the bottom edge so that forms could be fixtured from the ‎underside– basically, you need to be able to get your hands under it. We used scrap plywood ‎and pocket holes to make our basic shape, then used a thinner piece of plywood to create a ‎curved backdrop that Emily would later paint.‎‎

becky-stern-emily-graslie-rat-diorama-build-31

becky-stern-emily-graslie-rat-diorama-build-32

becky-stern-emily-graslie-rat-diorama-build-33

becky-stern-emily-graslie-rat-diorama-build-11

Diorama - Installing the Electronics

The next morning, we installed the control board in the back corner of the box.‎

Then I cut a hole for the dryer vent cover, and we installed the brick wall into the diorama box. I ‎used a plastic sandwich bag to act as a funnel for the water vapor by taping the silicone tube into ‎one corner. The bag is squished in the space between the vent and the foam. I think it came out ‎great.‎

I also added pixel strips to the upper edge to simulate city lighting.‎

becky-stern-emily-graslie-rat-diorama-build-13

becky-stern-emily-graslie-rat-diorama-build-14

becky-stern-emily-graslie-rat-diorama-build-20

becky-stern-emily-graslie-rat-diorama-build-17

becky-stern-emily-graslie-rat-diorama-build-18

3D Scanning and Printing of the Heads‎

We used an app called Polycam to 3D scan our rats’ heads so we could then 3D print them for ‎use inside the taxidermy. We heard that sculpting the face is one of the more challenging parts ‎of mammal taxidermy so hopefully, this would give us a leg up. ‎

The process involved putting the heads on wires so that I could move my phone all around it to ‎capture images for the photogrammetry. ‎

I left Chicago with a rat skin and a bunch of files.‎

becky-stern-emily-graslie-rat-diorama-build-34

becky-stern-emily-graslie-rat-diorama-build-35

becky-stern-emily-graslie-rat-diorama-build-36

becky-stern-emily-graslie-rat-diorama-build-37

becky-stern-emily-graslie-rat-diorama-build-38

becky-stern-emily-graslie-rat-diorama-build-39

Making and Revising the Taxidermy Form

To contrast the technology, we used for the head, I made the rest of my form the old-fashioned ‎way, using some stiff wire wrapped in slightly dampened wood wool, held in place with strong ‎thread. ‎

This is where the tracings and reference photos of the carcass would be useful, but I didn’t have ‎those for this particular skin which was prepared ahead of time so we could “cooking-show” ‎everything during the limited time of my visit.‎

Taxidermy, like many other skills, takes practice to get good at, so please be gentle with your ‎feedback as this is my first time. We’re following Allis Markham’s tutorials - she’s a super expert ‎who makes pieces for museums. I highly recommend taking one of her classes and appreciate ‎her sharing resources with us to get started with this fun and strange hobby.‎

becky-stern-emily-graslie-rat-diorama-build-16

Wiring Form for Flashlight

becky-stern-emily-graslie-rat-diorama-build-40

While building, I discovered that the flashlight I wanted my rat to hold couldn’t be assembled ‎already before wiring up the form. We want the hole for the flashlight wires to be as small as ‎possible, so I added the wires to the form first. ‎

To see the final diorama, subscribe to Emily’s channel so you’ll be notified when it comes out!

Download Code

 

Número de parte del fabricante K6PICF.ITU
ESD 6-PC KIT TWEEZERS,CARBON FIB
Ideal-tek S.A.
$37.77
Ver más Details
Número de parte del fabricante K4MPTSS
4-PC SPATULA STAINLESS STEEL KIT
Ideal-tek S.A.
$18.56
Ver más Details
Número de parte del fabricante M50TASSM
SYRINGE MANUAL 50CC 5PC
Apex Tool Group
$19.50
Ver más Details
Número de parte del fabricante M10LLASSM
SYRINGE MANUAL 10CC 15PC
Apex Tool Group
$14.10
Ver más Details
Número de parte del fabricante 80131
DIAMOND HANDFILE FLX 1.5" 1=1SET
3M
$54.91
Ver más Details
Número de parte del fabricante 10310
PLIERS ELEC BENT NOSE 4.5"
Aven Tools
$22.09
Ver más Details
Número de parte del fabricante 10313
PLIERS ELEC BENT NOSE 6"
Aven Tools
$22.09
Ver más Details
Número de parte del fabricante 18475USA
TWEEZER ASSORT AA OO OOD 3C 5 7
Aven Tools
$42.43
Ver más Details
Número de parte del fabricante ST14-075-60BK
TAPE ELECTRICAL BLACK 3/4"X20YDS
Panduit Corp
Número de parte del fabricante 4026-3/4"X3/4"
TAPE DBL SIDED NATURAL 3/4"X3/4"
3M
Número de parte del fabricante 101+ 24MM
TAPE MASKING TAN 15/16"X60YDS
3M
Número de parte del fabricante 313080343
AC/DC DSKTP ADPT 4.75V-5.25V 21W
Seeed Technology Co., Ltd
Número de parte del fabricante DKS-SOLDERBREAD-02
BREADBOARD GENERAL PURPOSE PTH
DigiKey Standard
Número de parte del fabricante TLP206USB
2-OUTLET SURGE PROTECTOR WITH 2
Eaton Tripp Lite
$26.51
Ver más Details
Número de parte del fabricante 4700
AIR PUMP AND VACUUM DC MOTOR - 4
Adafruit Industries LLC
Número de parte del fabricante NCS10C-20G
NEUTRAL CURE SILICONE ADHESIVE S
Chip Quik Inc.
Número de parte del fabricante 4661
SILICONE TUBING FOR AIR PUMPS AN
Adafruit Industries LLC
Número de parte del fabricante 615
NEEDLE SET SIZE 3-9 20PC
Adafruit Industries LLC
Número de parte del fabricante A000073
ARDUINO UNO SMD R3 ATMEGA328
Arduino
$26.30
Ver más Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.