Artículos y blogs

Image of Dielectric Elastomer Switches: Building Logic Gates with Soft Membranes Dielectric Elastomer Switches: Building Logic Gates with Soft Membranes

When you think of "electronics," you probably picture rigid green circuit boards, silicon chips, and soldering irons. But what if you could build a circuit entirely out of soft, stretchy rubber?

Image of How to Establish a Secure Hardware Foundation for Long-Term CRA Compliance How to Establish a Secure Hardware Foundation for Long-Term CRA Compliance Fecha de publicación: 2026-04-08

Learn how to use the NXP EdgeLock secure enclave to establish a secure hardware foundation for long-term CRA compliance.

Image of Understanding the Difference Between Latching and Non-Latching Relays Understanding the Difference Between Latching and Non-Latching Relays Fecha de publicación: 2026-04-07

Relays are a foundational component in electronic systems, enabling reliable control of circuits across industrial, commercial, and consumer applications.

Image of Connector Testing and Its Importance to User Safety and End Use Connector Testing and Its Importance to User Safety and End Use

Connector testing, performed by accredited test facilities, is an important phase in ensuring electrical connector safety.

Image of Docker Part 1: Fixing “It Works on My Machine” Docker Part 1: Fixing “It Works on My Machine"

In this post, I want to explain what Docker is, why it helps with these problems, and give a practical understanding of how it fits into development workflows.

Image of Humanoids – What Does the Future Look Like? Humanoids – What Does the Future Look Like?

The pace of innovation is accelerating rapidly, driven by advances in AI, robotics, and computing power, with the possibilities expanding beyond simple tasks.

Image of DC/DC Converters for AI Data Centers: Tackling Space and Thermal Challenges DC/DC Converters for AI Data Centers: Tackling Space and Thermal Challenges

AI data center GPUs are pushing beyond 1 kW per device resulting in rack power densities in the megawatt scale, stressing cooling schemes past comfort zones.

Image of Webinar – Meet the LAN Squad: Defeating Ethernet Design Challenges Seminario web: Conozca al equipo LAN: Superar los retos del diseño Ethernet

Descubra cómo las soluciones de Würth Elektronik ofrecen ventajas personalizadas para LAN que mejoran la resistencia, simplifican las decisiones de distribución y reducen el costo total del sistema.

Image of Measuring the Speed of Sound Using an Ultrasonic Sensor and Oscilloscope Measuring the Speed of Sound Using an Ultrasonic Sensor and Oscilloscope

In this blog, I will walk through a simple experiment that uses an ultrasonic sensor and oscilloscope to measure how fast sound travels through the air.

Image of Select the Right Connectors to Meet Stringent Mil/Aero Electrical and Mechanical Requirements Seleccione los conectores adecuados para cumplir los estrictos requisitos eléctricos y mecánicos Mil/Aero Fecha de publicación: 2026-04-01

Los conectores para el sector aeroespacial y de defensa integran materiales sofisticados, diseño de contactos y cuerpos, fabricación y evaluación para cumplir los objetivos exigidos.

Image of Single-Chip Systems, MCUs for Matter-Enabled Smart Home Devices Fill Multiple Mesh Network Roles Los sistemas de un solo chip y las MCU para dispositivos domésticos inteligentes habilitados para la materia cumplen múltiples funciones de red en malla Fecha de publicación: 2026-03-31

Los componentes de bajo consumo y baja latencia de NXP son compatibles con las redes domésticas inteligentes habilitadas para Matter, mientras que las herramientas de desarrollo ayudan a los diseñadores a crear nuevos prototipos.

Image of Power Distribution Boards: Smart Alternative to Relays Power Distribution Boards: Smart Alternative to Relays

This blog will talk about the core concepts and the theory behind the circuit schematic and how it was approached.

Image of Harnessing AI at the Edge with iWave’s Agilex™ 5 System on Module Aprovechar la IA en el borde con el sistema en el módulo Agilex™ 5 de iWave

A medida que el procesamiento de datos se acerca cada vez más al borde, se necesitan plataformas que ofrezcan un rendimiento eficiente de IA con baja latencia y alta personalización.

Image of Webinar – Seven Reasons to Move from 12 V to 48 V Today Seminario web: Siete razones para pasar de 12 V a 48 V hoy

Una discusión sobre por qué 48 V se está convirtiendo en la red dominante de suministro de energía y cómo las soluciones modulares pueden acelerar y simplificar la transición.

Image of Simplifying Frequency Stability for High-Speed 5G and Data Converter Designs Simplificación de la estabilidad de frecuencia para diseños de convertidores de datos y 5G de alta velocidad Fecha de publicación: 2026-03-25

Descubra cómo los PLL ADF4382 de ADI con VCO integrados mejoran la estabilidad de frecuencia y la velocidad para convertidores de datos de alta velocidad y diseños de radio 5G.

Image of Building Quantum-Resilient Embedded Systems with iWave’s Agilex™ 5 System on Module Construcción de sistemas integrados cuánticamente resilientes con el sistema Agilex™ 5 de iWave en un módulo

iWave Global se ha asociado con Xiphera para ofrecer capacidad criptográfica cuántica segura en el sistema Agilex™ 5 System on Module (SoM) de iWave impulsado por Altera.

Image of How to Select Cables for Reliable VFD Motor Control and Sensor Feedback Cómo seleccionar los cables para un control fiable del motor VFD y la retroalimentación del sensor Fecha de publicación: 2026-03-24

El aumento de la automatización industrial y la búsqueda de una mayor eficiencia energética están acelerando la adopción de los variadores de frecuencia en los sistemas accionados por motor.

Image of Solder Smarter Using DigiKey Standard Helping Hands Solder Smarter Using DigiKey Standard Helping Hands

Explore DigiKey Helping Hands features including magnetic PCB pillars, flexible arms, LED magnifier, and a heavy steel base for stable soldering.

Image of Automotive Ethernet: The Backbone of Modern In-Vehicle Communication Ethernet automotriz: la columna vertebral de la comunicación moderna a bordo del vehículo

A medida que los vehículos se vuelven cada vez más autónomos y centrados en datos, la necesidad de una columna vertebral de comunicación a bordo de alta velocidad, escalable y fiable es mayor que nunca.

Image of Webinar – Select the Right Cables for Harsh Industrial Automation Applications Seminario web: Seleccione los cables adecuados para aplicaciones de automatización industrial exigente

Este seminario web en profundidad explica lo que se necesita para seleccionar el cable y cable adecuado para entornos industriales.