Typically, address pins are only used on I²C devices to allow multiple devices with the same base slave address to be on the same bus. The SPI devices also have address pins to allow multiple devices on the same bus while using one chip select.
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
Typically, address pins are only used on I²C devices to allow multiple devices with the same base slave address to be on the same bus. The SPI devices also have address pins to allow multiple devices on the same bus while using one chip select.