Maker.io main logo

How to Select Cables and Connectors for Your Application

348

2019-10-21 | By Maker.io Staff

While there are many connectors available to choose from, finding the right one for your project can be a challenge. For your convenience, here is a link to our picture Connector Selector. To start with, we’ll discuss some of the idiosyncrasies and issues associated with using cables, jumper wires, and connectors.

Noise

Noise can be a problem for cables, especially when high frequency signals travel long distances. Even short jumper wires used to read analog voltages from sensors may be prone to picking up EMR (Electromagnetic Radiation) from other circuits generating EMI (Electromagnetic Interference) and wires carrying digital signals, with a potential to interfere with the analog voltages coming from a sensor. In this case, using shielded cables or shielding products may help eliminate those disruptions.

Messy Wires

Using three or four jumper wires may be perfectly acceptable for connecting an Arduino to a serial EEPROM chip, however using 24 wires to control a parallel EEPROM can be difficult to troubleshoot the path and signal unless each colored wire and pin numbers are defined.

Repeatability

Many Jumper wires used in a project can be made permanent by soldering to its PC board. However, most projects that use jumper wires are removable and if used many times can become bent or broken. Always have multiple sets of jumper wires available when prototyping. Prototyping often involves connecting and disconnecting modules while testing, so integrating a connector between them makes it very convenient.

How to Select Cables and Connectors for Your Application

Bridging the gap between modules with connectors can be a convenient way to eliminate jumper wires. See these Male headers for PC mount and Female sockets to mate with the headers. Also, see this article to learn more about connecting boards together.

The Versatility of Connectors

Depending on your requirements, you may need to pick a connector that provides more standardized interfacing and or requires many mating cycles. If your concern is related to noise-sensitive signals, get a connector that is shielded (I.E., USB, D-SUB 9); if you are dealing with too many individual wires that don’t need to be shielded from noise, consider using our ribbon cables;

Here are some popular connector types and application uses.

Below are the links to the list of parts in the chart and their part family links for your further review to choose a connector for your next project:

How to Select Cables and Connectors for Your Application

USB-A

  • ED2989-ND
  • Standard USB connection
  • Used with many Type-A Male USB cables typically connect to PCs, Printers and other computer equipment

How to Select Cables and Connectors for Your Application

USB-C

  • WM12856CT-ND
  • New USB shape trending to help eliminate frustrating one-way insertion
  • For connecting data transfer between devices, charging and powering boards

USB Micro-B PCB Receptacle Surface Mount

  • 609-4616-1-ND
  • Low Profile Micro-B USB with PCB mounting tabs
  • For connecting data transfer between devices, charging and powering boards

How to Select Cables and Connectors for Your Application

USB-B

  • ED2983-ND
  • Low Profile PCB Solder with mounting tabs
  • Used for connecting data and power from mostly older devices and products

How to Select Cables and Connectors for Your Application

9 Pin D-Sub Connector

  • AE10972-ND
  • The old RS232 type connector typically used in the old days
  • General connector for connecting peripherals. 15 pin High Density versions of this D-Sub shape were used to connect PCs to monitors - termed VGA connector

How to Select Cables and Connectors for Your Application

IDC Ribbon Cable Socket Connector with Strain Relief

  • 732-5447-ND
  • Using 28AWG ribbon cable and this connector, you'll need a press to crush the wire into the V shaped contents for proper connection. This one comes with a strain relief to eliminate tearing the ribbon cable when moving it off a dual row pc mounted header
  • Connecting signals from one board to another; like inside a PC from one hard drive to its motherboard. Raspberry Pi's can use a 40-pin version of this to get the I/O for connecting to sensors and other devices to the outside world

How to Select Cables and Connectors for Your Application

Barrel Audio Connectors PC Mount

  • SC1464-ND
  • Usually soldered to a board and mounted inside a box or to a panel and using the circular nut to secure it in place
  • Used to help provide stereo output to headphones which typically have 3.5mm plugs

How to Select Cables and Connectors for Your Application

8-8 Modular Jack PC Mount

  • WM5466-ND
  • PC Leads and Mounting posts
  • Older devices that use 8-bit data bus protocol were conveniently connected with 8-8 modular cables - although larger in size, these jacks and plugs can still be used to transfer signals in your project design. The connect and release work really well together

How to Select Cables and Connectors for Your Application

4 Position Rectangular Housing Connector

  • WM13985-ND
  • Easy and reliable connection with a flexible remove tab on top for quick release
  • These power connectors can take a lot of current and work well when you need to connect and disconnect powering your device

Additional Resources includes a great article discussing the basics of connectors here.

Número de parte del fabricante USB-A1HSW6
CONN RCPT TYPEA 4POS R/A
On Shore Technology Inc.
Número de parte del fabricante 1054500101
CONN RCP USB3.1 TYPEC 24P SMD RA
Molex
Número de parte del fabricante 10118193-0001LF
CONN RCPT USB2.0 MICRO B SMD R/A
Amphenol ICC (FCI)
Número de parte del fabricante USB-B1HSB6
CONN RCPT TYPEB 4POS R/A
On Shore Technology Inc.
Número de parte del fabricante A-DS 09 LL/Z
CONN D-SUB PLUG 9POS SOLDER CUP
Assmann WSW Components
Número de parte del fabricante 61203423021
CONN RCPT 34POS IDC 28AWG GOLD
Würth Elektronik
Número de parte del fabricante 35RAPC4BH3
CONN JACK STEREO 3.5MM R/A
Switchcraft Inc.
Número de parte del fabricante 0436450408
CONN RCPT HSG 4POS 3.00MM
Molex
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.