Maker.io main logo

Starry Mood Light Enclosure for Kitronik Round USB LED Lamps

2022-10-13 | By Kitronik Maker

License: See Original Project

Courtesy of Kitronik

Guide By Kitronik Maker

Emma has designed these fantastic starry custom enclosures for our Kitronik ‎Round RGB USB LED Board and Kitronik Round White USB LED Board. All of the ‎files needed are available as a free download, for you to use or customise.‎

These enclosures will look great anywhere, on a desk, bedside table, or wherever ‎you need some light. You will find a list of the things we used below, but you can ‎substitute the materials for ones you have to hand. A good alternative is our value ‎acrylic range, it'll get you where you need to go for less.‎

We Used:‎

Starry Mood Light Enclosure:‎

files_1

Grab the DXF files and either head straight to the laser cutter or load the files into ‎your favourite CAD program. There are two files; the first contains the parts for the ‎base and lid for both of the board options, and the other contains the designs for ‎the polypropylene surrounds, which fit both lamps.‎‎ ‎

Step 1: To the Laser Cutter:‎

cutter_2

Cut out the DXF as above, either the White or RGB version depending on the board. ‎The solid areas of the above image are the parts you will want to keep. The round ‎parts should be made from Acrylic or Perspex, and the flat sheets from ‎polypropylene. The patterned polypropylene should be opaque (preferably black) ‎and the plain piece can either be white frosted or colour tinted polypropylene, both ‎of 0.5mm. We suggest coloured polypropylene for the white lamp, and the plain ‎frosted for the RGB lamp. ‎‎ ‎

Step 2: Assembling the Base and Lid:‎

assemble_3

Assemble your base and lid. The base will be glued around the board, with the ‎noodle cable already attached. Make sure the gap between the outer and inner ‎discs is even all the way around.‎‎ ‎

Step 3: Putting it All Together:‎

putting_4

Finally pop the polypropylene into the base as shown, then fit the top on! You may ‎need to either secure the polypropylene in shape using a little electrical tape as we ‎have or form it to shape using a heat gun. We did both, just to be sure!‎‎ ‎

One of the best sources of new Kitronik information is our Newsletter. To make ‎sure you always know what's going on, sign up for our newsletter here! The next ‎one's a good one, don't miss it!

‎‎©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof ‎without Kitronik's prior written consent.‎

Número de parte del fabricante 35158
LED ENG RGB ROUND
Kitronik Ltd.
Número de parte del fabricante 35157
LED ENG COOL WHT 6500K
Kitronik Ltd.
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.