Maker.io main logo

Qwiic Dynamic NFC/RFID Tag Hookup Guide

110

2023-09-05 | By SparkFun Electronics

License: See Original Project RFID / NFC

Courtesy of SparkFun

Guide by EL DUDERINO

Introduction

The SparkFun Qwiic Dynamic NFC/RFID Tag features the ST25DV64KC dynamic Near Frequency ‎Communication (NFC) / Radio Frequency Identification (RFID) tag IC from STMicroelectronics©. The ‎ST25DV64KC offers 64-kBit (8-kBytes) of EEPROM memory which can be accessed over both I2C and RF (NFC)! ‎It's a state-of-the-art tag which conforms to ISO/IEC 15693 or NFC Forum Type 5 recommendations. You can ‎read and write the tag's memory using NFC even while the tag is powered down or disconnected!‎

SparkFun Qwiic Dynamic NFC/RFID Tag

In this guide we'll go into some detail on the ST25DV64KC IC and other hardware on this Qwiic breakout, how ‎to assemble it into a Qwiic circuit and then install the SparkFun ST25DV64KC Arduino Library.‎

Required Materials

To follow along with this guide, you will need a microcontroller to communicate with the Qwiic Dynamic ‎NFC/RFID Tag. Below are a few options that come Qwiic-enabled out of the box:‎

If your chosen microcontroller is not already Qwiic-enabled, you can add that functionality with one or more of ‎the following items:‎

You will also need at least one Qwiic cable to connect your sensor to your microcontroller.‎

Optional Materials

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview.‎

qwiic_1

We also recommend taking a look at the following tutorials if you aren't familiar with the concepts covered in ‎them. If you are using one of the Qwiic Shields listed above, you may want to read through their respective ‎Hookup Guides as well before you get started with the Qwiic Dynamic NFC/RFID Tag.‎

Hardware Overview

Let's take a closer look at the ST25DV64KC and other hardware present on the Qwiic Dynamic NFC/RFID Tag.‎

ST25DV64KC Dynamic NFC/RFID Tag

The ST25DV64KC from STMicroelectronics is a unique tag IC that communicates over both I2C and RF (NFC). It ‎conforms to ISO/IEC 15693 (13.56 MHz frequency) and NFC Forum Type 5 recommendations.‎

tag_2

The ST25DV64KC includes 64 Kbit EEPROM for users to write and read data from, a general-purpose output to ‎act as an external interrupt reporting events such as RF field changes, RF activity, I2C writes and RF switch ‎toggling over I2C. The IC has a supply voltage range of 1.8V to 5.5V though when in a Qwiic circuit it runs ‎at 3.3V. It also includes an energy harvesting pin capable of outputting µW of power with an RF field of ‎sufficient strength. For a complete overview of the ST25DV64KC, refer to the datasheet.‎

The ST25DV64KC supports a fast transfer mode to send the contents of a 256-byte buffer between a device ‎connected to the tag over I2C (referred to as the tag's Mailbox) and an RF device such as a reader or ‎smartphone. This makes it so you can store data on the tag and have it available for reading by an RF device by ‎simply bringing it into the RF read range, even if the tag is powered off. This data can also be password ‎protected with a 64-bit value.‎

Power and Communication Interfaces

The Qwiic Dynamic NFC/RFID Tag has two interfaces for powering and communicating with the ST25DV64KC: ‎a pair of Qwiic connectors and a plated through hole (PTH) header.‎

Qwiic Connector

The board has a pair of Qwiic connectors to integrate it into a Qwiic ecosystem.‎

board_3

The Qwiic connectors route the SDA/SCL connections as well as 3.3V and Ground to power the board and ‎communicate with the ST25DV64KC over I2C.‎

Plated Through Hole Header

The board has a 0.1"-spaced PTH header that breaks out the power pins (3.3V and Ground), I2C interface ‎‎(SDA/SCL), energy harvesting pin (VEH), and general-purpose output pin (GPO).‎

plated_4

The Energy Harvesting Pin outputs an analog voltage when energy harvesting mode is enabled and in the ‎presence of a strong enough RF field. Refer to section 5.5 of the datasheet for specifics on using this pin. The ‎General-Purpose Output is an open-drain configurable pin used for interrupt events.‎

Antenna

The board includes a PCB antenna for the ST25DV64KC to help boost the read range a bit. In our testing with a ‎smart phone running an NFC reader app we found it had a range of a few centimeters.‎

antenna_5

LED

The sole LED on this board is a power status LED.‎

led_6

Solder Jumpers

The board has three solder jumpers labeled LED, GPO, and I2C. The table below outlines their labels, default ‎state, functionality, and any notes regarding their use.‎

jumpers_7

table_8

Board Dimensions

The Qwiic Dynamic NFC/RFID Tag matches the standard Qwiic breakout size of 1" x 1" (25.4mm x 25.4mm) ‎and has two mounting holes that fit a 4-40 screw.‎

dimensions_9

Hardware Assembly

Now that we're familiar with the hardware on the Qwiic Dynamic NFC/RFID Tag, it's time to assemble it into a ‎Qwiic circuit.‎

Basic Assembly

The Qwiic ecosystem makes building a circuit with the Qwiic Dynamic NFC/RFID Tag simple. Just use a Qwiic ‎cable to connect the breakout to your development board like the image shown below:‎

assembly_10

As a reminder, the Qwiic connectors only include the power pins and I2C lines so if you wish to use the Energy ‎Harvesting pin or the General Purpose pin you'll need to solder to them or use something like these IC ‎Hooks for a temporary prototyping connection.‎

Soldered Assembly

Users who prefer a traditional soldered connection should solder headers or wires to the Qwiic Dynamic ‎NFC/RFID Tag and then make the appropriate connections to your development board. If you've never ‎soldered before or would like some tips, check out our How to Solder Tutorial.‎

SparkFun ST25DV64KC Arduino Library

Note: This library assumes you are using the latest version of the Arduino IDE on your desktop. If this is your ‎first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously ‎installed an Arduino library, please check out our installation guide.‎

The SparkFun ST25DV64KC Arduino Library provides an exhaustive collection of examples to take full ‎advantage of the Qwiic Dynamic NFC/RFID Tag including reading and writing the user memory, controlling the ‎read/write permissions, altering the read area sizes, and applying password control. On top of this the library ‎includes examples showing how to use NDEF (NFC Forum Data Exchange Format) URI, WiFi, and Text records ‎you can read with a smart phone. You'll need a compatible app on your phone like ST's "NFC Tap" App available ‎on the Apple© App store or Google© Play.‎

Install the library into Arduino by searching for "SparkFun ST25DV64KX Arduino Library" in the Arduino Library ‎Manager. Users who prefer to install the library manually can download it by clicking the button below:‎

SPARKFUN ST25DV64KC ARDUINO LIBRARY (ZIP)‎

Arduino Library Documentation

We have an in-depth guide for the library covering all examples as well as the complete API reference you can ‎read through here:‎

SPARKFUN ST25DV64KC ARDUINO LIBRARY - DOCUMENTATION

Troubleshooting

General Troubleshooting

Not working as expected and need help? ‎

If you need technical assistance and more information on a product that is not working as you expected, we ‎recommend heading on over to the SparkFun Technical Assistance page for some initial troubleshooting.

SPARKFUN TECHNICAL ASSISTANCE PAGE

If you don't find what you need there, the SparkFun Forums are a great place to find and ask for help. If this is ‎your first visit, you'll need to create a Forum Account to search product forums and post questions.

CREATE NEW FORUM ACCOUNT     LOG INTO SPARKFUN FORUMS

Resources and Going Further

That's all for this guide. For more information about the Qwiic Dynamic NFC/RFID Tag, check out the resources ‎below:‎

Número de parte del fabricante 21274
SPARKFUN QWIIC DYNAMIC NFC/RFID
SparkFun Electronics
$11.95
Ver más Details
Número de parte del fabricante 15663
SPARKFUN THING PLUS ESP32 WROOM
SparkFun Electronics
$24.95
Ver más Details
Número de parte del fabricante 18158
SPARKFUN REDBOARD PLUS
SparkFun Electronics
$29.56
Ver más Details
Número de parte del fabricante 15574
SPARKFUN THING PLUS - ARTEMIS
SparkFun Electronics
$22.50
Ver más Details
Número de parte del fabricante 15444
REDBOARD ARTEMIS
SparkFun Electronics
$24.95
Ver más Details
Número de parte del fabricante 15081
QWIIC CABLE KIT
SparkFun Electronics
$12.95
Ver más Details
Número de parte del fabricante 14495
QWIIC ADAPTER
SparkFun Electronics
Número de parte del fabricante 14352
QWIIC SHIELD FOR ARDUINO
SparkFun Electronics
Número de parte del fabricante 16790
QWIIC SHIELD FOR THING PLUS
SparkFun Electronics
Número de parte del fabricante 14427
QWIIC CABLE - 100MM
SparkFun Electronics
More Info
Ver más Details
Número de parte del fabricante 14429
QWIIC CABLE - 500MM
SparkFun Electronics
Número de parte del fabricante 14426
QWIIC CABLE - 50MM
SparkFun Electronics
More Info
Ver más Details
Número de parte del fabricante 14428
QWIIC CABLE - 200MM
SparkFun Electronics
Número de parte del fabricante 09741
TEST LEAD HOOK TO TIP PLUG 2.5"
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.