Maker.io main logo

Mini Neon Sign Prop & n00ds Booster Case

156

2025-09-16 | By Adafruit Industries

License: See Original Project 3D Printing Batteries LED Strips

Courtesy of Adafruit

Guide by Ruiz Brothers

Overview

Print a case for the Adafruit TPS61169 Constant Current Boost Converter for LEDs!

The case has cutouts for the terminal blocks to attach LED nOOds, and cutouts for the current adjustment switches -- useful when powering multiple strips.

Tabs on the sides make it easy to mount to any prop, such as a sign or wearable.

The case snap fits together without the need for any additional hardware to mount the board inside the case.

case_1

case_2

case_3

Parts

Circuit Diagram

The diagram provides a general visual reference for wiring of the components once you get to the Assembly page. This diagram was created using the software package Fritzing.

Adafruit Library for Fritzing

Adafruit uses the Adafruit's Fritzing parts library to create circuit diagrams for projects. You can download the library or just grab individual parts. Get the library and parts from GitHub - Adafruit Fritzing Parts.

parts_4

The anode (+) end of a nOOd can be identified by a teeny-tiny hole or dot in the metal end tab.

end_5

3D Print

3D Printed Parts

STL files for 3D printing will need to be oriented for printing using FDM machines.

Parts were printed with PLA filament.

The 3MF file is ready to print with colors assigned to print on multi color printers.

Original design source files may be downloaded using the links below.

printed_6

printed_7

The dropdown on the Fusion 360 site allows you to pick your preferred 3D file format like STEP, STL, etc.

Edit Case Design

Edit Sign Design

nOOd Case + Bar Sign 3mf

Slice with settings for PLA material

The parts were sliced using BambuStudio using the slice settings below.

  • PLA filament 220c extruder

  • 0.2 layer height

  • 10% gyroid infill

  • 200mm/s print speed

  • 60c heated bed

sliced_8

Multi color print

Letters on the sign have a .1mm indent on the front and back making it easy to "color" with the paint bucket tool. Use translucent filament to allow the light to diffuse.

multicolor_9

Assemble

Measure wires

Use silicone wire to solder to the ends of the nOOds. Denote the positive and negative connections with markings or with red (+) and black (-) wires.

Use heat shrink tubing to protect the soldered ends. Slip a piece on before soldering and then slip it over the joint and heat to seal.

Use a flat head screwdriver on the terminal blocks to attach the wires into the + and - CC out connectors.

Measure and cut a JST socket wire for power and connect to the 3-5 Vin terminal blocks.

Assemble case

Note the + and - labels on the case to correctly align the terminal blocks on the board to place inside the case.

Align the lid part to the mini–DIP switches. Place one side of the lid over the snap fit part and then use force to snap fit the other side into place.

Use M2.5x5mm screws on the two tabs to mount the case.

measure_10

measure_11

Attach nOOds

The LED nOOds press fit into the channels on the sign part. Align the strip and gently press fit at the same angle so the filament strip does not twist along the channel.

Connect power and adjust the current to achieve to the desired brightness.

attach_12

attach_13

attach_14

Número de parte del fabricante 6354
CONSTANT CURR LED DRVR TPS61169
Adafruit Industries LLC
Número de parte del fabricante 5508
LED MOD BLUE LINEAR STRIP
Adafruit Industries LLC
Número de parte del fabricante 5506
LED MOD RED LINEAR STRIP
Adafruit Industries LLC
Número de parte del fabricante 3814
JST PH 2 PIN CABLE MALE HEADER 2
Adafruit Industries LLC
Número de parte del fabricante 3165
HOOK-UP 30AWG 600V RED 50'
Adafruit Industries LLC
Número de parte del fabricante 3164
HOOK-UP 30AWG 600V BLACK 50'
Adafruit Industries LLC
Número de parte del fabricante 4559
PRE-CUT MULTI-COLORED HEAT SHRIN
Adafruit Industries LLC
Número de parte del fabricante 3434
STAINLESS STEEL SPUDGER - DOUBLE
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.