Maker.io main logo

LO-LA59 Droid

87

2022-08-30 | By Adafruit Industries

License: See Original Project 3D Printing Wearables

Courtesy of Adafruit

Guide by Ruiz Brothers

Overview

Build Lola, the companion droid to young Princess Leia.‎

 

This cute shoulder bot emotes by flapping her wings and blinking ‎both LED eyes. Small and light enough to carry around on your next ‎mission!‎

Embedded magnets allow Lola to attach to your shoulder or metal ‎surfaces!‎

magnets_1

magnets_2

Animatronic Wings‎

Two micro servos articulate each wing by pushing under the panel. ‎This makes it simple to assemble and less likely to strip the servos. ‎

wings_3

Mount with Magnets ‎‎

The bottom of the body feature spots for press fitting magnets to ‎attach to legs, shoulders, or metal objects!‎

wings_3a

ItsyBitsy RP2040‎‎

Powered by the ItsyBitsy RP2040. This dev board is packed with lots ‎of great features and has the ability to use both Arduino and ‎CircuitPython.‎

mount_4

body_5

Parts

parts_6

body_6

Circuit Diagram

The wiring diagram below provides a visual reference for connecting ‎the components. It is not true to scale; it is just meant to be used as ‎reference. This diagram was created using the Fritzing software ‎package.‎

Take a moment to review the components in the circuit diagram. ‎This illustration is meant for referencing wired connections - the ‎length of wire, position, and size of components are not exact. ‎

Wires are measured and cut to have enough slack to reach each ‎component.‎

Silicone ribbon wire is used to make them easier to coil and manage ‎each wire inside the tight enclosure space.‎

diagram_7

Wired Connections

The two micro-servos share voltage, ground, and signal connections.‎

NeoPixel to ItsyBisty

  • DIN from NeoPixel to pin 5 on ItsyBitsy

  • ‎5V from NeoPixel to VHI on ItsyBitsy

  • GND from NeoPixel to GND on ItsyBitsy

Servo

  • VCC wire to VHI on ItsyBitsy

  • GND wire to GND on ItsyBitsy

  • Signal wire to pin A2 on ItsyBitsy

Lipoly Backpack

  • Bat on Backpack to Bat on ItsyBitsy

  • G on Backpack to G on ItsyBitsy

  • ‎5V on Backpack to USB on ItsyBitsy‎

Slide Switch

  • Pin 1 to switch pin on Lipoly Backpack

  • Pin 2 to switch pin on Lipoly Backpack

CircuitPython

CircuitPython is a derivative of MicroPython designed to simplify ‎experimentation and education on low-cost microcontrollers. It ‎makes it easier than ever to get prototyping by requiring no upfront ‎desktop software downloads. Simply copy and edit files on ‎the CIRCUITPY drive to iterate.‎

CircuitPython QuickStart

Follow this step-by-step to quickly get CircuitPython running on your ‎board.‎

Download the latest version of CircuitPython for this board

Click the link above to download the latest CircuitPython UF2 file.‎

Save it wherever is convenient for you.‎

download_8

board_9

To enter the bootloader, hold down the BOOT/BOOTSEL ‎button (highlighted in red above), and while continuing to hold it ‎‎(don't let go!), press and release the reset button (highlighted in ‎blue above). Continue to hold the BOOT/BOOTSEL button until the ‎RPI-RP2 drive appears!‎

If the drive does not appear, release all the buttons, and then repeat ‎the process above.‎

You can also start with your board unplugged from USB, press, and ‎hold the BOOTSEL button (highlighted in red above), continue to ‎hold it while plugging it into USB, and wait for the drive to appear ‎before releasing the button.‎

A lot of people end up using charge-only USB cables and it is very ‎frustrating! Make sure you have a USB cable you know is good for ‎data sync.‎

You will see a new disk drive appear called RPI-RP2.‎‎ ‎

Drag the adafruit_circuitpython_etc.uf2 file to RPI-RP2.‎

drag_10

drag_11

The RPI-RP2 drive will disappear, and a new disk drive ‎called CIRCUITPY will appear.‎

That's it, you're done! :)‎

drive_12

Safe Mode

You want to edit your code.py or modify the files on ‎your CIRCUITPY drive but find that you can't. Perhaps your board ‎has gotten into a state where CIRCUITPY is read-only. You may have ‎turned off the CIRCUITPY drive altogether. Whatever the reason, safe ‎mode can help.‎

Safe mode in CircuitPython does not run any user code on startup ‎and disables auto-reload. This means a few things. First, safe ‎mode bypasses any code in boot.py (where you can ‎set CIRCUITPY read-only or turn it off completely). Second, it does ‎not run the code in code.py. And finally, it does not automatically ‎soft-reload when data is written to the CIRCUITPY drive.‎

Therefore, whatever you may have done to put your board in a non-‎interactive state, safe mode gives you the opportunity to correct it ‎without losing all of the data on the CIRCUITPY drive.‎

Entering Safe Mode in CircuitPython 6.x

This section explains entering safe mode on CircuitPython 6.x.‎

section_13

To enter safe mode when using CircuitPython 6.x, plug in your board ‎or hit reset (highlighted in red above). Immediately after the board ‎starts up or resets, it waits 700ms. On some boards, the onboard ‎status LED (highlighted in green above) will turn solid yellow during ‎this time. If you press reset during that 700ms, the board will start up ‎in safe mode. It can be difficult to react to the yellow LED, so you ‎may want to think of it simply as a slow double click of the reset ‎button. (Remember, a fast double click of reset enters the ‎bootloader.)‎

Entering Safe Mode in CircuitPython 7.x

This section explains entering safe mode on CircuitPython 7.x.‎

To enter safe mode when using CircuitPython 7.x, plug in your board ‎or hit reset (highlighted in red above). Immediately after the board ‎starts up or resets, it waits 1000ms. On some boards, the onboard ‎status LED (highlighted in green above) will blink yellow during that ‎time. If you press reset during that 1000ms, the board will start up in ‎safe mode. It can be difficult to react to the yellow LED, so you may ‎want to think of it simply as a slow double click of the reset button. ‎‎(Remember, a fast double click of reset enters the bootloader.)‎

In Safe Mode

Once you've entered safe mode successfully in CircuitPython 6.x, the ‎LED will pulse yellow.‎

If you successfully enter safe mode on CircuitPython 7.x, the LED will ‎intermittently blink yellow three times.‎

If you connect to the serial console, you'll find the following message.‎

Copy Code
Auto-reload is off.
Running in safe mode! Not running saved code.

CircuitPython is in safe mode because you pressed the reset button during boot. Press again to exit safe mode.

Press any key to enter the REPL. Use CTRL-D to reload.

You can now edit the contents of the CIRCUITPY drive. ‎Remember, your code will not run until you press the reset button, or ‎unplug and plug in your board, to get out of safe mode.‎

Flash Resetting UF2‎

If your board ever gets into a really weird state and doesn't even ‎show up as a disk drive when installing CircuitPython, try loading ‎this 'nuke' UF2 which will do a 'deep clean' on your Flash ‎Memory. You will lose all the files on the board, but at least you'll be ‎able to revive it! After loading this UF2, follow the steps above to re-‎install CircuitPython.‎

Download flash erasing "nuke" UF2‎

Code

code_14

Once you've finished setting up your ItsyBitsy with CircuitPython, ‎you can access the code and necessary libraries by downloading the ‎Project Bundle.‎

To do this, click on the Download Project Bundle button in the ‎window below. It will download as a zipped folder.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2021 Phil Burgess for Adafruit Industries
#
# SPDX-License-Identifier: MIT

"""
Lola Droid Shoulder Robot with servo and NeoPixel
"""

# pylint: disable=import-error
import time
import random
import board
import pwmio
import neopixel
from adafruit_motor import servo
from adafruit_led_animation.animation.comet import Comet
from adafruit_led_animation.animation.SparklePulse import SparklePulse
from adafruit_led_animation.sequence import AnimationSequence
from adafruit_led_animation.color import RED, BLUE

PIXEL_PIN = board.D5
SERVO_PIN = board.A2
NUM_PIXELS = 12
ORDER = neopixel.GRB
BRIGHTNESS = 0.1

# Initialize servo
PWM = pwmio.PWMOut(SERVO_PIN, frequency=50)
SERVO = servo.Servo(PWM)

# Initialize NeoPixels and animations
PIXELS = neopixel.NeoPixel(PIXEL_PIN, NUM_PIXELS, auto_write=False,
                           pixel_order=ORDER)
LARSON = Comet(PIXELS, bounce=True, speed=0.6/NUM_PIXELS,
               tail_length=NUM_PIXELS//2,
               color=(RED[0] * BRIGHTNESS,  # This is a little faster than
                      RED[1] * BRIGHTNESS,  # using the NeoPixel brightness
                      RED[2] * BRIGHTNESS)) # setting.
SPARKLE = SparklePulse(PIXELS, period=2, speed=0.15,
                       max_intensity=BRIGHTNESS, color=BLUE)
ANIMATIONS = AnimationSequence(LARSON, SPARKLE, advance_interval=7,
                               auto_clear=False)

SERVO.angle = POSITION = NEXT_POSITION = 7
MOVING = False                # Initial state = paused
START_TIME = time.monotonic() # Initial time
DURATION = 1.0                # Hold initial position for 1 sec

while True: # Loop forever...

    # Move turret -- randomly looks around and pauses
    NOW = time.monotonic()
    ELAPSED = NOW - START_TIME # Seconds since start of motion or pause
    if ELAPSED >= DURATION:    # End motion/pause?
        MOVING = not MOVING    # Toggle between those two states
        START_TIME = NOW       # and record the new starting time
        ELAPSED = 0.0
        if MOVING:             # Switching from paused to moving
            POSITION = NEXT_POSITION
            while abs(POSITION - NEXT_POSITION) < 10:  # Min +/- 10 degrees
                NEXT_POSITION = random.uniform(0, 90) # Try, try again
            DURATION = 0.2 + 0.6 * abs(POSITION - NEXT_POSITION) / 80
        else:                  # Switching from moving to paused
            SERVO.angle = NEXT_POSITION         # Move to end of sweep
            DURATION = random.uniform(0.5, 2.5) # Pause time
    if MOVING:
        FRACTION = ELAPSED / DURATION                        # Linear 0 to 1
        FRACTION = (3 * FRACTION ** 2) - (2 * FRACTION ** 3) # Ease in/out
        SERVO.angle = POSITION + (NEXT_POSITION - POSITION) * FRACTION

    ANIMATIONS.animate() # Cycle through NeoPixel animations

View on GitHub

Upload the Code and Libraries to the ItsyBitsy

After downloading the Project Bundle, plug your board into the ‎computer's USB port with a known good USB data+power cable. You ‎should see a new flash drive appear in the computer's File Explorer ‎or Finder (depending on your operating system) called CIRCUITPY. ‎Unzip the folder and copy the following items to the ‎PyPortal's CIRCUITPY drive. ‎

  • lib folder

  • code.py

Your PyPortal CIRCUITPY drive should look like this after copying ‎the lib folder and the code.py file.‎

pyportal_15

screen_16

3D Printing

Parts List

STL files for 3D printing are oriented to print "as-is" on FDM style ‎machines. Parts are designed to 3D print without any support ‎material. Original design source may be downloaded using the links ‎below.‎

3d_17

3d_18

Edit Design

Download STLs

Slice with settings for PLA material ‎‎

The parts were sliced using CURA using the slice settings below.‎

  • PLA filament 220c extruder

  • ‎0.2-layer height

  • ‎10% gyroid infill

  • 60mm/s print speed

  • ‎60c heated bed‎

Supports

  • Support Extrusion Width: .2

  • Support Density: 4%‎

  • Support Overhang Angle: 50

  • Support Z Height: .21

  • Interface: On

  • Support Roof: On

  • Support Pattern: Zig Zag

Build Plate Adhesion

  • Type: brim

  • Line Count: 8‎

slice_19

slice_20

Painting‎

Use a metallic paint to give the body a shine coat. It will take four to ‎five coats to cover the droid.‎

painting_21

Assemble

Solder Boards‎

‎Follow the circuit diagram to connect the two boards together. ‎

Place the components over the mounts on the case to measure wire ‎length.‎

solder_22

solder_23

Connectors‎ ‎

Use male and female headers to easy connect the two servos and ‎two NeoPixel boards. You may use Kapton tape to seal the ‎connections.‎

connectors_24

Mount Magnet

Align the magnet pin to press fit through the cutouts on the case.‎

magnet_25

magnet_25

Mount boards

The ItsyBitsy, Lipo backpack, and slide switch press fit into the ‎bottom body. Align the ItsyBitsy USB port to the opening of the case.‎

Mount Servo to Center Body

‎Place the two servos with the mounting holes against the flat walls ‎of the center body part. ‎

mount_28

mount_27

Servo Horns

‎The left horn attaches to the servo with the corner cut out on the ‎case. Use the included screws to secure both horns to each servo.‎

Thread wires‎

Push the two servo wires into the center hole on the case. Coil the ‎wires to avoid cutting them short.‎

Align Bottom and Center Body‎

Rotate the Bottom Part so the USB port opening points towards the ‎back of Lola. Orient the Center Body part so the two holes (LED eyes) ‎face the opposite side of the USB port.‎

Pass the two LED wires from the underside of the Center Part to the ‎top.‎

Place the battery on same side as the slide switch. The battery plugs ‎into the JST port on the lipo backpack board.‎

align_29

align_30

Connects‎

Plug all the connectors together.‎

Attach Center to Bottom Body‎

Align the Bottom Body part clips to the center body grooves.‎

Use a Spudger tool to disassemble if needed.‎

attach_31

attach_32

Wing Assemble‎

A metal paper clip is used to create the pin for the wings. Use ‎Precision Flat Pliers to carefully bend the wire to fit the curvature of ‎the wing tabs. ‎

wing_33

wing_34

‎Use eye and protection and gloves and use caution in cutting paper ‎clips as metal piece(s) may fly in uncertain directions.‎

Tail Assemble ‎‎

Align the tail so the cut corner faces the eyes. This allows the tail to ‎fully fold forward for transporting the droid. ‎

tail_35

tail_36

Connect NeoPixels‎

Solder male headers to the NeoPixel Jewel and NeoPixel Button.‎

Pass the LED wires into the Top Body cut outs. ‎

connect_37

connect_38

Attach Top Body‎

‎Align the clips on the top body part to the grooves on the Center ‎Body part. Seat the first to clips into the groove then the press fit the ‎last two clips into the grooves.‎

top_39

Attach diffuser domes

Connect the Neopixel boards to the wires.‎

domes_40

‎Complete‎

Use skate lubricant to help the wings to flap smoothly.‎

complete_41

Número de parte del fabricante 4888
ADAFRUIT ITSYBITSY RP2040
Adafruit Industries LLC
Número de parte del fabricante 1443
16MM ILLUMINATED PUSHBUTTON - GR
Adafruit Industries LLC
Número de parte del fabricante 169
SERVOMOTOR RC 5V TOWERPRO
Adafruit Industries LLC
Número de parte del fabricante 2226
ADDRESS LED MODULE SERIAL RGB
Adafruit Industries LLC
Número de parte del fabricante 1612
ADDRESS LED MOD SERIAL RGB 1=5
Adafruit Industries LLC
Número de parte del fabricante 3434
STAINLESS STEEL SPUDGER - DOUBLE
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.