Maker.io main logo

LilyPad E-Sewing ProtoSnap Hookup Guide

76

2018-01-03 | By SparkFun Electronics

License: See Original Project Switches Wearables Adafruit Feather

Courtesy of SparkFun

Introduction

The LilyPad E-Sewing ProtoSnap is a great way to explore how buttons and switches behave in simple e-sewing circuits before crafting your project. This guide will go over the individual components in the E-Sewing ProtoSnap and how to break it apart to prepare for use in a project. You can follow along with this guide for both the E-Sewing ProtoSnap and E-Sewing ProtoSnap Kit.

LilyPad E-Sewing ProtoSnap

LilyPad E-Sewing ProtoSnap

LilyPad E-Sewing ProtoSnap Kit

Suggested Reading

If this is your first sewable electronics project, we recommend you read our LilyPad E-Sewing tutorial.

LilyPad Basics E-Sewing

LilyPad Basics: E-Sewing

December 17, 2016

Learn how to use conductive thread with LilyPad components.

Hardware Overview and Features

Don’t snap apart your LilyPad E-Sewing ProtoSnap until you're ready to use the pieces in a project. If you leave the pieces attached to the board, you'll be able to prototype and test your project before you start sewing.

Like other LilyPad ProtoSnap series boards, the individual pieces of the board are pre-wired - allowing you to try out the function of the circuit before sewing. The E-Sewing ProtoSnap includes three white LilyPad LEDs: two connected to a LilyPad Slide Switch and one connected to a LilyPad Button Board. A LilyPad Coin Cell Battery Holder with a 3V Coin Cell Battery provides the power for the circuit. These parts are connected together by conductive pathways called traces.

Image 4

Required Materials and Tools

If you are using the E-Sewing ProtoSnap Kit, you will also have:

To create a finished project with the E-Sewing ProtoSnap you will also need:

  • Materials listed above (if not using the E-Sewing ProtoSnap Kit)

  • Felt or fabric to stitch your circuit into

  • Pen, marker, or chalk

  • Scissors

  • Hot glue gun (with extra glue)

  • Optional: Craft supplies for decorating (feathers, sequins, buttons, etc.)

Exploring the Sample Circuit

Let’s try out the circuit!

The LilyPad Battery Holder at the corner of the ProtoSnap holds a 20mm CR2032 Coin Cell Battery. With the battery installed, slide switch on the battery holder to the ON position.

LilyPad Battery Holder

Using the LilyPad Slide Switch

The LilyPad Slide Switch has a small switch labeled ON/OFF. When moved to the OFF position, parts inside the switch move away from each other and open the circuit (disconnecting it). The LEDs will not light up. When the toggle switch is moved to the ON position, the two sew tabs on the switch are connected, allowing current to flow through and close the circuit. You should see the two LEDs below the switch light up.

Image 6

Using the LilyPad Button

The LilyPad Button Board is also a type of switch. The circuit that is connected to the far right LED is open when the button is left by itself. When you press the button in the middle of the board, it connects the two sew tabs and allows current to flow through. When you let go of the button, the connection is opened again, and the button springs back into place. This button is an example of a momentary switch – it is only active when an action is applied.

This is slightly different from the slide switch, which is an example of a maintained switch, meaning its state remains the same until changed.

Image 7

Learn more about buttons and switches in our Switch Basics tutorial.

Stitching into a Project

Ready to sew into a project? First, slide the coin cell battery out of the battery holder and set aside.

Carefully snap apart the connected components on the E-Sewing ProtoSnap panel to prepare for sewing. Discard the non-sewable pieces and scraps. Use a set of pliers or diagonal cutters if you are having trouble snapping the pieces apart. You will end up with six individual LilyPad pieces: the battery holder with battery, three LEDs, button, and switch.

remove your battery

Always remove your battery when working on your circuit to avoid damaging your components.

Designing Your Project

Sketch on a piece of paper or arrange the LilyPad pieces on your felt or fabric to form your design. At this point, you can recreate the connections the pieces had in the ProtoSnap format or design your own new configuration. Keep in mind that the positive tabs of the LED must connect to the button or switch in order to be controlled by them. The negative tabs of the LEDs should connect back to the negative tab on the battery holder.

project diagram

The image above is an example of a project diagram using the E-Sewing ProtoSnap. For instructions and downloadable template, visit the Light-Up Plush tutorial.

When your circuit design is finalized, secure the LilyPad pieces on your project with a small dab of hot glue or fabric glue, making sure not to cover the holes in the sew tabs. Double check the orientation of the LilyPad pieces against your diagram (or template if using a SparkFun design) before gluing.

Image 10

To help you plan your stitch lines, draw your circuit onto the fabric with chalk or a washable marker.

use chalk or a washable marker

After arranging the circuit, carefully connect each LilyPad component together with conductive thread stitching. Each connection between components should be a separate piece of conductive thread and avoid crossing other stitch lines.

If have never sewn with conductive thread this tutorial covers the basics.

LilyPad Basics E-Sewing

LilyPad Basics: E-Sewing

December 17, 2016

Learn how to use conductive thread with LilyPad components.

Troubleshooting

With any electronics project, there are times you will have to troubleshoot if your circuit isn’t working. If your circuit isn’t lighting up, try a new battery or check that your project is switched on. Check your sewing for any loose threads or ends that may be touching other parts of your circuit and causing a short circuit. Learn more about troubleshooting your project in the LilyPad Basics: E-Sewing tutorial.

Example Projects and Templates

Check out the Light-Up Plush project tutorial for step-by-step instructions on using the E-Sewing ProtoSnap in a project.

Image 13

Light-Up Plush

December 16, 2016

Craft a light-up plush with LilyPad LEDs controlled by pressing a button and sliding a switch in the creature's hands.

Project Templates

Looking for some more project ideas? Below are a few templates to use with an embroidery hoop or making another plush. Click on the button to download and print (2 pages each).

Image 14

Image 14

DOWNLOAD FIREFLY TEMPLATE

Image 15

Image 15

DOWNLOAD ROBOT TEMPLATE

Image 16

Image 16

DOWNLOAD SPACE TEMPLATE

Image 17

Image 17

Image 17

DOWNLOAD PLUSH CAT TEMPLATE

Resources and Going Further

For more information about the LilyPad E-Sewing ProtoSnap, check out the resources below:   

Número de parte del fabricante 13902
LED WHITE LILYPAD 5PCS
SparkFun Electronics
Número de parte del fabricante 09350
SLIDE SWITCH
SparkFun Electronics
Número de parte del fabricante 08776
BUTTON BOARD
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.