Maker.io main logo

LED Silhouette Christmas Cards

47

2024-12-12 | By Kitronik Maker

License: None LEDs / Discrete / Modules

Courtesy of Kitronik

Guide by Kitronik Guide

For day eight of our 12 Makes of Christmas we made some LED Silhouette ‎Christmas Cards. Follow our step-by-step guide and make your own.‎

designs_1

We've included all of the DXF files so that you can cut out our designs with a ‎laser cutter. If you don't have access to a laser cutter, you can easily cut out your ‎own designs by hand and still follow along with the instructions below.‎

You Will Need:‎

‎‎LED Silhouette Christmas Cards:‎

cards_2

Create your own LED Christmas cards using a copper tape circuit! Use our ‎detailed laser cut designs, cut out the simpler designs by hand or design your own!‎

Step 1:‎

step1_3

Cut out your chosen card design from some black or dark coloured card. The ‎cutting files have been colour coded to indicate cutting order. For best results they ‎should be cut in the following order.‎

Red Lines - First.‎

Green Lines - Second.‎

Black Lines - Third.‎

‎Step 2:

step2_4

Use some coloured tissue paper and rip up the edges to create the background for ‎your scene.‎

tissue_5

Don’t use too many layers or the LEDs may not be visible – 3 to 5 is usually ‎enough.‎

Step 3:‎

step3_6

Begin glueing the layers of tissue paper to the rear of the card.‎

glueing_7

Glue them one layer at a time.‎

layer_8

Until all of your layers are in place.

place_9

Step 4:‎

step4_10

Plan out where you want to place your LEDs and cut some small slots, just enough ‎for the pins to fit through.‎

plan_11

Push the LEDs into place and spread the pins out, with the positive and negative ‎pins facing opposite directions.‎

push_12

For this card I used some RGB LEDs – I cut the red pin and used the others ‎together to create a turquoise colour.‎

Step 5:‎

step5_13

Plan out your circuit, starting with the position of the battery (a CR2032 3V battery ‎is recommended). The circuit needs to be laid out in parallel for all the LEDs to ‎work. Place the copper tape down where the battery will be and create a loop ‎passing over all of the negative pins.‎

circuit_14

For corners, fold the tape the opposite way and then back on itself as shown. ‎

Step 6:‎

step6_15

Create another loop of tape covering all of the positive pins, leading back to the ‎battery.‎

create_16

Fold the tape back on itself to make a tab to go over the battery.‎

fold_17

Create a loop of copper tape with the sticky side out to fix the battery in place. ‎

Step 7:

step7_18

Press the tab down over the battery and test that the LEDs turn on. If some of the ‎LEDs are struggling to light up, add some extra tape to give a better connection.‎

press_19

Cut a small door into the back of the card as shown to allow access to the battery ‎before gluing the inner piece of the card with the LEDs in place.‎

cut_20

Use some more copper tape to fix the tab of the circuit to the door on the back of ‎the card.‎

tape_21

Use a paperclip to hold the circuit shut and light up the LEDs. If sending in a card, ‎place a small piece of paper over the battery to break the circuit so the battery is ‎not wasted.‎

paperclip_22

This concludes the eighth of our 12 Makes of Christmas, we'll be back ‎tomorrow for the last in this series of festive making activities. You can check out ‎the other Makes of Christmas, here.‎

©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof ‎without Kitronik's prior written consent.

Número de parte del fabricante 3544
LED RGB DIFFUSED 10MM T/H
Kitronik Ltd.
Número de parte del fabricante 3527
LED RGB DIFFUSED 5MM T/H
Kitronik Ltd.
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.