Maker.io main logo

LED Noodle Holiday Tree

97

2023-12-12 | By Adafruit Industries

License: See Original Project 3D Printing Programmers

Courtesy of Adafruit

Guide by Ruiz Brothers

Overview

Build a light-up tree with LED noodles, QT Py RP2040 and an ‎AW9523 LED driver. This 3D printed project features eight helical ‎spokes that spiral and taper to form a tree. Each LED noodle fades ‎sequentially creating a subtle effect that brings the lights to life. ‎

 

The AW9523 LED driver connects to the QT Py RP2040 over STEMMA ‎QT to easily control the LED noodles using PWM with CircuitPython.‎

Choose from a range of LED noodle colors to create your own color ‎combination. Each easily press fits into the spokes of the tree ‎making a glue-free assembly.‎

driver_1

An elegant tree topper sits atop the tree, concealing the various ‎wires. A piece of heat shrink tubing keeps the wires held together ‎and passes down to the bottom connecting to the LED driver board.‎

topper_2

Prerequisite Guides

Take a moment to review the following guides to learn more about ‎the products.‎

tree_3

Parts

Hardware

Required screws and nuts for assembly.‎

  • ‎2x M3 x 6mm long pan head machine screws‎

  • ‎4x M3 x 10mm long pan head machine screws

  • ‎6x M3 hex nuts

  • ‎4x M2.5 x 6mm long pan head machine screw‎

Circuit Diagram

The diagram below provides a general visual reference for wiring of ‎the components once you get to the Assembly page. This diagram ‎was created using the software package Fritzing.‎

Adafruit Library for Fritzing

Adafruit uses the Adafruit's Fritzing parts library to create circuit ‎diagrams for projects. You can download the library or just grab ‎individual parts. Get the library and parts from GitHub - Adafruit Fritzing ‎Parts.‎

fritzing_4

Wired Connections

The QT Py RP2040 is powered by a 5V 1A USB power supply.‎

  • The AW9523 connects to the QT Py using Stemma QT cable

  • The 4x red LED noodles connect to pins 15-12 on the AW9523

  • The 4x green LED noodles connect to pins 7-5 on the AW9523

  • ‎220ohm resistors are in line with the ground (cathode) of the ‎green LED noodles‎

CAD Files

CAD Assembly

The QT Py RP2040 snap fits onto the PCB mount. The AW9523 is ‎secured to the PCB mount using M2.5 machine screws. The PCB ‎mount is secured to the bottom holder using M3 screws.‎

The bottom cover is fitted under the tree. The tree is secured to the ‎bottom holder using M3 screws and hex nuts. The tree topper fits ‎over the tip of the tree. The star press fits into the tree topper.‎

leds_CAD

‎3D Printed Parts List‎

  • ‎2x Adafruit Star.stl

  • ‎1x Bottom Cover.stl‎

  • ‎1x PCB Mount.stl

  • ‎1x Topper.stl

  • ‎1x Tree Holder.stl

  • ‎1x Tree.stl

  • Bottom Cover Wire Slit.stl (optional)‎

parts_5

Download CAD source

Download STLs.zip

Build Volume

The parts require a 3D printer with a minimum build volume.‎

  • ‎112mm (X) x 112mm (Y) x 230mm (Z)‎

require_6

Translucent Filament

Choose your desired color of filament. A white opaque colored ‎filament will offer a soft-even diffusion while a "clear" transparent ‎filament will give sharp and direct diffusion.‎

color_7

Design Source Files

The project assembly was designed in Fusion 360. This can be ‎downloaded in different formats like STEP, STL and more. Electronic ‎components like Adafruit's boards, displays, connectors and more ‎can be downloaded from the Adafruit CAD parts GitHub Repo.‎

board_8

CircuitPython

CircuitPython is a derivative of MicroPython designed to simplify ‎experimentation and education on low-cost microcontrollers. It ‎makes it easier than ever to get prototyping by requiring no upfront ‎desktop software downloads. Simply copy and edit files on ‎the CIRCUITPY drive to iterate.‎

CircuitPython Quickstart

Follow this step-by-step to quickly get CircuitPython running on your ‎board.‎

Download the latest version of CircuitPython for this board via ‎circuitpython.org

Click the link above to download the latest CircuitPython UF2 file.‎

Save it wherever is convenient for you.‎

click_9

button_10

To enter the bootloader, hold down the BOOT/BOOTSEL ‎button (highlighted in red above), and while continuing to hold it ‎‎(don't let go!), press and release the reset button (highlighted in ‎blue above). Continue to hold the BOOT/BOOTSEL button until the ‎RPI-RP2 drive appears!‎

If the drive does not appear, release all the buttons, and then repeat ‎the process above.‎

You can also start with your board unplugged from USB, press, and ‎hold the BOOTSEL button (highlighted in red above), continue to ‎hold it while plugging it into USB, and wait for the drive to appear ‎before releasing the button.‎

A lot of people end up using charge-only USB cables and it is very ‎frustrating! Make sure you have a USB cable you know is good for ‎data sync.

You will see a new disk drive appear called RPI-RP2.‎‎ ‎

Drag the adafruit_circuitpython_etc.uf2 file to RPI-RP2.‎

disk_11

disk_12

The RPI-RP2 drive will disappear, and a new disk drive ‎called CIRCUITPY will appear.‎

That's it, you're done! :)‎

drive_13

Safe Mode

You want to edit your code.py or modify the files on ‎your CIRCUITPY drive but find that you can't. Perhaps your board ‎has gotten into a state where CIRCUITPY is read-only. You may have ‎turned off the CIRCUITPY drive altogether. Whatever the reason, safe ‎mode can help.‎

Safe mode in CircuitPython does not run any user code on startup ‎and disables auto-reload. This means a few things. First, safe ‎mode bypasses any code in boot.py (where you can ‎set CIRCUITPY read-only or turn it off completely). Second, it does ‎not run the code in code.py. And finally, it does not automatically ‎soft-reload when data is written to the CIRCUITPY drive.‎

Therefore, whatever you may have done to put your board in a non-‎interactive state, safe mode gives you the opportunity to correct it ‎without losing all of the data on the CIRCUITPY drive.‎

Entering Safe Mode

To enter safe mode when using CircuitPython, plug in your board or ‎hit reset (highlighted in red above). Immediately after the board ‎starts up or resets, it waits 1000ms. On some boards, the onboard ‎status LED (highlighted in green above) will blink yellow during that ‎time. If you press reset during that 1000ms, the board will start up in ‎safe mode. It can be difficult to react to the yellow LED, so you may ‎want to think of it simply as a slow double click of the reset button. ‎‎(Remember, a fast double click of reset enters the bootloader.)‎

In Safe Mode

If you successfully enter safe mode on CircuitPython, the LED will ‎intermittently blink yellow three times.

‎If you connect to the serial console, you'll find the following message.‎

Copy Code
Auto-reload is off.
Running in safe mode! Not running saved code.

CircuitPython is in safe mode because you pressed the reset button during boot. Press again to exit safe mode.

Press any key to enter the REPL. Use CTRL-D to reload.

You can now edit the contents of the CIRCUITPY drive. ‎Remember, your code will not run until you press the reset button, or ‎unplug and plug in your board, to get out of safe mode.‎

Flash Resetting UF2‎

If your board ever gets into a really weird state and doesn't even ‎show up as a disk drive when installing CircuitPython, try loading ‎this 'nuke' UF2 which will do a 'deep clean' on your Flash ‎Memory. You will lose all the files on the board, but at least you'll be ‎able to revive it! After loading this UF2, follow the steps above to re-‎install CircuitPython.‎

Download flash erasing "nuke" UF2‎

Coding The LED Noodle Tree

Once you've finished setting up your QT Py RP2040 with ‎CircuitPython, you can access the code and necessary libraries by ‎downloading the Project Bundle.‎

To do this, click on the Download Project Bundle button in the ‎window below. It will download to your computer as a zipped folder.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2023 Phil Burgess for Adafruit Industries
#
# SPDX-License-Identifier: MIT

import math
import time
import board
import adafruit_aw9523

GAMMA = 2.6         # For perceptually-linear brightness
PINS = (15, 14, 13, 12, 7, 6, 5, 4) # List of pins, one per nOOd

# Instantiate AW9523 on STEMMA I2C bus. This was tested on QT Py RP2040.
# Other boards might require board.I2C() instead of board.STEMMA_I2C().
aw = adafruit_aw9523.AW9523(board.STEMMA_I2C())

for pin in PINS:
    aw.get_pin(pin).switch_to_output(value=True) # Activate pin, initialize OFF
    aw.LED_modes |= 1 << pin                     # Enable constant-current on pin

while True:                        # Repeat forever...
    for i, pin in enumerate(PINS): # For each pin...
        # Calc sine wave, phase offset for each pin, with gamma correction.
        # If using red, green, blue nOOds, you'll get a cycle of hues.
        phase = (time.monotonic() - 2 * i / len(PINS)) * math.pi
        brightness = int((math.sin(phase) + 1.0) * 0.5 ** GAMMA * 255 + 0.5)
        aw.set_constant_current(pin, brightness)

View on GitHub

Upload the Code and Libraries to the RP2040 ‎Prop-Maker Feather

After downloading the Project Bundle, plug your QT Py RP2040 into ‎the computer's USB port with a known good USB data+power cable. ‎You should see a new flash drive appear in the computer's File ‎Explorer or Finder (depending on your operating system) ‎called CIRCUITPY. Unzip the folder and copy the following items to ‎the QT Py RP2040's CIRCUITPY drive.‎

  • lib folder

  • code.py

Your QT Py RP2040 CIRCUITPY drive should look like this after ‎copying the lib folder and the code.py file.‎

file_14

Wiring and Assembly

Ground Wires

Create four wires for the green and red LED noodle ground ‎connections. These should have a length of 5 inches (12.7cm) each.‎

ground_15

Solder Ground Wires

Attach the ground wires to the cathode pins of the LED noodles with ‎solder. ‎

solder_16

To know which end of the n00d is cathode and which is anode, see ‎the guide page at https://learn.adafruit.com/noods-uberguide/electrical-‎properties

Voltage Wires

Create four wires for the green and red LED noodles voltage ‎connection. These should have a length of 13.5 inches (34cm) each.‎

voltage_17

Solder Voltage Wires

Attach the voltage wires to the anode pins of the LED noodles with ‎solder. The anode pins can be identified by a teeny-tiny hole in the ‎metal end tab.‎

attach_18

Wired LED Noodles

Check the wires have been properly soldered to the cathode pins on ‎each LED noodle.‎

noodles_19

noodles_20

Install Noodles

Add the green LED noodles to the outer spirals of the tree by ‎pressing them into the channels.‎

The red LED noodles can then be added to the inner spirals of the ‎tree. Precision tweezers or a fine tipped tool can be used to help ‎assist in pressing the noodles into the inner channels. ‎

install_21

install_22

Tree Tip

Ensure the LED noodles are fully seated in the channels, so the ‎voltage wires are pointing out towards the tip of the tree.‎

tip_23

Heat Shrink

Grab a piece of heat shrink tubbing, preferably a white color from ‎the multi-colored pack. The diameter of the tube should ‎accommodate the eight voltage wires.‎

Carefully insert the eight voltage wires through the heat shrink ‎tubbing.‎

heat_24

heat_25

Install Heat Shrink

Insert the end of the heat shrink with the eight wires through the ‎hole in the top of the tree. Push the tubing through the opening until ‎the wires are fully fed through. ‎

install_26

install_27

Installed Heat Shrink

Ensure the voltage wires have been fully inserted through the ‎opening in the tip of the tree.‎

Optionally add another piece of heat shrink tubing to cover the full ‎length of the voltage wires.‎

shrink_28

shrink_29

Install Wires to Bottom Cover

Get the bottom cover ready. Insert the eight voltage wires through ‎the center hole of the cover so there's enough slack to solder them ‎to the AW9523 board.‎

wire_30

wire_31

Install Bottom Cover

Carefully fit the bottom cover into the tree by pressing the mount ‎tabs through the tree's ring.‎

The tree's ring may need a bit of flexing to push the bottom cover ‎tabs through.‎

Line up the mounting tabs with the tree's mounting holes.‎

cover_32

Coincell Test

Use the CR2032 coin cell battery to test each LED noodle.‎

This helps determine the LED noodles matching ground and voltage ‎wires.‎

To achieve a sequential fading effect, the wires from the LED ‎noodles will need to be ordered sequentially with the pins on the ‎AW9523 board.‎

battery_33

battery_34

Solder Wires to AW9523‎

Attach the ground wires to pins 15 – 4. ‎

Attach the voltage wires to the corresponding voltage pins.‎Solder the 220ohm resistors inline with the ground wires of the ‎green LED noodles.‎

Remember to use to the coin cell battery to test the order of the LED ‎noodles to your desired sequence.‎

solder_35

Connect QT Py RP2040‎

Use the short STEMMA QT cable to connect the AW9523 to the QT Py ‎RP2040.‎

connect_36

USB Power Test

Use a USB-C type cable and a 5V 1A USB power supply to power up ‎the circuit.‎

power_37

Mount QT Py RP2040

‎Install the QT Py into the 3D printed PCB mount by fitting it into the ‎holder.‎

Fit the front edges of the PCB underneath the clips.‎

Slightly flex the mount to get the back edges of the PCB to snap ‎over.‎

Ensure the USB-C port is facing the correct orientation.‎

mount_38

mount_39

Mount the AW9523 Board

Place the AW9523 PCB over the built-in standoffs on the 3D printed ‎PCB mount with the mounting holes lined up.‎

Use four M2.5 x 6mm long machine screws to secure the board to ‎the mount.‎

place_40

place_41

Secure the PCBs

Ensure the QT Py RP2040 and AW9523 are secured to the 3D printed ‎PCB mount.‎

Connect the boards together using the short STEMMA QT cable.‎

secure_42

Hardware for PCB Mount

Use two M3 x 6mm long screws to secure the PCB mount to the ‎bottom base.‎

hardware_43

Secure PCB Mount

Place the PCB mount over the two mounting holes in the bottom ‎base with the holes lined up.‎

Insert the M3 x 6mm long screws to attach the PCB mount to the ‎bottom case. Use two M3 hex nuts to secure the mount.‎

pcb_44

pcb_45

Installed PCB Mount

Take a moment to inspect the PCB mount has been properly ‎secured to the bottom base.‎

installed_46

Install Tree ‎

Carefully fit the tree onto the bottom base with the mounting holes ‎lined up.‎

Ensure all of the wires are fitted inside the bottom case.‎

tree_47

tree_48

Secure Tree

Use four M3 x 10mm long machine screws and hex nuts to secure ‎the bottom base to the tree and bottom cover.‎

securetree_49

securetree_50

Rubber Feet

Get the four rubber feet ready to stick onto the bottom of the tree ‎assembly.‎

Peel off the rubber feet from the pack and stick them onto desired ‎spots on the bottom of the base.‎

rubber_51

rubber_52

Install Tree Topper

Glue the two halves of the star together using super glue or your ‎preferred adhesive. ‎

Press fit the stem of the star into the top hole of the tree topper.‎

Place the tree topper over the tip of the tree. Optionally use ‎mounting tack or tape to secure the tree topper in place.‎

topper_53

Final Build

Power the QT Py using a USB-C type cable and a 5V 1A power supply ‎to turn on the LED noodle tree.‎

Congratulations on your build!‎

final_54

 

Número de parte del fabricante 4900
QT PY RP2040
Adafruit Industries LLC
Número de parte del fabricante 4886
STEMMA QT GPIO EXPANDER AW9523
Adafruit Industries LLC
Número de parte del fabricante 5507
LED MOD GREEN LINEAR STRIP
Adafruit Industries LLC
Número de parte del fabricante 5506
LED MOD RED LINEAR STRIP
Adafruit Industries LLC
Número de parte del fabricante 4399
STEMMA QWIIC JST SH CABLE 50MM
Adafruit Industries LLC
Número de parte del fabricante 3165
HOOK-UP 30AWG 600V RED 50'
Adafruit Industries LLC
Número de parte del fabricante 3169
HOOK-UP 30AWG 600V WHITE 50'
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.