Maker.io main logo

Laser Cut Edge-Lit Sign for Halloween 2020

10

2020-10-20 | By Kitronik Maker

License: See Original Project

Courtesy of Kitronik

Although it promises to be more subdued than normal, Halloween is fast approaching and that means it's time to get making. We thought we would make something quick and simple this year. Something that doesn't require going out to enjoy and that will also brighten the place up.

We came up with a few ideas but settled on this spooky edge-lit sign. The base for this sign is the base we designed for this edge-lit sign. Why re-invent the wheel? It's super simple to do and the results are well worth it. If you've already made a base, then this will be a quick win for you!

What You Will Need:

Note: The image we used to demonstrate what it could look like was not of our own making, so the DXF Pumpkin file we provided is a blank canvas for you to get creative with. Let's get to it!

Laser Cut Edge-Lit Sign for Halloween 2020:

sign_1

We're going to assume that you've made your base and are ready to tackle making the sign. The image above shows the DXF file loaded into Autocad, all it needs is a design for etching added and you are good to go! Why not try etching your own face onto the pumpkin, for that personal touch.

The Sign Material:

Now that you have your sign designed and ready, it's time to pick a suitable material. We chose an Orange Perspex Sheet (Fluorescent) 5mm x 600mm x 400mm sheet as we thought it was the perfect choice for Pumpkin. Any fluorescent sheet would probably look just as good.

To the Laser Cutter:

cutter_2

Now it's time to load your design into your laser cutter software of choice for the final result. The above image shows just the template with no design on it. Once cut out and assembled you should have something like;

design_3

We think that it looks quite impressive as is, but still not a patch on how it looks in the dark and with the strip light switched on!

light_4

Once upon a time when we all had TV's that were 3 feet deep, this would have looked great sat one! Fortunately, it will look equally fetching on a table, mantelpiece, or on a window sill for the enjoyment of passers by. Happy Halloween!

Also, keep a hold of the base, I have a feeling that it might come in handy for other seasonal fun too!

Other Halloween Project Ideas:

©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof without Kitronik's prior written consent.

Número de parte del fabricante 29314
MACH SCREW PAN HEAD SLOTTED M3
Keystone Electronics
Número de parte del fabricante 29311
MACH SCREW PAN HEAD SLOTTED M3
Keystone Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.