Maker.io main logo

Inertial Handwriting Recognition using Arduino Sense

155

2021-04-23 | By Beryl Sui

License: Attribution No Derivatives Arduino

Introduction

In this project, my friend and I assembled a "virtual pen" with Arduino 33 BLE Sense (1050-ABX00035-ND) that determines which digit the user is writing based on the motion they make holding the pen, without the use of a camera. The layout is shown in Fig 1. The button is pressed to indicate the start of motion. 

 Breadboard layout

Figure 1. The breadboard layout of the data collection device.

We aim to minimize the need for external computation or additional sensors outside of the device. Ideally the user can “write” on any surface or in the air with little restriction on location, orientation, or occlusion between the pen and the receiving device. We want the handwriting recognition to be robust to differences in scale (e.g. from the scale of writing on paper to writing for lecturing purposes), writing speed, and handwriting style.

As a proof of concept, we will implement recognition for a subset of arabic numerals. Our main objective is to make the device capable of recognizing the numbers accurately given robust motions. The device will be able to tell the difference between the hand motions when writing different numbers and analyze the motion data. The user will press a button to indicate when they are writing a single digit as opposed to just moving the pen between digits or are not using the pen.

Approach

We divided this project into 4 main steps:

1. Arduino IMU data collection for digits 0-9 in Python. 

2. Preprocess the data on the Arduino so that it works well as an input to machine learning system. 

3. Train a model using RNN (recurrent neural network) or CNN (convolutional neural network).

4. Test the system and check the accuracy of the model's predictions.

approach

Figure 2. The overall approach of the project.

Data Collection

Below is the Python code we used to collect data. To avoid fatigue of writing the same digit over and over, we generated random numbers from 0 to 9. Each dataset contains 20 digits and their corresponding acceleration information. Considering each digit took different amount of motion and time to write, the ones that took less time to write were zero-padded so that all the data points are of the same length.

Copy Code
target = np.repeat(np.arange(10), 2)
np.random.shuffle(target)

bigdata = np.zeros([20,3*119,7])

for i in range(20):
printmd("<span style=\"font-size:3em;\">" + str(target[i]) + "</span>")
data = []
with serial.Serial('COM3', 38400, timeout=10) as ser:
startmess = ser.readline()
if not startmess:
raise(Exception("Timed Out"))
if startmess != b'IMU goes BBBBRRRR\r\n':
raise(Exception("Start message invalid:\n"+str(startmess)))
ser.timeout = 0.1
while True:
message = ser.read(28)
if not message:
raise(Exception("Timed Out"))
if len(message)<24:
raise(Exception("Message Too Short:\n"+str(message)))
values = np.array(struct.unpack('fffffff',message))
if np.any(np.isnan(values)):
if np.any(~np.isnan(values)):
raise Exception("Could not read data:\n"+str(message))
else:
break
data.append(values)
data = np.array(data)
clear_output(wait=True)
print(data.shape[0])
data = np.pad(data,((0, 3*119-data.shape[0],), (0,0)))
print(np.mean(data, axis=0))
bigdata[i] = data

 

data

Fig 3. Visual representation of a collected data point for the digit "8".

Classification Model

Because we eventually needed to put this model on the Arduino through tflite, which currently does not support RNN, we implemented a CNN for our model. Below are the layers we used in our model. This worked well for classifying 10 groups of data. We achieved 90% of accuracy with testing and validation data, and a similar percentage when using this device.

CNN

Fig 4. CNN layers used in the inertial handwriting recognition system.

A Small Demo

 

I hope you liked this project and let me know if you have any questions and suggestions!

Número de parte del fabricante TW-E41-T1
BREADBOARD ASSEMBLY 6.50X2.20"
Twin Industries
$20.98
Ver más Details
Número de parte del fabricante HP0315AFKP2-R
SWITCH TACTILE SPST-NO 3VA 28V
NKK Switches
Número de parte del fabricante ABX00031
ARDUINO NANO 33 BLE SENSE
Arduino
More Info
Ver más Details
Número de parte del fabricante 64
BREADBOARD TERM STRIP 3.40X2.20"
Adafruit Industries LLC
Número de parte del fabricante FIT0010
JUMPER WIRE M TO M VARIOUS
DFRobot
Número de parte del fabricante TL1105F160Q
SWITCH TACTILE SPST-NO 0.05A 12V
E-Switch
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.