Maker.io main logo

How to Make an LED Matrix Digital Clock With Arduino Uno R4 WiFi

143

2026-01-12 | By Ron Cutts

License: GNU Lesser General Public License Displays LED / Display Drivers LED Matrix Real Time Clocks (RTCs) Arduino

In this Visual Programming Visuino tutorial, we’ll use the Arduino Uno R4 WiFi’s built-in RTC and LED Matrix to create a digital clock without any external hardware.

The built-in RTC (Real-Time Clock) is used to keep accurate time, while the onboard LED matrix displays the hours and minutes directly on the board.

Time data from the RTC is formatted and continuously sent to the LED matrix, updating the display in real time.

Using Visuino’s drag-and-drop interface, you can easily configure the RTC, format the time output, and control how the clock is displayed on the LED matrix.

This project demonstrates how to build a fully functional digital clock using only the Arduino Uno R4 WiFi, making it perfect for quick demos, learning RTC usage, or compact clock projects.

Note: No external RTC module or LED display is required — everything is already built into the Arduino Uno R4 WiFi board.

Watch the Video!

Step 1: What You Will Need

What You Will Need

What You Will Need

  1. Arduino UNO R4 Wifi

  2. Visuino program: Download Visuino

Step 2: Start Visuino, and Select the Arduino UNO R4 WiFi Board Type

Start Visuino, and Select the Arduino UNO R4 WiFi Board Type

Start Visuino, and Select the Arduino UNO R4 WiFi Board Type

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO R4 WiFi" as shown in Picture 2

Step 3: In Visuino, Add Components

In Visuino Add Components

In Visuino Add Components

  1. Add "Date/Time Value" component

  2. Add "Decode(Split) Date/Time" component

Step 4: In Visuino, Set Components

In Visuino Set Components

In Visuino Set Components

In Visuino Set Components

In Visuino Set Components

In Visuino Set Components

In Visuino Set Components

In Visuino Set Components

In Visuino Set Components

  1. Select ArduinoUNO R4 WiFi board and in the properties window expand Modules>Display and select Elements and click on the 3 dots button, in the Elements window drag "Text Field" to the left side and in the properties window select "Elements" and click on the 3 dots.

  2. A new Elements window will open. Drag the "Font" element to the left and in the properties, set the font "Adafruit\Picopixel"

  3. Close the "elements" windows

  4. Drag another "Text Field" to the left side and in the properties window set "Y" to 6, select "Elements" and click on the 3 dots.

  5. A new Elements window will open. Drag the "Font" element to the left and in the properties, set the font "Adafruit\Picopixel"

  6. Close all the "elements" windows

  7. Select ArduinoUNO R4 WiFi board and in the properties window expand Modules>Display and set "Orientation" to goRight

  8. Select "DateTimeValue1" and in the properties window set your current time under "Value"

Step 5: In Visuino, Connect Components

imageimageimage

  1. Connect DateTimeValue1 pin [Out] to Arduino Real Time Clock pin [In]

  2. Connect Arduino Real Time Clock pin [Out] to DecodeDateTime1 pin [In]

  3. Connect DecodeDateTime1 pin [Hour] to Arduino Display Text Field1 pin [In]

  4. Connect DecodeDateTime1 pin [Minute] to Arduino Display Text Field2 pin [In]

Step 6: Generate, Compile, and Upload the Arduino Code

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" Tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Step 7: Play

Congratulations! You have completed your project with Visuino. Also attached is the Visuino project that I created for this tutorial. You can download it and open it in Visuino: https://www.visuino.com

Download Visuino file: UNO-R4-Clock.visuino

Número de parte del fabricante ABX00087
ARDUINO UNO R4 WIFI
Arduino
$27.50
Ver más Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.