Maker.io main logo

Harnessing the Power of the Sun with a Solar Garden Light

380

2024-03-07 | By Kitronik Maker

License: See Original Project

Courtesy of Kitronik

Guide by Kitronik Maker

With the world's non-renewable resources being consumed at an alarming rate, it's ‎no surprise that when the new curriculum was released, 2½ years ago, the word ‎‎'environmental' appeared in the key concepts. The programme of study goes on to ‎add that this includes the opportunity to explore issues relating to sustainability. ‎Therefore, teachers are now looking for projects that allow students to consider ‎sustainability, and what better way to do this, than with a solar garden light. This ‎project allows electronic construction, resistant materials, renewable energy, and ‎the study of designers, to be included in one scheme of work.‎

harnessing_1

This product is very similar to the solar garden lights that can be found in garden ‎centres and hardware stores. During the day, a solar panel is used to charge up a ‎rechargeable cell, and then at night, when the light level falls, the LED turns on ‎allowing a path, step, or other feature to be illuminated. The soldering in the project ‎is fairly simple as the circuit uses just 15 components and no ICs. Assuming ‎students have practiced some soldering prior to assembling the board, any key ‎stage 3 class, should find building it relatively straight forward. With the essential ‎job of making the board complete, the rest of the scheme of work can be designed ‎to cover as many areas as time allows. Students can either design an enclosure ‎for the board to go in to, or, alternatively, if time is short, a large jar can be used to ‎house the board. In this case, reuse/recycling can be added to the project.‎

harnessing_2

“The solar garden light is a perfect way to deliver ‎sustainability” Renewable energy can be examined; just as solar, wind, hydro, or ‎any other renewable energy sources could be studied. Math can be included into ‎the project by studying how long it takes to charge the battery. The electronics can ‎be studied in more detail by looking at the components the circuit uses, such as ‎LEDs, resistors, capacitors, and transistors. A case study of product designers or ‎inventors, like Trevor Baylis, who famously designed the wind-up radio, could be ‎included in the project (www.trevorbaylisbrands.com).‎

diagram_3

The circuit diagram (above) shows how the components are connected up to make ‎the solar garden light. The diode allows the battery to be charged during the day ‎and prevents it from discharging through the solar cell at night. The transistor, Q1, ‎turns the rest of the circuit on when it goes dark. Since the LED needs 3.5 Volts, ‎and the cell only delivers 1.2 Volts, some extra circuitry is needed. This turns the ‎LED on for a third of the time, but at 3 times the battery voltage, and, because this ‎happens hundreds of times a second, the human eye thinks the LED is always on. ‎Our solar garden light kit includes the PCB, parts, solar cell, and rechargeable ‎battery. Click here to view ordering information. Learn more about the author read ‎more »‎

‎©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof ‎without Kitronik's prior written consent.

Número de parte del fabricante 2134
SOLAR GARDEN LIGHT WITH BATTERY
Kitronik Ltd.
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.