Maker.io main logo

GPS Geo-Mapping at the Push of a Button

74

2019-11-07 | By SparkFun Electronics

License: See Original Project

Courtesy of SparkFun

Introduction

If you need an intermediate GPS project to tickle your fancy, we've got one ready to go. In a previous tutorial, we slapped some boards together to see our GPS locations on an OLED Screen. It was a great learning experience, but we need something more. Today we'll do some more good 'ol board slappin', and we'll save multiple coordinates in a KML file and take over the world! Okay, not take over, but we can easily see collections of coordinates all over the world with Google Earth.

Required Materials

GPS Tutorial 2 SparkFun Wish List

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview.

qwiic

 We would also recommend taking a look at the following tutorials if you aren't familiar with them.

Hardware Overview

If you followed along with the last GPS tutorial, you'll have an idea of where we're going. However, since we're packing more stuff into a small module, we'll need more power. Unfortunately, the five libraries we'll be using pushes the original RedBoard to its limits. So, to make up the gap, we'll use the SAMD21. Specifically speaking, the SparkFun RedBoard Turbo!

RedBoard Turbo

The Turbo is a relatively new development board, sporting the versatile ATSAMD21G18 ARM Cortex-M0+ microcontroller. It's also carrying an RTC Crystal, WS2812 addressable RGB LED, and a LiPo battery connector with charging capabilities. It's almost TOO powerful for our purposes, but it conveniently has everything we need.

turbo_1

SparkFun RedBoard Turbo - SAMD21 Development Board

MicroSD Shield

The microSD shield is an Arduino Uno layout compatible memory shield. We'll interact with the microSD shield using the SPI bus through the shield's on-board hex converter. Quick note, since the microSD shield is an older component than the Turbo there are some communication bugs, but we'll get to that a little later.

Shield_2

SparkFun microSD Shield

SAM-M8Q Chip Antenna GPS Breakout and Qwiic Micro OLED

It's worth mentioning once more the components carried across from the last tutorial. The SAM-M8Q Chip Antenna GPS provides simple and powerful GPS capabilities from Ublox's GPS systems. Those coordinates are then displayed to the user on the easy to wire, and no solder required, Qwiic Micro OLED screen.

Hardware Hookup

This part of the build will require some assembly (but that's what we're all really here for anyway). Since most of our components carry over from the simple push button GPS tracker tutorial, we only have a few additional parts to assemble. Now, if you're fresh to the GPS tracker projects you don't have to worry. We'll run through all of it again anyway.

Assembly

Push Button Wiring

Our push button will be rather straightforward. The table below shows the connections between the button and our Turbo via the microSD shield.

button_3

Table1_3

These pins will connect to the Turbo pins (via the microSD shield PTH pins) as shown in the fritzing diagram above.

MicroSD Shield

The first step would be to solder our break away headers to the pins aligning with the RedBoard Turbo female headers. We also need to solder the 2x3 Female ISP connector to the bottom of the microSD shield. We'll use that ISP header for a modification needed for communication.

I mentioned earlier that there was a special note for communication between the Turbo and our microSD shield. The best explanation currently is there is a naming difference in libraries and the SERCOM tools used on the Turbo. We can easily circumvent the issue by hardwiring our Digital Pins (13 -11) to the ISP header found on all our RedBoards.

microSDcommunicationsoldering_4

I discovered this issue when I was running a simple datalogger sketch and I kept getting a false return from the SD.begin() call. After making these hotwiring corrections, I got correct functionality.

Once we're done with the headers, we can move on to connecting our pushbutton. Following the table mentioned earlier, we need to solder our wires to the microSD shield. There are PTH holes alongside all the header holes to solder to. We're looking for these specific pins:

pushbuttonpins_5

Table2_6

Reference Diagrams

HookupShield_7

HookupDisplay_8

Optional Assembly

Aluminum Case

We do have an aluminum case added to the required materials list. While it is optional, it provides a sturdy case for practical application purposes. If you purchase the case, then you'll have to make extra modifications. We'll need to drill screw holes and protruding areas for our OLED screen and GPS chip antenna.

case_9

Software Setup

Note: This code/library has been written and tested on Arduino IDE version 1.8.9. Otherwise, make sure you are using the latest stable version of the Arduino IDE on your desktop.

If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

Component Libraries

First let's start with the two libraries for our Qwiic Micro OLED Breakout and SAM-M8Q Chip Antenna GPS Module.

SPARKFUN MICRO OLED LIBRARY (ZIP)

SPARKFUN U-BLOX ARDUINO LIBRARY (ZIP)

Add these libraries using the Include Library option under the Arduino IDE option "Sketch".

Arduino_10

Turbo Specialties

The Turbo does require some extras before we can program. Those are all done through the SAMD Arduino Libraries. Open Tools -> Board: " " -> Boards Manager... and find the following:

board_11

After the main Arduino board files are installed, we'll need the SparkFun specific boards. For those we'll need to copy and paste the following in our Arduino "Additional Boards Manager URLs" preferences. Copy and paste:

https://raw.githubusercontent.com/sparkfun/Arduino_Boards/master/IDE_Board_Manager/package_sparkfun_index.json

Boards_Manager_12

If you need reminders for what you're looking for later down the road, the code in the next section will have all required software components listed in the comments.

Google Earth and KML

Off the bat, if you need to download Google Earth. See you in a minute, no worries.

With that out of the way, KML is starkly different from the Arduino C or MicroPython we usually see here. It’s very similar to HTML used for websites. If you’re not familiar with the Hyper Text Markup Language, don’t worry because I’ll give you a rough (and I mean rough) overview of what we’re trying to achieve with it.

HTML

HTML mostly is a file with text (or images, or videos, or whatever black magic websites use nowadays) that is formatted using sectioning tags. Tags act like boxes, what’s in a box is owned by the box.

For example, in our code, we’ll see a tag called Placemark. In Google Earth, we will see our placemarks as yellow pins on the globe. If we save a placemark as follows:

Copy Code
<placemark>
    <Point>
        <coordinates> 12.345678, 123.456789 </coordinates>
    </Point>
</placemark>

Then we’ve made a box called placemark with the GPS values inside. When Google Earth reads this a yellow pin will be placed on that exact coordinate. There are many more useful tags and tools for KML files. If you want to dive deeper, please feel free to visit the Google Developers page for KML. All of that is, in essence, what we’re trying to achieve.

Example Code

The code below is nothing fancy and doesn't have clever algorithms. There are many places within that can be improved for performance and efficiency. My hope was to allow a novice programmer to read and understand the big picture of what we're trying to do. From there improvements can and should be made!

Feel free to download the code from the GitHub location, or by clicking on the button below:

DOWNLOADING GPS TRACKER TUTORIAL EXAMPLE CODE

Alternatively, you can copy and paste the code from here:

Copy Code
/******************************************************************************
Google Earth KML GPS Position Logger v1.6
brandon.williams@sparkfun.com
May 6, 2019

The user will press a momentary button to log a GPS location into a KML file, 
a file that's stored on a microSD card in the microSD shield. If the user holds 
the button for 5 seconds, the program will effectively "end" with an infinite 
while loop after safely closing the file. The user can then remove the memory 
card to retrive the file and open using Google Earth.

** Significant changes and improvements can be made, please enjoy mod-ing! **

Resources:
SFE MicroOLED library: SFE_MicroOLED.h
SFE Ublox GPS library: http://librarymanager/All#SparkFun_Ublox_GPS 
Arduino SD required libraries: SPI.h & SD.h

Download Google Earth: https://www.google.com/earth/versions/

Development environment specifics:
Arduino IDE 1.8.9
Board Definition Packages:
  Arduino SAMD board Boards (32-bits ARM Cortex-M0+) 1.6.21
  SFE SAMD Boards 1.6.1
******************************************************************************/
//SD Shield libraries
#include <SPI.h>
#include <SD.h>
//OLED and Ublox libraries
#include <Wire.h>
#include <SFE_MicroOLED.h>
#include "SparkFun_Ublox_Arduino_Library.h"

#define PIN_RESET 9   //OLED
#define DC_JUMPER 1   //OLED

//create objects
SFE_UBLOX_GPS myGPS;
MicroOLED oled(PIN_RESET, DC_JUMPER);
File dataFile;

//declare golbal variables
const int buttonPin =  2;
const int chipSelect = 8; //Specific for SFE microSD shield, differs from Arduino SD libraries
int buttonState = 0;

void setup() {

  Wire.begin();

  //Classic SFE flame
  oled.begin();
  oled.clear(ALL);
  oled.display();
  delay(500);
  oled.clear(PAGE);
  oled.display();
  oled.setFontType(0);
  oled.setCursor(0,0);

  pinMode(buttonPin, INPUT_PULLUP);

  pinMode(chipSelect,OUTPUT);

  if(!SD.begin(chipSelect)){
    //If the SD card can't be initiallized/found just freeze with a loop
    oled.setCursor(0,0);
    oled.clear(PAGE);
    oled.print("SD, no work");
    oled.display();
    while(1);
  }
  oled.setCursor(0,0);
  oled.clear(PAGE);
      //Oh yea! don't forget the GPS shield needs to get it's first fix
  oled.print("Revving up the GPS unit, please wait");
  oled.display();
  delay(29000);
  oled.setCursor(0,0);
  oled.clear(PAGE);
  oled.print("Ready to start!");
  oled.display();
  oled.clear(PAGE);
  oled.display();

}

void loop() {
  double latitude;
  double longitude;

  // A little redundant, but simple fix to not add on to the file 
  SD.remove("sparkGPS.kml");

  dataFile = SD.open("sparkGPS.kml", FILE_WRITE);

  if (dataFile){
    //Write opening tags to file
    dataFile.println("<?xml version=\"1.0\" encoding=\"UTF-8\"?>");
    dataFile.println("<kml xmlns=\"http://www.opengis.net/kml/2.2\">");
    dataFile.println("<Document>");
    int state = 0;
    myGPS.begin();
    /* "Continous" (not quite) loop will run until user performs kill action.
     *  
     *  1. Button is pushed and released, then one coordinate 
     *  point will add to the file
     *  
     *  2. If the button is pushed and held, one last coordinate is saved. 
     *  Hold button till "Goodbye" appears to kill the loop. File is 
     *  closed and it is safe to remove power
     *  and remove the SD card.
     */
    while(state < 4){
      buttonState = digitalRead(buttonPin);
      state = 0;
      if(buttonState == LOW){
        oled.setCursor(0,0);
        oled.clear(PAGE);
        oled.print("button pressed");
        oled.display();
        delay(1000);
        oled.clear(PAGE);
        oled.display();

        state = 1;
        delay(900);
        if(buttonState == LOW){

          oled.setCursor(0,0);
          oled.clear(PAGE);
          oled.print("Getting Coordinates");
          oled.display();
          delay(1000);
          oled.clear(PAGE);
          oled.display();

          float latitude = myGPS.getLatitude();
          latitude = latitude / 10000000;

          float longitude = myGPS.getLongitude();
          longitude = longitude / 10000000;


          dataFile.println("\t<Placemark>");
          dataFile.println("\t\t<name>SFE GPS Extravaganza</name>");
          dataFile.println("\t\t<description>Where am I?</description>");
          dataFile.println("\t\t<Point>");
          dataFile.print("\t\t\t<coordinates>");
          dataFile.print(longitude,6);
          dataFile.print(",");
          dataFile.print(latitude,6);
          dataFile.print(",0");
          dataFile.println("</coordinates>");
          dataFile.println("\t\t</Point>");
          dataFile.println("\t</Placemark>");
          //Visual coordinates for the user to see
          oled.clear(PAGE);
          oled.setCursor(0,0);
          oled.print("Lat:");
          oled.print(latitude,6);
          oled.print("\nLong:");
          oled.print(longitude,6);
          oled.display();
          delay(1500);
          oled.clear(PAGE);
          oled.display();
        }
        buttonState = digitalRead(buttonPin);
        if(buttonState == LOW && state == 1){
          state = 2;
          delay(4000);
          buttonState = digitalRead(buttonPin);
          if(buttonState == LOW && state == 2){
            dataFile.println("</Document>");
            dataFile.println("</kml>");
            dataFile.close();
            oled.setCursor(0,0);
            oled.print("Goodbye");
            oled.display();
            delay(1000);
            oled.clear(PAGE);
            oled.display();
            //it is safe to remove power and remove data
            while(1); //"Ends program" more or less
          }

        }

      }
    }
  }
}

Upload the code using your Arduino IDE, and with any luck you'll start seeing coordinates across your OLED screen!

Resources and Going Further

GPS is a great technology for anyone to have in their back pocket. Thanks to the size of my enclosure, I literally have it in my back pocket. In all seriousness, this was a great project. It builds on good engineering principles and processes, teaches new technologies and platforms, as well as pushes ourselves out of our comfort zones just far enough. Thank you and I hope you can track your progress as much as I have!

Número de parte del fabricante 14812
REDBOARD TURBO ATSAMD21G18 EVAL
SparkFun Electronics
$23.56
Ver más Details
Número de parte del fabricante 12761
SPARKFUN MICROSD SHIELD
SparkFun Electronics
$17.95
Ver más Details
Número de parte del fabricante 11375
HOOK-UP WIRE ASSORT STRAND 22AWG
SparkFun Electronics
$25.85
Ver más Details
Número de parte del fabricante 10512
BATTERY HOLDER 9V BARREL PLUG
SparkFun Electronics
Número de parte del fabricante 6LF22XWA/B
BATTERY ALKALINE 9V
Panasonic Energy
Número de parte del fabricante 15210
SPARKFUN GPS BREAKOUT - CHIP ANT
SparkFun Electronics
$43.95
Ver más Details
Número de parte del fabricante 14532
QWIIC MICRO OLED BREAKOUT
SparkFun Electronics
$18.50
Ver más Details
Número de parte del fabricante 14426
QWIIC CABLE - 50MM
SparkFun Electronics
More Info
Ver más Details
Número de parte del fabricante 13839
STOMP BOX ALUM 4.41"L X 2.4"W
SparkFun Electronics
Número de parte del fabricante HDR100IMP40M-G-V-TH
CONN HEADER VERT 40POS 2.54MM
Chip Quik Inc.
Número de parte del fabricante AP8GMCSH4-B
MEMORY CARD MICROSD 8GB CLASS 4
Apacer Memory America
$85.33
Ver más Details
Número de parte del fabricante 11968
METAL PUSHBUTTON - MOMENTARY (16
SparkFun Electronics
$11.19
Ver más Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.