Maker.io main logo

Getting Started with NVMe Base Duo for Raspberry Pi 5

395

2024-06-27 | By Pimoroni

License: See Original Project Raspberry Pi SBC

Courtesy of Pimoroni

Guide by Pimoroni

About NVMe Base Duo

NVMe Base Duo lets you connect up two large NVMe solid state drives (SSD) ‎to the PCIe (that's 'Peripheral Component Interconnect Express') connector ‎on Raspberry Pi 5 for oodles of fast storage.‎

You could use one drive to store your data and one to store incremental ‎backups, or you could get really fancy and use both drives to set up a RAID ‎array. Read on to find out how to put it together!‎

What You'll Need

If you're planning on sourcing your own NVMe SSD, then bear in mind the ‎following:‎

  • The SSD needs to be NVMe M.2. Don't get this confused with SATA ‎M.2 drives which sometimes look similar but are not compatible. NVMe ‎and SATA refer to the interface communications standards, and M.2 to ‎the form factor.‎

  • Duo can take SSDs of physical sizes between 2230 and 2280 (the ‎numbers refer to the size of the board - i.e., 22mm wide by 30mm to ‎‎80mm long).‎

There is a list of SSDs that we've tested with Duo on the shop page.‎

Note that currently you cannot boot from NVMe drives installed on NVMe ‎Base Duo. We hope the Raspberry Pi firmware will support this in the future, ‎but for now, it can only boot from drives that are the root device on the PCIe ‎Bus. i.e., not behind a packet switcher/multiplexer.‎

Putting It Together

The kit contains the following:‎

kit_1

  • A NVMe Base Duo PCB.

  • A flexible ribbon cable with writing on one side.

  • Four sticks on rubber feet.

  • A standoff set.‎

If you purchased a bundle that includes SSDs then you will also have:‎

• Two 250GB or 500GB NVMe drives.‎

ATTACHING THE STANDOFFS TO THE DUO

Inside the standoff set, you will find:‎

  • Four long M2.5 hex standoffs, for attaching the base to your Pi

  • Eight short M2.5 screws

  • Four long M2.5 screws

  • Two short M2 hex standoffs for mounting the drives

  • Four teeny tiny M2 screws

‎(You may also have a few spares!)‎

If you're missing anything, drop support a line (please do double check the ‎bag before you do though, the ribbon cables in particular like to hide in the ‎corners).‎

STANDARD BASE ASSEMBLY

Attach the long standoffs to the top of the base with four of the short M2.5 ‎screws.

Base Assembly

 

ALTERNATE BASE ASSEMBLY (WITH HAT)‎

If you are planning on mounting a HAT (or other hardware) on top of your Pi 5, ‎you might find it useful to use the longer screws.‎

Attach the long standoffs to the top of the base with four of the long M2.5 ‎screws. The screw thread will poke out of the top of the standoff, providing ‎some handy mounting points that you can attach your HAT's standoffs to.

Base Assembly

THE RIBBON CABLE

We suggest connecting the ribbon cable to the base next before you attach ‎anything else to it.‎

One end of the cable is wider and is labelled ADDON - this is the end which ‎goes into the connector on the base. The other end (labelled RPI 5) goes into ‎the Raspberry Pi 5's PCIe connector.

cable_4

When the Base is in its final position, the writing and Pirate logo will face ‎outwards.‎

ATTACHING THE RIBBON CABLE TO THE BASE

The ribbon cable connectors have small plastic clips which you have to 'open' ‎to put the ribbon in, and close again to secure it in place. These clips require ‎very little pressure to move and are quite fragile, so it's worth being careful ‎with them.‎

Note that the clips on the base and the Raspberry Pi work slightly ‎differently from each other!‎

Using tweezers or a fingernail, flip the grey clip of the one of the sockets on ‎the base upwards. It will swivel into an upright position.

Attaching Ribbon Cable

Now gently push the ADDON end of the ribbon cable into the socket, ensuring ‎the side with the writing is pointing downwards. You should see the cable go ‎underneath the line of silver prongs.‎

Attaching Ribbon Cable

Gently rotate the clip back down into its original position. Check that this end ‎of the cable is nice and square in the connector, it will be tricky to adjust it ‎later when the drives are in place.

Attaching Ribbon Cable

ATTACHING THE SSDS

Next, we'll attach the small standoffs that hold the drives in place. Take one ‎of the tiny M2 screws and post it through one of the small holes running ‎down the middle of the board, from the bottom. Use the hole which ‎corresponds to the length of your SSD (2280 if you're using one of our SSDs). ‎Secure it in place with one of the short standoffs.‎

Repeat this process for the second small standoff.

Attaching the SSDS

Unpack your SSD, being careful to avoid touching any of the gold connectors ‎on the end.‎

You will notice a notch breaking up the connectors on one end of the SSD. ‎This is the end which fits into the socket on the base.‎

ssd_9

There is a round semicircular cutout in the middle of the other end. This will ‎sit on top of the short standoff and is where you will secure the SSD to the ‎base.‎

Now carefully push the SSD into the socket. It will only go in one direction ‎and doesn't need much effort.

socket_10

Gently push the SSD down at the other end and secure it in place by ‎screwing another tiny M2 screw into the short standoff.‎

ATTACHING THE SSDS

If you have a second drive to attach, repeat this process!‎

ATTACHING THE RIBBON CABLE TO THE RASPBERRY PI 5‎

Ensure your Raspberry Pi 5 is not powered on!‎

Locate the Raspberry Pi 5 PCIe connector - it is located next to the Pi's on/off ‎switch. It has a brown clip which slides up and down, at right angles to the ‎Raspberry Pi board.‎

switch_12

Carefully lift the clip up by about 1mm.‎

With the Raspberry Pi on your desk, hold your base directly above the Pi's ‎PCIe connector with the SSD pointing away from the Pi.‎

place_13

Gently lower the Base, posting the ribbon into the PCIe connector until you ‎feel that it has gone as far as it can. With your thumb nail or tweezers, push ‎the brown clip down and back in place.‎

FINAL ASSEMBLY

Now is a good time to plug in the SD card to your Pi, before the ribbon cable ‎gets in the way of the slot. If you don't already have a microSD card with ‎Raspberry Pi OS written to it, you can create one using Raspberry Pi ‎Imager (it's available for Windows, macOS and Linux).‎

Now that the two boards are connected, fold the base down under the ‎Raspberry Pi as though the ribbon cable is a hinge. Make sure you don't put ‎the ribbon under any strain.‎

With the Raspberry Pi sitting on top of the base, use the four remaining short ‎screws to secure the Raspberry Pi 5 on top of the base's spacers.‎

spacers_14

If you used the long screws to attach the standoffs, post the long screws ‎through the four mounting holes of the Pi, and then screw the HAT's spacers ‎onto the threads.‎

Finally (and optionally) stick the four rubber feet onto the bottom of the base, ‎one near each corner.‎

Updating Everything

If you're working with NVMe drives, you'll want to be using the most recent ‎version of Raspberry Pi OS (and the bootloader firmware) on your Pi 5.‎

You can update both by opening up a terminal (Ctrl-Alt-T, or find it in the Pi ‎OS menus) and typing the following:‎

Copy Code
sudo apt update
sudo apt upgrade

Once you've finished updating and upgrading, you should then reboot your Pi:‎

Copy Code
sudo reboot

For NVMe drives to play nicely with Pi 5, your bootloader firmware should be ‎dated newer than December 2023. The commands above should have ‎updated it for you, but if you'd like to double check you can enter:‎

Copy Code
sudo rpi-eeprom-update

If it is not post-December 2023, you can update it using the Raspberry Pi ‎Configuration utility (sudo raspi-config > Advanced Options > Bootloader Version).‎

Checking Base Installation

To check that the ribbon cable has been connected correctly and the SSD ‎installed properly, open a Terminal window and type:‎

lsblk

This will show you a list of all the drives available on your Pi - if your drives ‎are successfully connected, there should be entries ‎under nvme0n1 and/or nvme1n1.‎

devices_15

If your drives aren't showing up, turn off your Raspberry Pi and recheck the ‎ribbon cable connections and the SSD installation. Remember that the clips ‎on the base and on your Raspberry Pi 5 both need to be folded/pressed back ‎in place for the connections to work.‎

Next Steps

You should now have a Raspberry Pi 5 with lots of extra capacity to store all ‎your lovely data!‎

We love to see what you're making - drop us a line on Twitter/X (@pimoroni), ‎Bluesky (@pimoroni.com) or other social media and let us know what you are ‎getting up to with Duo.‎

That's all folks!

Número de parte del fabricante SC1153
27W USB-C PSU UL(US), WHITE
Raspberry Pi
$12.00
Ver más Details
Número de parte del fabricante SC1148
HEATSINK ALUMINUM
Raspberry Pi
Número de parte del fabricante SC1432
SBC 2.4GHZ 4 CORE 8GB PI 5
Raspberry Pi
$175.00
Ver más Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.