Maker.io main logo

Getting Started with Clipper HAT Mini

410

2025-05-08 | By Pimoroni

License: See Original Project Single Board Computers Raspberry Pi SBC

Courtesy of Pimoroni

Guide by Pimoroni

Clipper HAT Mini is a straightforward way of giving your Raspberry Pi the power to chat with ‎‎4G LTE mobile/cellular networks. This guide will show you how to set it up!‎

What You'll Need

  • A Clipper HAT Mini. These instructions should also work if you're using a Clipper ‎breakout with your Raspberry Pi, but you'll have to figure out your own wiring.‎

  • A data-capable SIM card

  • An antenna

Assembly

Connect the antenna, insert the SIM, and press the HAT firmly down onto your Pi's 40-pin ‎header. Here's what that looks like on a Raspberry Pi Zero 2 W:‎

antenna_1

If you wanted to fasten the HAT in place securely, you could add a couple of these 10mm ‎standoffs.‎

Here's what it looks like on a Raspberry Pi 5 that's fully loaded with an Active ‎Cooler and NVMe Base. We've used some extended 17mm standoffs and a booster ‎header to make enough of a gap for the cooler.‎

cooler_2

cooler_3

You'll need to be running Raspberry Pi OS (Desktop or Lite) on your Pi. If you choose Lite, ‎we'll assume you're a Linux wizard and can work around any hiccups in these instructions.‎

Configure Serial

Fire up your Pi, the NET and STATUS lights on your Clipper should light up and the NET light ‎should start blinking.‎

Open a Terminal (Ctrl-Alt-T or find it in the Raspberry Pi OS menus). Alternatively, you could ‎SSH in from another computer if that's your preference.‎

serial_4

Run:‎

Copy Code
sudo raspi-config

And select Interface Options -> Serial Port.‎

options_5

Say NO to enabling the login shell at startup and YES to enabling the serial port.‎

Exit, and reboot so your serial port configuration takes effect.‎

Initial Test

Now let's check things are connected and working properly.‎

Once again, open a Terminal (or SSH in) and install minicom:‎

Copy Code
sudo apt install minicom

And then connect to your Clipper HAT:‎

On a Pi 5, that looks like this:‎

Copy Code
minicom -b 115200 -D /dev/ttyAMA0‎

If you're using a different version of Pi, you may need to do:‎

Copy Code
minicom -b 115200 -D /dev/ttyS0‎

Now you should be able to type "AT" and hit Enter.‎

If everything is working, you should see an "OK" response pop up in minicom!‎

minicom_6

Press Ctrl+A and then X and select "Yes" to leave minicom. It's time to enable PPP!‎

Setting Up PPP

You know the routine, open up a terminal (it's open from the last step, right?) and copy the ‎reference configuration to a new clipper config like so:‎

Copy Code
sudo cp /etc/ppp/peers/provider /etc/ppp/peers/clipper‎

Edit your new config:‎

Copy Code
sudo nano /etc/ppp/peers/clipper

In nano you'll want to:‎

  1. ‎Pop an # before the user line to comment it out, we won’t need this!‎

  2. On the 'connect' line, replace pap with gprs.‎

  3. On this same line, replace the ******* with your apn, for our 1nce sim this would ‎be iot.1nce.net.‎

  4. Change /dev/modem to /dev/ttyAMA0 (or /dev/ttyS0).‎

  5. At the end of the file, add the line nocrtscts to disable hardware flow control (RTS, ‎and CTS)‎.

  6. Add the line local to disable modem control lines (CD, and DTR)‎.

That's everything, press Ctrl+X to exit nano and 'Y' to save your chances, it's time to test ‎PPP!‎

test_7

Enabling & Testing PPP

Still in your Terminal (or SSH session) fire up Clipper with the following command:‎

Copy Code
sudo pon clipper

If you wish, you can list all the available network interfaces with ifconfig.‎

list_8

Finally test your connection to the internet with:‎

Copy Code
ping -I ppp0 1.1.1.1‎

This will ensure your ping attempt is routed via PPP rather than any other network ‎connection you might be using.‎

This might take a minute or so to start returning results. If it takes a while, try moving your ‎antenna and making sure you're in a good signal position.‎

signal_9

Troubleshooting

unrecognized option '/dev/ttyAMA0' when running sudo pon clipper

This is the Clipper configuration looking for a specific serial port, make sure serial is ‎enabled and use ls /dev/tty* to check it's available.‎

That's all folks!

Número de parte del fabricante SC1176
SBC 1.0GHZ 4 CORE 512MB RAM
Raspberry Pi
$15.00
Ver más Details
Número de parte del fabricante SC1113
SBC 2.4GHZ 4 CORE 16GB PI 5
Raspberry Pi
$305.00
Ver más Details
Número de parte del fabricante SC1148
HEATSINK ALUMINUM
Raspberry Pi
Número de parte del fabricante PIM699
NVME BASE FOR RASPBERRY PI 5
Pimoroni Ltd
$15.75
Ver más Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.