Maker.io main logo

DIY Arduino VFO with AD9850 & TM1638 Pure Sine Wave Signal Generator for

99

2026-04-06 | By Mirko Pavleski

License: General Public License Arduino

A Variable Frequency Oscillator (VFO) is an electronic circuit that generates a signal at a tunable, adjustable frequency, essential for controlling the operating frequency in radio transmitters and receivers. So far, in several of my previous videos, I have shown you how to make such a device using the Si5351 clock generator. This time, I will explain how to make a VFO, but now with the AD9850 Signal Generator Module.

The AD9850 chip generates a pure sine signal in the range from 0 to 40 MHz. The Si5351 is indeed more advanced and cheaper, but at the output, it generates a rectangular signal rich in harmonics, which in the receiver generates non-existent image signals, which means we listen to the same radio station on multiple receiving frequencies.

hyugf

In that sense, the AD9850 is superior because it generates a pure sine signal that has a much smaller number of harmonics and is very suitable for use in local oscillators of HF radio devices. This time, to display the generated frequency, I will use the TM1638 module, which is ideal for this purpose, combining an 8-digit 7-segment display, 8 LEDs, and 8 buttons, all controlled via only 3 digital pins.

ghf

The 7-segment LED numbers give the entire device a nice retro feel. The module is also compact and well-made, so it can be used directly on the front of the box, greatly simplifying the construction of the device.

Now let's take a look inside and see what components this device contains.

- first, there's the AD98500 module,

- Arduino Nano microcontroller board,

- a rotary encoder,

- and the previously mentioned TM1638 module.

hk

You can see two more components mounted on heat sinks and an additional assembly with two transistors on the PCB. The assembly is a Buffer Amplifier that raises the signal level from 1 to 5Vpp. This one is an LM317 stabilizer and provides 9V for the buffer circuit, and the other one is a 7805 linear stabilizer through which the AD98500 module is powered. I made these additional modifications for the needs of one of my devices with special requirements; otherwise, the assembly without these modifications is quite sufficient, using a direct 5V power supply. You can also see the schematic of the buffer amplifier below.

mnk

Now let's see how the device works in real conditions. Immediately after turning on, the display shows the default frequency that was previously entered in the code. With the rotary encoder, we can change this frequency in steps of 1kHz. On the first button, we can change this step to 10Hz, 100Hz, 1kHz, 10kHz, and 100kHz. On the second button, the modulation type AM, USB, or LSB is changed. The next 5 buttons are used to directly activate one of the 5 most used HF Bands successively. (1.8, 3.5, 7,...). It is important to note that we can continuously change the frequency from one band to another, so this also includes broadcast frequencies. The last button has a function when using this VFO with Superheterodyne receivers with an IF of 455KHz. Namely, by activating this option, the actual output signal is 455KHz higher than the one shown on the display. The eight LEDs at the top signal which of the options is currently active. Another very useful feature is the ability to change the intensity of the display and LED lighting. By pressing the encoder button, we enter a mode where the display brightness can be changed from 0 to 100%. This is very useful in conditions of work at night, which is the most common case in reality.

kljk

To verify what I've said so far, we'll connect the output of this VFO to an oscilloscope to see the shape of the signal.

And finally, a short conclusion: The AD9850-based VFO provides a clean, sine-wave alternative to square-wave oscillators, ensuring your HF receiver remains free from unwanted harmonic interference. With the TM1638 interface, it offers a functional, retro-styled control center perfect for any homebrew radio build.

ghju

Copy Code
// by mircemk Mar.2026

#include <TM1638lite.h>

TM1638lite module(4, 3, 2); 

#define W_CLK 8
#define FQ_UD 9
#define DATA 10
#define RESET 11
#define ENC_A A0
#define ENC_B A1
#define ENC_SW A2 // Копчето на енкодерот

unsigned long freq = 7000000; 
unsigned long steps[] = {10, 100, 1000, 10000, 100000, 1000000};
int stepIndex = 2; 
const char* modes[] = {"A       ", "USB     ", "LSB     "};
int modeIndex = 0;
long offset = 0; 
bool offsetActive = false;

// Brightness контроли
int brightnessPercent = 50; // Почетна на 50%
bool brightnessMode = false;

unsigned long tempDisplayTimer = 0;
bool showingTemp = false;

const byte segmentMap[] = { 0x3F, 0x06, 0x5B, 0x4F, 0x66, 0x6D, 0x7D, 0x07, 0x7F, 0x6F };

void setup() {
  pinMode(W_CLK, OUTPUT); pinMode(FQ_UD, OUTPUT);
  pinMode(DATA, OUTPUT);  pinMode(RESET, OUTPUT);
  pinMode(ENC_A, INPUT_PULLUP); 
  pinMode(ENC_B, INPUT_PULLUP);
  pinMode(ENC_SW, INPUT_PULLUP);
  
  ad9850_reset();
  updateDDS(freq + offset);
  setBrightnessLevel(brightnessPercent);
  updateMainDisplay();
}

void loop() {
  // Читање на копчето на енкодерот (A3)
  if (digitalRead(ENC_SW) == LOW) {
    brightnessMode = !brightnessMode;
    if (brightnessMode) showTempMsg("BRIGHT  ");
    else updateMainDisplay();
    delay(300); // Debounce
  }

  uint8_t buttons = module.readButtons();

  // Додека сме во Brightness Mode, другите тастери се деактивирани
  if (!brightnessMode) {
    if (buttons == 1) { 
      stepIndex = (stepIndex + 1) % 6;
      char buffer[9];
      sprintf(buffer, "S%7ld", steps[stepIndex]); 
      showTempMsg(buffer);
      while(module.readButtons() == 1); 
    }
    if (buttons == 2) {
      modeIndex = (modeIndex + 1) % 3;
      showTempMsg(modes[modeIndex]);
      while(module.readButtons() == 2);
    }
    if (buttons == 4)   setBand(1800000, 2); 
    if (buttons == 8)   setBand(3500000, 3); 
    if (buttons == 16)  setBand(7000000, 4); 
    if (buttons == 32)  setBand(14000000, 5); 
    if (buttons == 64)  setBand(21000000, 6); 

    if (buttons == 128) {
      offsetActive = !offsetActive;
      offset = offsetActive ? 455000 : 0;
      showTempMsg(offsetActive ? "_455_   " : "OFF     ");
      module.setLED(7, offsetActive ? 1 : 0); 
      updateDDS(freq + offset);
      while(module.readButtons() == 128);
    }
  }

  // Енкодер логика (за Фреквенција или за Brightness)
  static int lastA = HIGH;
  int currentA = digitalRead(ENC_A);
  if (currentA != lastA && currentA == LOW) {
    if (brightnessMode) {
      // Менување на осветленост (чекор по 10%)
      if (digitalRead(ENC_B) == LOW) brightnessPercent -= 10;
      else brightnessPercent += 10;
      brightnessPercent = constrain(brightnessPercent, 0, 100);
      
      setBrightnessLevel(brightnessPercent);
      char brBuf[9];
      sprintf(brBuf, "BR  %3d ", brightnessPercent);
      module.displayText(brBuf);
    } else {
      // Стандардна фреквенција
      if (digitalRead(ENC_B) == LOW) freq -= steps[stepIndex];
      else freq += steps[stepIndex];
      freq = constrain(freq, 0, 49999999);
      updateDDS(freq + offset);
      if (!showingTemp) updateMainDisplay();
    }
  }
  lastA = currentA;

  if (showingTemp && (millis() > tempDisplayTimer) && !brightnessMode) {
    showingTemp = false;
    updateMainDisplay();
  }
}

void showTempMsg(const char* msg) {
  module.displayText(msg);
  tempDisplayTimer = millis() + 1000;
  showingTemp = true;
}

void setBrightnessLevel(int percent) {
  // TM1638 користи 0x88 (минимум) до 0x8F (максимум) за осветленост
  byte level = map(percent, 0, 100, 0, 7);
  digitalWrite(4, LOW); // STB
  shiftOut(2, 3, LSBFIRST, 0x88 + level); 
  digitalWrite(4, HIGH); // STB
}

void updateMainDisplay() {
  unsigned long tempFreq = freq;
  for (int i = 7; i >= 0; i--) {
    byte segs = 0;
    if (tempFreq > 0 || i == 7) { 
      segs = segmentMap[tempFreq % 10];
      tempFreq /= 10;
    } else {
      segs = 0x00; 
    }
    if (i == 1 || i == 4) segs |= 0x80; 
    sendRawData(i, segs);
  }
}

void sendRawData(byte position, byte data) {
  digitalWrite(4, LOW);
  shiftOut(2, 3, LSBFIRST, 0xC0 + (position * 2));
  shiftOut(2, 3, LSBFIRST, data);
  digitalWrite(4, HIGH);
}

void setBand(unsigned long f, int ledIndex) {
  freq = f;
  for (int i = 0; i < 7; i++) module.setLED(i, 0); 
  module.setLED(ledIndex, 1); 
  updateDDS(freq + offset);
  updateMainDisplay();
}

void ad9850_reset() {
  digitalWrite(W_CLK, LOW); digitalWrite(FQ_UD, LOW);
  digitalWrite(RESET, LOW); digitalWrite(RESET, HIGH); digitalWrite(RESET, LOW);
}

void updateDDS(unsigned long f) {
  unsigned long tuning_word = f * 4294967296ULL / 125000000;
  for (int i = 0; i < 32; i++) {
    digitalWrite(DATA, tuning_word & 0x01);
    digitalWrite(W_CLK, HIGH); digitalWrite(W_CLK, LOW);
    tuning_word >>= 1;
  }
  for (int i = 0; i < 8; i++) {
    digitalWrite(DATA, LOW);
    digitalWrite(W_CLK, HIGH); digitalWrite(W_CLK, LOW);
  }
  digitalWrite(FQ_UD, HIGH); digitalWrite(FQ_UD, LOW);
}
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.