Maker.io main logo

Color-sensor Driven NeoPixel Dress

47

2022-11-01 | By Adafruit Industries

License: See Original Project Wearables Gemma

Courtesy of Adafruit

Guide by Irete Hamdani

Overview

Here's a Halloween costume that includes a whole lot of LEDs and a ‎color sensor that determines the colors of those LEDs. The costume ‎is made up of detachable elements that can be added to any dress, ‎skirt, or other piece of clothing.‎

dress_1

Parts List

And for the garments:‎

  • ‎1 x Black Dress

  • ‎1 x Petticoat

  • ‎1 x Black Sash Belt

Initial Setup

setup_2

For setting up the wiring and initial code, the image above shows ‎an Adafruit NeoPixel Ring instead of the LED strips. In the code, it's ‎just a matter of setting the number of LEDs.‎

The Adafruit NeoPixel LED Dots Strands come with black plastic ‎connectors. You can take the end connector, clip it off of the last ‎strand and use it to connect the first strand to the ‎microcontroller. This guide gives a good explanation on how to do ‎this properly. ‎

You'll also have 2 additional wires coming out of the female ‎connectors, you can clip them for all of the strands, they won't be ‎needed in this project.‎

Wiring

Start with alligator clips, sewing will come later.‎

From the NeoPixels to the Gemma, using the pins on the right side ‎of the Gemma, you connect:‎

  • Top strand to GND

  • Middle strand to D1

  • Red (bottom) strand to the Vout

From the Gemma to the Color Sensor, using mostly the pins on the ‎left side of the Gemma, you connect:‎

  • SCL (A1/D2) to SCL

  • SDA (A2/D0) to SDA

  • 3Vo to 3V

  • GND (on the right side) to GND

In the end, you've should have 2 connections to GND on the Gemma ‎‎- one from the LED strand(s) and one from the color sensor. And one ‎connection per each of the other Gemma pins.‎

You also connect the USB connector for uploading the code and later ‎the battery instead of the USB.‎

Coding

Download the Arduino IDE and the required libraries:‎

  1. ‎FastLED

  2. Color Sensor TCS34725‎

The attached code can work as is. There are a few lines you may ‎consider changing:‎

1. ‎This project used 9 strands of 20 LEDs, total of 180 LEDs. If you ‎use a different amount, change the number in this line of code:‎

‎#define NUM_LEDS 180 // Change this to reflect the number of LEDs ‎you have

2. While working on the project, the lights might be too bright, if ‎so, reduce the number in this line of code. 255 is the maximum ‎for brightness:

‎#define BRIGHTNESS 255 // Set Brightness here 255

3. In the setup, the following code makes one of the LEDs blink 3 ‎times to let you know that the color sensor is ready to read a ‎color value. For this project, it made sense to light up LED #17 ‎since it was closest to the microcontroller in the layout. You can ‎choose the first LED instead. The counter starts with 0, so ‎change the below to leds[0]. Also, you can change the color of ‎the blinking light. In this code, it goes from Black to White ‎making it blink White.‎

‎Download File

Copy Code
for (int i=0; i<3; i++){ //this sequence flashes the first pixel three times none/white as a countdown to the color reading.
&nbsp; &nbsp; leds[16] = CRGB::Black;&nbsp;
&nbsp; &nbsp; FastLED.show();&nbsp;
&nbsp; &nbsp; delay(1000);
&nbsp; &nbsp; leds[16] = CRGB::White;&nbsp;
&nbsp; &nbsp; FastLED.show();&nbsp;
&nbsp; &nbsp; delay(500);
&nbsp; }

The rest of the code is pretty much a combination of FastLED ‎sample code and Color Sensor code.‎

In this project, it is set it up so that on restart the color sensor reads ‎the color and the skirt fills up with a transition gradient of that color ‎until the next reset. Similar to the Adafruit Chameleon Scarf project. ‎You can also set it up so that it fires off the color sensor every x ‎second and changes the lights according to the color it picks up. This ‎can be achieved by moving the code starting from tcs.begin(); from ‎the setup() function to the loop() function and doing some ‎modifications. ‎

Download the code by clicking the "Download Project Bundle" ‎button below or via the link here.‎

To upload code, you need to quickly double press the reset button on ‎the Gemma. You know it's uploading if the green and red lights on ‎the Gemma are on.‎

Download File

Copy Code
// SPDX-FileCopyrightText: 2021 Irete Hamdani for Adafruit Industries
//
// SPDX-License-Identifier: MIT
//
#include <FastLED.h>
#include <Wire.h>
#include "Adafruit_TCS34725.h"

#define DATA_PIN   1
#define LED_TYPE    WS2812B
#define COLOR_ORDER GRB
#define NUM_LEDS    180     // Change this to reflect the number of LEDs you have
#define BRIGHTNESS  255     // Set Brightness here 255

CRGB leds[NUM_LEDS];
 
// color sensor
// our RGB -> eye-recognized gamma color
byte gammatable[256];
//used to store color sensor received color
uint16_t clear, red, green, blue;

// color sensor
Adafruit_TCS34725 tcs = Adafruit_TCS34725(TCS34725_INTEGRATIONTIME_50MS, TCS34725_GAIN_4X);

void setup() {
  delay(3000); // 3 second delay for recovery

  // tell FastLED about the LED strip configuration
  FastLED.addLeds<LED_TYPE,DATA_PIN, COLOR_ORDER>(leds, NUM_LEDS)
    .setCorrection(TypicalLEDStrip) // cpt-city palettes have different color balance
    .setDither(BRIGHTNESS < 255);
 
  // set master brightness control
  FastLED.setBrightness(BRIGHTNESS);

  tcs.begin();

  // helps convert RGB colors to what humans see
  for (int i=0; i<256; i++) {
    float x = i;
    x /= 255;
    x = pow(x, 2.5);
    x *= 255;
      
    gammatable[i] = x;      
  }

  for (int i=0; i<3; i++){ //this sequence flashes the first pixel three times none/white as a countdown to the color reading.
    leds[16] = CRGB::Black; 
    FastLED.show(); 
    delay(1000);
    leds[16] = CRGB::White; 
    FastLED.show(); 
    delay(500);
  }

  // turn on LED
  tcs.setInterrupt(false);        
  delay(60);  // takes 50ms to read 
  
  tcs.getRawData(&red, &green, &blue, &clear);

  tcs.setInterrupt(true);  // turn off LED
}

void loop()
{
  // Figure out some basic hex code for visualization
  uint32_t sum = red;
  sum += green;
  sum += blue;
  //sum += clear; // clear contains RGB already so no need to re-add it
  
  float r, g, b;
  r = red; r /= sum;
  g = green; g /= sum;
  b = blue; b /= sum;
  r *= 256; g *= 256; b *= 256;
  
  CRGBPalette16 gTargetPalette (
   CRGB (gammatable[(int)r], gammatable[(int)g], gammatable[(int)b]));
  
  colorwaves( leds, NUM_LEDS, gTargetPalette);//gCurrentPalette);
 
  FastLED.show();
  FastLED.delay(20);
}
 
// This function draws color waves with an ever-changing,
// widely-varying set of parameters, using a color palette.
void colorwaves( CRGB* ledarray, uint16_t numleds, CRGBPalette16& palette) 
{
  static uint16_t sPseudotime = 0;
  static uint16_t sLastMillis = 0;
  static uint16_t sHue16 = 0;
 
  uint8_t sat8 = beatsin88( 87, 220, 250);
  uint8_t brightdepth = beatsin88( 341, 96, 224);
  uint16_t brightnessthetainc16 = beatsin88( 203, (25 * 256), (40 * 256));
  uint8_t msmultiplier = beat8(147); //beatsin88(147, 23, 60); - creates a more dynamic pattern [IH]
 
  uint16_t hue16 = sHue16;//gHue * 256;
  uint16_t hueinc16 = beatsin88(113, 300, 1500);
  
  uint16_t ms = millis();
  uint16_t deltams = ms - sLastMillis ;
  sLastMillis  = ms;
  sPseudotime += deltams * msmultiplier;
  sHue16 += deltams * beatsin88( 400, 5,9);
  uint16_t brightnesstheta16 = sPseudotime;
  
  for( uint16_t i = 0 ; i < numleds; i++) {
    hue16 += hueinc16;
    uint8_t hue8 = hue16 / 256;
    uint16_t h16_128 = hue16 >> 7;
    if( h16_128 & 0x100) {
      hue8 = 255 - (h16_128 >> 1);
    } else {
      hue8 = h16_128 >> 1;
    }
 
    brightnesstheta16  += brightnessthetainc16;
    uint16_t b16 = sin16( brightnesstheta16  ) + 32768;
 
    uint16_t bri16 = (uint32_t)((uint32_t)b16 * (uint32_t)b16) / 65536;
    uint8_t bri8 = (uint32_t)(((uint32_t)bri16) * brightdepth) / 65536;
    bri8 += (255 - brightdepth);
    
    uint8_t index = hue8;
    //index = triwave8( index);
    index = scale8( index, 240);
 
    CRGB newcolor = ColorFromPalette( palette, index, bri8);
 
    uint16_t pixelnumber = i;
    pixelnumber = (numleds-1) - pixelnumber;
    
    nblend( ledarray[pixelnumber], newcolor, 128);
  }
}

View on GitHub

red_3

Testing with a red object 

blue_4

Testing with a blue object

Assembly

Planning

The petticoat with the microcontroller, battery, and all of the LEDs ‎sits underneath the dress and can't be accessed without pulling up ‎the dress or putting the microcontroller at the bottom making it ‎hard to reach. In addition, the color sensor needs to be in a central ‎place on top of the dress.‎

The solution to connecting it all together - snaps! Or to be ‎precise conductive snaps.‎

The idea is to snap the petticoat to the dress, then snap on another ‎element on top of the dress (the belt) to hold the color sensor and ‎then run conductive thread from one set of snaps to the other. This ‎will also enable detaching the belt and the petticoat and connecting ‎them to another dress/skirt.‎

Finally, there is an on/off reset snap on the dress that runs all the ‎way down to the battery.‎

Sewing the Petticoat

Planning

  1. ‎Decide on the placement of the microcontroller. That will ‎determine the battery, the snaps that hook up to the dress and ‎the starting point of the LEDs. On the waistline to the left is the ‎recommended placing in order to be as close as possible to ‎where the belt will be on the dress.‎

  2. Decide on the pattern of the LED strands. They can spiral ‎around the petticoat, swirl around semi randomly, zig zag up ‎and down, whatever. It's recommended to connect them with a ‎whole bunch of safety pins first before sewing them in place. In ‎this project, the LEDs spiral around and around the petticoat. ‎The dress was shorter than the petticoat, so the LEDs spiral ‎finished up before they crossed over the edge of the dress.‎

  3. Decide on the placement of the snaps. For the petticoat to ‎dress snaps, use the larger magnetic buttons. You can go with ‎either 4 snaps for just the color sensor or 6 snaps for both the ‎color sensor and the on/off switch. You need to space them to ‎make sure you can create separate connections that don't ‎cross each other. And plan the order right so that you have ‎direct lines to the place where the belt will be connected.‎

Sewing

It is extremely recommended to test all of the time! There's nothing ‎more annoying that having a project not work and try to trace all of ‎the connections to see where there might be a problem. ‎

Fun fact: Alligator clip to the magnetic buttons so they easily ‎connect for testing.‎

Sew in the microcontroller with some regular black thread to keep ‎it in place. Then start with the LEDs strand's connector. Using ‎conductive thread connect the GND, D1, and Vout on the right to the ‎wiring the connects to the strands.‎

sew_5

Sewing the microcontroller

Next sew the snaps to the GND on the right and the SCL (A1/D2), ‎SDA (A2/D0) and 3Vo on the left. Use both the front side and inner ‎side of the petticoat to avoid crossing circuits. You can later sew ‎ribbon on top of each connection to further ensure they won't touch ‎each other and also to avoid irritating the skin on the inner side. ‎There are different techniques for sewing with conductive thread. ‎You can read more about that here.‎

snaps_6

Sewing the magnetic snaps

Sew up the LED strands. In this project, I sewed around every 5 ‎LEDs either the LED itself or the wiring. Try to follow the natural ‎curves of the petticoat so that the LEDs with flow nicely under the ‎dress. What's nice about the Adafruit LEDs strands is that they ‎barely weight anything and don't burden the petticoat.‎

testing_7

Testing with alligator clips connected to the color sensor

For the battery, to have control over resetting the color, plan for a ‎switch closer to the belt on the outside of the dress. To do this, cut ‎the red wire to the battery and split it between 2 snaps. When the ‎switch is "on" it essentially connects these 2 snaps and closes the ‎circuit.‎

connect_8

Sewing the battery snaps - notice the red wire is split between them and the black wire is ‎connected directly to the battery.

Also see the sewed on battery pocket.‎

Lastly add a battery pocket that is held secure with a ‎nonconductive snap to keep it from moving around. There's a nice ‎rubber band trick to keep the wires from detaching from the battery. ‎It’s in nearly all of the Adafruit tutorials, for example here. Make sure ‎you choose the right battery size before sewing the pocket.‎

final_9

Final petticoat part

Sewing the Belt

Planning

  1. ‎Decide on the placement of the belt relative to the dress and ‎where you'll position the belt snaps. In this project, I'm using ‎the smaller snaps for the belt. Lastly, trace the lines between ‎the belt connections and the petticoat connections to ensure ‎separation of the lines.‎

  2. Remove some of the jewels on the belt to make room for the ‎color sensor. ‎

Sewing

Sew in the color sensor with some regular black thread to keep it in ‎place. Sew conductive thread from the 4 pins on the color sensor to ‎the placement of the belt snaps. The belt is pretty narrow so make ‎sure to space out correctly. A banana type shape for the snaps will ‎probably work best.‎

Use a scrap piece of black satin and sew it on both sides of the belt ‎sash to both cover the stiches and keep them from touching each ‎other.‎

belt_10

Belt - Front, color sensor instead of some of the gems

belt_11

Belt - Back, snaps need to be spaced out and circuits need to be separate

bow_12

Bow in the belt back

Instead of just tying the belt on, you can create a bow at the back at ‎the right length and use non-conductive snaps to put it together. ‎You can also add a few non-conductive snaps around the dress to ‎keep the belt in place.‎

bow_13

Bow closed

Sewing the Dress

Planning

  1. ‎The snaps on the dress should go according to the plan for ‎sewing the petticoat and the belt. For the 4 color sensor ‎connections, you should align the positioning of the petticoat ‎snaps to their position on the inside of the dress, create direct ‎lines from them to the back side of the belt connections and ‎verify the lines don't intersect.‎

  2. Plan where on the dress you want to put the on/off switch and ‎align the connection to the remaining 2 magnetic snaps.‎

Sewing

You can use ribbon to cover up the thread lines. Therefore, you don't ‎need to sew from one snap to other, rather leave the thread flat with ‎some extra room for flexibility. For each connection, start with the ‎petticoat matching snap, sew that on with conductive thread, lay ‎enough thread on the dress and sew the other side of that ‎connection to the back side of where the belt snap will be.‎

sewing_14

Lay the conductive thread on the inside of the dress from the petticoat snap to the belt snap

sewing_15

Cover the thread with ribbon

Sew on ribbon to conceal the connections and keep them separated.‎

ribbon_16

The snaps on the dress that correspond with the belt snaps

On/Off switch - using another pair of conductive snaps, place a ‎decorative button to connect 2 snaps in a relatively convenient place ‎on the dress.‎

switch_17

The on/off switch in 'Off' position

switch_18

The on/off switch in 'On' position

Final Project and Additional ‎Resources

 

To put it on, start with putting on the dress, then turn on the ‎microcontroller, hook up the petticoat underneath and then the belt ‎on top, then connect the 'On' switch on the dress.‎

Additional Resources

  1. Color Sensors - more info on Adafruit color sensors

  2. Color Waves With Palettes - excellent code that goes through ‎predefined color pallets. Can be used instead of using a color ‎sensor

  3. Powering Neo Pixels - depending on how many stands you ‎hook up; you may need a different battery.‎

  4. FastLED - API documentation

Número de parte del fabricante 3501
ADAFRUIT GEMMA M0 - MINIATURE WE
Adafruit Industries LLC
Número de parte del fabricante 1356
FLORA COLOR SENSOR WHT TCS34725
Adafruit Industries LLC
Número de parte del fabricante 259
EVAL BOARD FOR MCP73833
Adafruit Industries LLC
$12.50
Ver más Details
Número de parte del fabricante 3630
ADDRESS LED STRIP R/G/B/W
Adafruit Industries LLC
$27.50
Ver más Details
Número de parte del fabricante 641
THREAD 316L THIN COND 3PLY 60'
Adafruit Industries LLC
Número de parte del fabricante 592
CABLE A PLUG TO MCR B PLUG 3'
Adafruit Industries LLC
PANEL MOUNT 1K POTENTIOMETER (BR
Número de parte del fabricante 1789
PANEL MOUNT 1K POTENTIOMETER (BR
Adafruit Industries LLC
Número de parte del fabricante 1131
JST-PH BATTERY EXT CABLE
Adafruit Industries LLC
Número de parte del fabricante 1463
ADDRESS LED RING SERIAL RGB
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.