Maker.io main logo

Circuit Playground Slouch Detector

32

2017-05-08 | By Adafruit Industries

License: See Original Project Wearables

Courtesy of Adafruit

Guide by Carter Nelson

Overview

In this guide we will go through the steps to turn your Circuit Playground into a slouch detector. Using one of several pinning options along with various battery supply options, you can then wear your Slouch Detector while sitting at a desk. It will provide a warning if you, well, get a little slouchy - hopefully with reminders, you can keep your good posture and maintain a healthy back!

Circuit Playground Slouch Detector

Required Parts

This project uses the sensors already included on the Circuit Playground so no additional electronics or soldering are required. You will also need some batteries and a holder for the batteries.

Required Parts

Optional Parts

These items help make this project more wearable. There are a couple ways to pin the Circuit Playground in the right location. Additionally, there are a few smaller sized battery options to make it more pocketable. A battery extension cable allows for placing the battery in a different pocket.

Optional Parts

Before Starting

If you are new to the Circuit Playground, you may want to first read these overview guides.

Circuit Playground Classic

Circuit Playground Express

Hello Slouch

First, what is slouching? It has a few meanings, but we are concerned about how it applies to posture. We'll mainly focus on sitting posture, so let's introduce a reference standard sitting Stick Figure of Engineering (SFoE), as shown below.

Good Posture Example

The SFoE is sitting nice and straight with good posture. If we imagine a line going up through the body of the SFoE, then we can think of slouch as an angle between this line and the vertical as shown in the figure below.

slouchAngle

The basic idea is to monitor this angle. We will constantly compare it to a preset value. If the angle exceeds this value, then we'll say the SFoE is slouching. Let's see how we can measure this angle with the Circuit Playground.

Measuring Slouch Angle

We will use the accelerometer on the Circuit Playground to measure the slouch angle. A more in depth overview of the accelerometer can be found in the How Tall Is It? Guide. If you look at the Circuit Playground sideways, the coordinate system of the accelerometer is defined as shown in the figure below.

Measuring Slouch Angle

In the figure below, the Circuit Playground is tilted away from the vertical by an amount we are calling currentAngle. The big green arrow is the acceleration due to gravity. It is always present and always points vertically. (see How Tall Is It? Guide for more info)

currentAngle

A portion of the green arrow will be sensed by the X axis and returned by  motionX() . Similarly, a portion will be sensed by the Z axis as returned by  motionZ() . All together, these values form a right triangle as shown in the figure below. This let's us use the basic right angle functions shown to compute the value for currentAngle.

Measuring currentAngle

Note that the portion of gravity sensed by the Z axis is in the negative direction. Therefore, a - sign shows up in the equations.

Two ways are shown above for computing currentAngle. One uses both the  motionX()  and  motionZ()  values in the arctangent function,  atan() . The second one only uses the  motionZ()  value in the arcsine function,  asin() . GRAVITY is a constant which, on Earth at sea level, is about 9.80665 m/s2.

So which equation should we use? We'll let's take a look at how they behave.

Arctan Vs. Arcsine

You can use the sketch below to observe the behavior of computing the Circuit Playground tilt angle via the two different methods.

Copy Code
///////////////////////////////////////////////////////////////////////////////
// Circuit Playground Slouch Detector Angle Demo
//
// Compute current angle using accelerometer.
// Compare asin() to atan2().
//
// Author: Carter Nelson
// MIT License (https://opensource.org/licenses/MIT)

#include <Adafruit_CircuitPlayground.h>

#define GRAVITY 9.80665 // standard gravity (m/s^s)
#define RAD2DEG 52.29578 // convert radians to degrees

float currentAngle1;
float currentAngle2;

///////////////////////////////////////////////////////////////////////////////
void setup() {
Serial.begin(9600);

// Initialize Circuit Playground
CircuitPlayground.begin();
}

///////////////////////////////////////////////////////////////////////////////
void loop() {
// Compute current angle
currentAngle1 = RAD2DEG * asin(-CircuitPlayground.motionZ() / GRAVITY);
currentAngle2 = RAD2DEG * atan2(-CircuitPlayground.motionZ() ,
CircuitPlayground.motionX() );

// Print current angle
Serial.println(currentAngle1);
Serial.print(",");
Serial.println(currentAngle2);

// But not too fast
delay(100);
}

Copy and paste this code into the Arduino IDE and upload it to the Circuit Playground. Then open the serial plotter:

Tools -> Serial Plotter

First, try holding the Circuit Playground with the micro USB connector pointed up. This makes the X axis point up as shown in the figures in the previous section. Now tilt the Circuit Playground a little and watch the two lines. They should follow each other pretty closely. Now rotate the Circuit Playground so the micro USB connector is pointed to the side. Tilt the Circuit Playground again and you should see the lines behaving very differently. Something like what is shown in the figure below.

Arctan Vs. Arcsine

The blue line is from the  asin()  function and continues to behave correctly. However, the orange line, which comes from the  atan2()  function only works when the X axis is pointing up. For our slouch detector, we can't assume this to be true. Therefore, we will use the  asin()  equation to compute the value for currentAngle.

Slouch Detector v1

The idea of the slouch detector is simple. If the current angle sensed by the Circuit Playground (currentAngle) exceeds a preset value (SLOUCH_ANGLE), then we are slouching and should sound an alarm. We can achieve this with a simple modification of our previous sketch. Here's the code.

Copy Code
///////////////////////////////////////////////////////////////////////////////
// Circuit Playground Slouch Detector v1
//
// Compute current angle using accelerometer and compare
// to preset slouch angle. Sound alarm if slouching.
//
// Author: Carter Nelson
// MIT License (https://opensource.org/licenses/MIT)

#include <Adafruit_CircuitPlayground.h>

#define SLOUCH_ANGLE 10.0 // allowable slouch angle (deg)
#define GRAVITY 9.80665 // standard gravity (m/s^s)
#define RAD2DEG 52.29578 // convert radians to degrees

float currentAngle;

///////////////////////////////////////////////////////////////////////////////
void setup() {
// Initialize Circuit Playground
CircuitPlayground.begin();
}

///////////////////////////////////////////////////////////////////////////////
void loop() {
// Compute current angle
currentAngle = RAD2DEG * asin(-CircuitPlayground.motionZ() / GRAVITY);

// Check if slouching
if (currentAngle > SLOUCH_ANGLE) {
// Sound alarm
CircuitPlayground.playTone(800, 500);
}
}

The preset angle is defined globally at the top of the sketch.

Copy Code
#define SLOUCH_ANGLE        10.0      // allowable slouch angle (deg)

And then a simple if statement is used to check for slouching.

Copy Code
  // Check if slouching
if (currentAngle > SLOUCH_ANGLE) {
// Sound alarm
CircuitPlayground.playTone(800, 500);
}

With the above sketch loaded and running on the Circuit Playground, you should hear the alarm sound if the tilt (slouch) angle is greater than 10 degrees.

Slouch Detector v2

While the v1 version of our slouch detector works, there are a few features we need to add. The first is to account for the fact that the Circuit Playground may not sit perfectly vertical when being worn.

To deal with this, we need to generalize the problem a little further. Here is another version of our SFoE with some more angle definitions.

SFoE with some more angle definitions

The dashed lines represent the SFoE sitting with good posture, which we are defining as the targetAngle. We want to determine if the SFoE exceeds the slouchAngle (SLOUCH_ANGLE), but the Circuit Playground only reports the angle relative to the vertical line, currentAngle.

If we could determine the targetAngle, we could compute the slouchAngle from the currentAngle as follows:

currentAngle = targetAngle + slouchAngle

(rearrange)

slouchAngle = targetAngle - currentAngle

So how do we come up with the targetAngle? We will make this settable by using the buttons on the Circuit Playground. The idea will be:

    • Attach Circuit Playground to clothing.
    • Sit with good posture.
    • Press either button to set currentAngle as targetAngle.
    • Do math shown above to compute slouchAngle.
    • Compare slouchAngle to preset value, SLOUCH_ANGLE.
    • Sound alarm if vaue exceeded.

Here is the code that adds this feature:

Copy Code
///////////////////////////////////////////////////////////////////////////////
// Circuit Playground Slouch Detector v2
//
// Push button(s) to set a target angle.
// Compute current angle using accelerometer and compare
// to preset slouch angle. Sound alarm if slouching.
//
// Author: Carter Nelson
// MIT License (https://opensource.org/licenses/MIT)

#include <Adafruit_CircuitPlayground.h>

#define SLOUCH_ANGLE 10.0 // allowable slouch angle (deg)
#define GRAVITY 9.80665 // standard gravity (m/s^s)
#define RAD2DEG 52.29578 // convert radians to degrees

float currentAngle;
float targetAngle;

///////////////////////////////////////////////////////////////////////////////
void setup() {
// Initialize Circuit Playground
CircuitPlayground.begin();

// Initialize target angle to zero.
targetAngle = 0;
}

///////////////////////////////////////////////////////////////////////////////
void loop() {
// Compute current angle
currentAngle = RAD2DEG * asin(-CircuitPlayground.motionZ() / GRAVITY);

// Set target angle on button press
if ((CircuitPlayground.leftButton()) || (CircuitPlayground.rightButton())) {
targetAngle = currentAngle;
CircuitPlayground.playTone(900,100);
delay(100);
CircuitPlayground.playTone(900,100);
delay(100);
}

// Check if slouching
if (currentAngle - targetAngle > SLOUCH_ANGLE) {
// Sound alarm
CircuitPlayground.playTone(800, 500);
}
}

Now you can press either button to set the targetAngle to the currentAngle. Two small beeps will sound to confirm this.

Slouch Detector v3

The next feature we need to add is a time delay for the alarm. Currently, it sounds the instant the slouch angle is exceeded. But what if you were just leaning over to look at something? We should give you a chance to straighten back up before sounding the alarm.

This idea is shown in the figure below, which shows two cases where the current angle exceeded the slouch angle.

Slouch Detector v3

We don't want to sound an alarm for the first case (TIME1). That was a brief event like someone bending over to look at something. However, in the second case, the angle has been exceed for a longer period of time (TIME2). Either the person is slouching or has fallen asleep. In either case, we want to sound the alarm.

To make this work, we need to keep track of time. Specifically, how long we've been slouching, and compare that to a preset value (SLOUCH_TIME). We only sound the alarm if (a) we are slouching, and (b) we've been doing so for longer than this preset value.

Here is the code that adds this feature:

Copy Code
///////////////////////////////////////////////////////////////////////////////
// Circuit Playground Slouch Detector v3
//
// Push button(s) to set a target angle.
// Compute current angle using accelerometer and compare
// to preset slouch angle. Sound alarm if slouching after
// a preset period of time.
//
// Author: Carter Nelson
// MIT License (https://opensource.org/licenses/MIT)

#include <Adafruit_CircuitPlayground.h>

#define SLOUCH_ANGLE 10.0 // allowable slouch angle (deg)
#define SLOUCH_TIME 3000 // allowable slouch time (secs)
#define GRAVITY 9.80665 // standard gravity (m/s^s)
#define RAD2DEG 52.29578 // convert radians to degrees

float currentAngle;
float targetAngle;
unsigned long slouchStartTime;
bool slouching;

///////////////////////////////////////////////////////////////////////////////
void setup() {
// Initialize Circuit Playground
CircuitPlayground.begin();

// Initialize target angle to zero.
targetAngle = 0;
}

///////////////////////////////////////////////////////////////////////////////
void loop() {
// Compute current angle
currentAngle = RAD2DEG * asin(-CircuitPlayground.motionZ() / GRAVITY);

// Set target angle on button press
if ((CircuitPlayground.leftButton()) || (CircuitPlayground.rightButton())) {
targetAngle = currentAngle;
CircuitPlayground.playTone(900,100);
delay(100);
CircuitPlayground.playTone(900,100);
delay(100);
}

// Check for slouching
if (currentAngle - targetAngle > SLOUCH_ANGLE) {
if (!slouching) slouchStartTime = millis();
slouching = true;
} else {
slouching = false;
}

// If we are slouching
if (slouching) {
// Check how long we've been slouching
if (millis() - slouchStartTime > SLOUCH_TIME) {
// Play a tone
CircuitPlayground.playTone(800, 500);
}
}
}

Our new preset value is again set globally at the top of the sketch.

Copy Code
#define SLOUCH_TIME         3000      // allowable slouch time (secs) 

We add a few variables to keep track of how long we've been slouching.

Copy Code
unsigned long slouchStartTime;
bool slouching;

We replace the alarm with time tracking logic. If we aren't slouching, then we set that value false and nothing else happens. However, if we are currently slouching, we set the value to true and note the time when this started.

Copy Code
  // Check for slouching
if (currentAngle - targetAngle > SLOUCH_ANGLE) {
if (!slouching) slouchStartTime = millis();
slouching = true;
} else {
slouching = false;
}

And then move the alarm to a new set of if statements. If we are currently slouching, then check for how long. If it's been too long, sound the alarm.

Copy Code
  // If we are slouching
if (slouching) {
// Check how long we've been slouching
if (millis() - slouchStartTime > SLOUCH_TIME) {
// Play a tone
CircuitPlayground.playTone(800, 500);
}
}

And that's it. Now let's see how we can make this thing wearable.

Make It Wearable

There are a few options for attaching your Circuit Playground Slouch Detector to your garment. Some other items, like the JST extension cable, can also make locating the battery more convenient.

Pocket It

If you have a shirt with a front pocket, you can just drop it in there.

Pocket It

Silver Pin

The silver pin with adhesive foam back can be used to attach the Circuit Playground to most any garment.

Silver Pin

Remove the protective film from the adhesive back and apply the pin to the back of the Circuit Playground.

Silver Pin

Press it down firmly and you're good to go.

Magnetic Pin

The magnetic pin is a nice option if you don't want to stick holes in your shirt. Or just don't like sharp pointy things.

Magnetic Pin

Remove the protective film from the adhesive back and apply the metal strip to the back of the Circuit Playground.

Magnetic Pin

Just to be safe, apply the pin at the angle shown. It is metal and if you put it on horizontally, there's a slim chance it could short the 3.3V pad on one side to the GND pad on the other.

Locating and Activating

Somewhere below your shoulder seems to work best.

Locating and Activating

The best location is in the general area below your shoulder.

Locating and Activating

Now sit up straight. Press either button to set the target angle. Two beeps should sound. The slouch detector is now activated!

Questions and Code Challenges

The following are some questions related to this project along with some suggested code challenges. The idea is to provoke thought, test your understanding, and get you coding!

While the sketches provided in this guide work, there is room for improvement and additional features. Have fun playing with the provided code to see what you can do with it.

Questions

    • What are good values for SLOUCH_ANGLE and SLOUCH_TIME?
    • Will the alarm sound if the wearer leans back too far?
    • In the v3 code, what prevents slouchStartTime from constantly being reset?

Code Challenges

    • Use NeoPixels instead of the speaker to create a silent alarm.
    • Use the slide switch to choose between silent or audible alarm.
Número de parte del fabricante 3000
CIRC PLAYGROUND CLASS ATMEGA32U4
Adafruit Industries LLC
$19.95
Ver más Details
Número de parte del fabricante 727
BATTERY HOLDER AAA 3 CELL LEADS
Adafruit Industries LLC
Número de parte del fabricante 783
BATT HLDR COIN 20MM 2 CELL LEADS
Adafruit Industries LLC
Número de parte del fabricante 1131
JST-PH BATTERY EXT CABLE
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.