Maker.io main logo

Circuit Playground & Bluetooth Low Energy

96

2016-09-30 | By Adafruit Industries

License: See Original Project

Courtesy of Adafruit

Guide by Tony DiCola

Overview 

Circuit Playground is an excellent all-in-one board for learning electronics, but did you know you can control Circuit Playground wirelessly from your phone or tablet? With the magic of Bluetooth Low Energy and a little helper like the Flora Bluefruit LE module you can start experimenting with wireless control of Circuit Playground today!

Adafruit's Bluefruit LE Connect apps for both iOS and Android provide a simple interface for controlling the digital inputs/outputs on Circuit Playground. Toggle digital pins high or low to control LEDs, relays, or other digital devices. Read digital inputs to detect when buttons are pressed or simple digital sensors activate. You can even control the color of the NeoPixels on Circuit Playground wirelessly from a few clicks in the app.

Best of all there's no soldering required for this project--just connect a few components with alligator clips and you're all set!

Before you get started you'll want to familiarize yourself with a few guides:

Continue on to learn about the parts needed to follow this guide.

Parts

Circuit Playground & Bluetooth Low Energy

To follow this guide you'll need the following parts:

  • Circuit Playground
  • Flora Bluefruit LE or Bluefruit LE UART Friend
    • I recommend using the Flora Bluefruit LE module with Circuit Playground because it has big pads that are easy to connect with alligator clips--no soldering necessary!  You could however use a Bluefruit LE UART friend module but you'll need to solder headers or wires to it and Circuit Playground.  Be aware only Bluefruit LE modules with a serial connection (like Flora Bluefruit LE or Bluefruit LE UART Friend) will work with Circuit Playground!
  • Alligator Clip Test Leads
    • To reduce noise on the serial connection try to use short cables (less than 12" or so).  Longer cables should still work but you might notice small glitches or errors from time to time.
  • Android or iOS device with Bluetooth Low Energy support
    • You'll need to run the Bluefruit LE Connect application from Adafruit which is available on both Android and iOS platforms.  Make sure your device has Bluetooth Low Energy support (not just Bluetooth 'Classic' support, LE is different!).  Most phones and tablets sold in the last ~5 years should have Bluetooth LE support.

If you're using the Flora Bluefruit LE module this project is very easy to put together and requires no soldering--just connect components with alligator clip wires as shown on the next page!

Wiring

To connect a Flora Bluefruit LE module to Circuit Playground wire it up as follows:

Circuit Playground & Bluetooth Low Energy

Circuit Playground & Bluetooth Low Energy

  • Circuit Playground 3.3V to Flora Bluefruit LE 3.3V (red wire).
  • Circuit Playground GND to Flora Bluefruit GND (black wire).
  • Circuit Playground serial TX to Flora Bluefruit serial RX (yellow wire).  Double check you connect TX to RX and not TX to TX!
  • Circuit Playground serial RX to Flora Bluefruit serial TX (green wire).  Again double check you connect RX to TX and not RX to RX!
  • Circuit Playground #12 to Flora Bluefruit MODE (blue wire).  You can actually use any of the other numbered pins on Circuit Playground for this mode switch connection, however you'll need to modify the examples to use the pin number.  For simplicity stick with pin 12 so you don't need to modify the code in the rest of the guide.

Note if you're using a Bluefruit LE UART Friend the connections are the same but the MODE pin is labeled MOD, 3.3V is labeled VIN, RX is labeled RXI, and TX is labeled TXO. In addition you can ignore the other pins like CTS, RTS, and DFU.

One last very important step is to flip the mode switch on the Flora Bluefruit LE module (or Bluefruit LE UART Friend) into the DATA position. If the switch is in the CMD position the software won't work correctly so be careful to double check the switch is in DATA mode.

Circuit Playground & Bluetooth Low Energy

Arduino Setup

After wiring the Bluefruit LE module to Circuit Playground you'll need to do a small bit of software setup to run the examples.

First if you're new to Circuit Playground be sure to follow its guide to setup Arduino for programming the board. Make sure you can load some of the basic examples like blinking a LED on the board before continuing further. Also don't forget to install the Circuit Playground library in Arduino as the guide mentions.

Next follow the Bluefruit LE module guide to install the necessary Arduino libraries for using the module. In particular you need to install this library (use the library manager in Arduino to search for and easily install it):

That should be all the setup necessary to program Circuit Playground with sketches that use a Bluefruit LE module! The next pages explain example sketches to control Circuit Playground with the Bluefruit LE module.

Pin IO

 

Pin IO is a way to control the digital inputs, outputs, and more on Circuit Playground wirelessly from a phone or tablet. Right now only basic components like digital inputs, outputs, and even PWM (i.e. dimming an LED) are controllable with pin IO.

Pin IO works using the Firmata protocol to remotely control the Circuit Playground. Normally Firmata is used with a USB or serial connection between an Arduino and a computer. However by hooking up a Bluefruit LE module to the serial pins on Circuit Playground you can wirelessly talk the Firmata protocol to control Circuit Playground too. You don't need to write any code to control the board--just load the Bluefruit LE Connect iOS or Android apps!

To use pin IO mode make sure you've followed all of the previous pages in this guide and have a Circuit Playground wired to a Bluefruit LE module, and the Arduino IDE setup to program both Circuit Playground and the Bluefruit LE module.

Next install the following Arduino library (use the library manager to find it, filter to BLEFirmata and install the Adafruit BLEFirmata library):

Once the library is installed open the CircuitPlayground_nRF51822 example from the library in Arduino. This sketch implements the Firmata protocol and uses the Bluefruit LE module to listen for commands.

Circuit Playground & Bluetooth Low Energy

You don't need to make any modifications to the sketch to use it, however if you changed the mode pin from 12 to something else you will need to modify the BLUEFRUIT_UART_MODE_PIN define in the BluefruitConfig.h tab.

Upload the sketch to Circuit Playground and you should be ready to start controlling the pins with either the Bluefruit LE Connect iOS app or Bluefruit LE Connect Android app. If you haven't used the Bluefruit LE Connect app before be sure to skim the guide on its usage (although the guide is for iOS that application is very similar on Android).

Circuit Playground & Bluetooth Low Energy

Open the Bluefruit LE Connect application and look for a device called "BLE_Firmata". Click the Connect button to connect to the Bluefruit LE module.

Circuit Playground & Bluetooth Low Energy

Click the Pin I/O button (on the iOS app look at the icons on the bottom of the screen) to enter Pin IO mode.

Circuit Playground & Bluetooth Low Energy

After entering Pin IO mode you should see a list of the digital inputs & outputs on Circuit Playground.

Circuit Playground & Bluetooth Low Energy

You can tap a pin to see options like turning it into an input and reading its state, or turning it into an output and setting it to a high or low logic level. 

Try turning pin 13 into an output and toggling it high or low. This pin is actually connected to the red LED on Circuit Playground and you should see it turn on/off as the pin toggles.

Circuit Playground & Bluetooth Low Energy

Some of the components on Circuit Playground work just with digital IO and pin control:

  • The red LED on the board is pin 13 and can be turned on or off as a digital output.
  • The slide switch is pin 21 and will read a low level when on the right/ and high level when on the left/-.
  • The left push button is pin 4 and right push button is pin 19, each will read a low level when not pressed and a high level when pressed.

Try pushing the buttons or moving the slide switch--you should see the pin state change in the Bluefruit LE Connect application. That's all there is to the basics of controlling digital pins wirelessly with Bluefruit LE & Circuit Playground!

NeoPixels

In addition to toggling pins on Circuit Playground you can also control the color of its NeoPixel LEDs wirelessly from a phone or tablet. The Bluefruit LE Connect iOS and Android apps have a special color picker mode which makes it easy to change pixel colors.

To use this NeoPixel control sketch make sure you've followed all the steps in this guide and have a Circuit Playground wired up to a Bluefruit LE module. In addition make sure you have the Circuit Playground and Adafruit Bluefruit LE nRF51 Arduino libraries installed as previously mentioned.

Next open the Arduino IDE and pick the cplay_neopixel_picker example from the Adafruit Bluefruit LE nRF51 library.

Circuit Playground & Bluetooth Low Energy

You shouldn't need to modify anything in the sketch, however there are some #define values near the top that can adjust the behavior like the intensity of the NeoPixel brightness. Also if you changed the mode pin from 12 to something else you will need to modify the BLUEFRUIT_UART_MODE_PIN define in the BluefruitConfig.h tab.

Upload the sketch to Circuit Playground and you should be ready to start controlling the NeoPixels with either the Bluefruit LE Connect iOS app or Bluefruit LE Connect Android app. If you haven't used the Bluefruit LE Connect app before be sure to skim the guide on its usage (although the guide is for iOS that application is very similar on Android).

Circuit Playground & Bluetooth Low Energy

On your iOS or Android device open the Bluefruit LE application. You should see a device called "CPlay_BLE" (sometimes in rare cases when the serial connection has too much noise you might see it called "Adafruit Bluefruit LE").

Circuit Playground & Bluetooth Low Energy

Click the device, then click the Controller mode (not the NeoPixel mode, that's a more advanced NeoPixel control system that isn't supported by this sketch).

Circuit Playground & Bluetooth Low Energy

Click the Color Picker at the bottom to enter the basic NeoPixel color picker control.

Circuit Playground & Bluetooth Low Energy

Choose a color, then click Send to send it over Bluetooth Low Energy to Circuit Playground. You should see the NeoPixels on the board light up the chosen color!

Circuit Playground & Bluetooth Low Energy

Finally go back to the Controller mode and select Control Pad at the bottom. Press the left arrow or right arrow to change which pixels are lit up.

Circuit Playground & Bluetooth Low Energy

That's all there is to controlling Circuit Playground's NeoPixels with a Bluefruit LE module & Bluetooth Low Energy!

Número de parte del fabricante 3000
CIRC PLAYGROUND CLASS ATMEGA32U4
Adafruit Industries LLC
$19.95
Ver más Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.