Maker.io main logo

Arduino Linear Actuator Position Control With Smooth Start

2026-05-26 | By Ron Cutts

License: GNU Lesser General Public License Microcontrollers Motors PWM Serial / UART Arduino

In this simple tutorial, you will learn how to control the position of a linear actuator using the Arduino and L298N DC motor driver.

Watch the video!

Learn more about Visuino: What is Visuino

What You Will Need

What You Will Need

What You Will Need photo 2

What You Will Need photo 3

What You Will Need photo 4

What You Will Need photo 5

What You Will Need photo 6

What You Will Need photo 7

The Circuit

  • Connect the power supply (batteries) pin (gnd) to the motor driver controller pin (gnd)

  • Connect the power supply (batteries) pin (+) to motor driver controller pin (+)

  • Connect the power supply (batteries) pin (+) to the Arduino pin (VIN)

  • Connect GND from the Arduino to the motor driver controller pin (gnd)

  • Connect digital pin(6) from Arduino to motor driver pin (IN1)

  • Connect digital pin(8) from Arduino to motor driver pin (IN2)

  • Connect the linear actuator to the motor driver, as you can see on the schematic

  • Connect the potentiometer pin [DTA] to arduino analog pin [A0]

  • Connect the potentiometer pin [VCC] to the breadboard positive pin [5V]

  • Connect the potentiometer pin [GND] to the breadboard pin [GND]

The Circuit

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino, and Select the Arduino UNO Board Type photo 2

In Visuino, Add Components

  • Add "Dual DC Motor Driver Digital and PWM Pins Bridge (L9110S, L298N)" component

  • Add "Ramp To Analog Value" component

In Visuino Add Components

In Visuino Add Components photo 2

In Visuino Connect Components

  • Connect Arduino Analog pin [0] to "RampToValue1" pin [In]

  • Connect "RampToValue1" pin [Out] to "DualMotorDriver1" > Motors [0] Pin [In]

  • Connect "DualMotorDriver1" > Motors [0] Pin [Direction]" to Arduino digital pin[8]

  • Connect "DualMotorDriver1" > Motors [0] Pin [Speed]" to Arduino digital pin Analog PWM[6]

In Visuino Connect Components

In Visuino Connect Components photo 2

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" tab, make sure the correct port is selected, and then click on the "Compile/Build and Upload" button.

Generate, Compile, and Upload the Arduino Code

Play

If you power the Arduino module and change the potentiometer position, then the linear actuator will start to move in one direction, and if you move the potentiometer position to the other side, it will reverse.

Congratulations! You have completed your project with Visuino. Also attached is the Visuino project that I created for this. You can download it here and open it in Visuino: https://www.visuino.eu

Downloads

Número de parte del fabricante DRI0002
EVAL BOARD FOR L298
DFRobot
$12.90
Ver más Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.