Maker.io main logo

Analog MEMS Microphone (VM2020) Hookup Guide

121

2023-10-11 | By SparkFun Electronics

License: See Original Project

Courtesy of SparkFun

Guide by QCPETE, BBOYHO

Introduction

Note: This tutorial covers the SparkFun Analog MEMS Microphone - VM2020 (BOB-21537). While this tutorial was based on the previous MEMS microphone tutorials, this version of the MEMS microphone is a differential microphone and was designed for noisy environments. For ‎specific details regarding the microphone ICs, refer to the Documents tab on their product pages ‎or the previous release of this Hookup Guide:

ADMP401 & ICS-40180 MEMS MICROPHONE HOOKUP GUIDE

The SparkFun Analog MEMS Microphone Breakout makes it easy to work with the Vesper ‎VM2020 analog microphone. The VM2020 is an ultra-high Acoustic Overload Point (AOP), high ‎dynamic range, differential analog output piezoelectric MEMS microphone. What separates this ‎from other analog MEMS microphones is that it was designed to be used in loud environments.‎

SparkFun Analog MEMS Microphone Breakout - VM2020‎

 

speaker_1

VM2020 Compared to Capacitive MEMS Microphone in the Back Cavity of a Smart Speaker. ‎Video courtesy of Vesper Technologies.‎

Read this guide to get an overview of the breakout board and how to use it, including its ‎technical specifications, how to hook it up to a microcontroller, and example code to get started!‎

Required Materials

To follow along with this tutorial, you will need the following materials at a minimum. You may ‎not need everything though depending on what you have. Add it to your cart, read through the ‎guide, and adjust the cart as necessary.‎

Wishlist for Analog MEMS Microphone VM2020 SparkFun Wish List

Arduino Microcontroller

You'll want a microcontroller to power the microphone. We will be using the ESP32 WROOM.‎

Amplifier and Differential ADC Converter

Since the analog pins on an Arduino microcontroller are usually single ended, you will need a ‎way to amplify the signal to a reasonable level. You will also need a differential ADC converter. ‎We recommend using the audio codec breakout WM8960. The audio codec can amplify the ‎signal to a reasonable level and already has input pins for a differential microphone.‎

  • SparkFun Audio Codec Breakout - WM8960 (Qwiic)‎

Tools

Building a circuit using this breakout requires some assembly and soldering. You may already ‎have a few of these items but if not, the tools and hardware below help with that assembly.‎

Prototyping Accessories

Depending on your setup, you may want to use IC hooks for a temporary connection. However, ‎you will want to solder header pins to connect devices to the plated through holes for a secure ‎connection. Depending on your application, you could use straight headers or right-angle headers. ‎Of course, you could also solder wire as well.‎

Recommended Reading

To successfully use the SparkFun MEMS microphone breakout board, you'll need to be familiar ‎with Arduino microcontrollers, analog (aka ADC) input, and sound waves. For folks new to ‎these topics, check out the following resources to get a feel for the concepts and verbiage used ‎throughout this tutorial.‎

  • Installing Arduino IDE: A step-by-step guide to installing and testing the Arduino software ‎on Windows, Mac, and Linux.‎

  • Analog vs. Digital: This tutorial covers the concept of analog and digital signals, as they relate ‎to electronics.‎

  • IoT RedBoard ESP32 Development Board Hookup Guide: Delve into the ‎functionality-rich world of the IoT RedBoard ESP32 Development Board!‎

  • Audio Codec Breakout - WM8960 Hookup Guide: The SparkFun Audio Codec ‎Breakout - WM8960 is a low power, high quality stereo codec chock full of features. In this ‎tutorial, some of these features by using an Arduino microcontroller to configure the audio codec ‎and pass audio to the headphone or speaker channels.‎

Hardware Overview

Note: The footprint for the VM2020 is different compared to previous versions of the Analog ‎MEMS Microphone. Besides just being a differential MEMS microphone, the location of the ‎header pins are slightly different.‎

The SparkFun Analog MEMS microphone breakout board breaks out the microphone for sound ‎detection in loud environments. Each version breaks out the VM2020 on the top side of the ‎board.‎

board_2

The board receives audio input from the bottom of the board. For users soldering straight headers, ‎you may want to consider soldering them from the back.‎

board_3

  • OUT− - Audio signal output for differential −output

  • OUT+ - Audio signal output for differential +output

  • VCC - Voltage input (1.6V to 3.6V). To power this lil' mic, use a DC voltage with a supply ‎current of about 248μA for VM2020. We'll be using 3.3V from an Arduino

  • GND - Ground.‎

For technically minded folks, here are some of the features of the VM2020 and a comparison ‎with other SparkFun MEMS Microphone Breakout boards. Make sure to check out VM2020 ‎datasheet in the Resources & Going Further for a complete overview of the microphone.‎

table_3

Note that the acoustic overload point of the VM2020 is greater than the other MEMS ‎microphones. The audio is less likely to be clipped in louder settings (such as concerts, dance ‎studios, etc.) or when the microphone is placed beside a speaker. Below is a table of typical ‎sounds, their approximate decibel levels, and the AOP of the three microphones listed earlier. ‎The information was gathered from a variety of sources online. Keep in mind noise-induced ‎hearing loss varies depending on the sound intensity, the amount of exposure time, and how ‎close your ears are to the sound source.‎

table_4

Board Dimensions

The board dimensions for the breakout are 0.40" x 0.55" (10.16mm x 13.97mm). The location of ‎the header pins is different compared to previous versions with the extra pin for the differential ‎output.‎

dim_5

Hardware Hookup

Now that we're familiar with the microphone breakout, let's connect it to a microcontroller and ‎monitor some sound!‎

Microphone Breakout Connections

For a permanent connection, we recommend soldering four wires (or headers) to the PTHs on the ‎breakout. We opted for soldering header pins and using jumper wires. Of course, you could also ‎solder wires to the breakout board as well. For a temporary connection during prototyping, you ‎can use IC hooks like these.‎

connect_6

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.‎

connect_7

Working with Wire

How to strip, crimp, and work with wire.‎

We recommend soldering right angle headers. Right angle headers will provide a low height ‎profile. This is more versatile as users can angle the microphone or add M/F jumper wires ‎between the board and breadboard. The microphone will also sit up and away from the board.‎

headers_8

Note: You can use any connection as explained above to connect. If you decide to solder straight ‎header pins, we recommend inserting the straight header pin's tail from the top of the board so ‎that the audio input for the microphone is facing away from a surface. This can also be a low ‎profile as the board is flush with the breadboard.

straight_9

Straight header pins being soldered to MEMS microphone.‎‎ ‎

However, depending on your application, you can also solder wires to the board. We recommend ‎using the following colors of wire to easily distinguish the signals, but you can always select a ‎different color if you prefer (or do not have the colors used available).

right_10

Right angle header pins being soldered to MEMS microphone.‎‎

  • Green (or some other color not Red or Black) for Output−

  • Blue (or some other color not Red or Black) for Output+

  • Red for VCC

  • Black for GND

Connecting to a Microcontroller and Audio Codec WM8960‎

Next up we'll connect the breakout to an audio codec to amplify and read the signal. Then we ‎will connect the boards to a microcontroller to monitor the audio signal output. For this tutorial, ‎we used the MEMS microphone with the audio codec WM8960 and SparkFun IoT RedBoard - ‎ESP32. The ESP32 module has I2S support and is recommended in this setup with the WM8960. ‎Make the following connections between the breakout and IoT RedBoard - ESP32 (or whichever ‎ESP32 variant that you choose).‎

Note: If you decide to use a variant of the ESP32 like the Thing Plus, you can adjust the I2S ‎connections by using a different GPIO. Make sure to adjust the pin definitions in the example ‎code if you decide to use a different ESP32 module.‎

table_11

The completed circuit should look something like the photo below:‎

circuit_12

Software Installation

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. ‎If this is your first-time using Arduino, please review the following tutorials. ‎

Arduino Board Definitions and Driver

We'll assume that you installed the necessary board files and drivers for your development board. ‎In this case, we used the IoT RedBoard - ESP32 which uses the CH340 USB-to-serial converter. ‎If you are using a Processor Board, make sure to check out its hookup guide for your Processor ‎Board.‎

manager_13

Installing Board Definitions in the Arduino IDE

‎How do I install a custom Arduino board/core?

It's easy! This tutorial will go over how to install ‎an Arduino board definition using the Arduino Board Manager.

We will also go over manually ‎installing third-party cores, such as the board definitions required for many of the SparkFun ‎development boards.‎

board_14

IoT RedBoard ESP32 Development Board Hookup Guide

Delve into the functionality-rich world of the IoT RedBoard ESP32 Development Board!‎

install_15

How to Install CH340 Drivers

How to install CH340 drivers (if you need them) on Windows, Mac OS X, and Linux.‎

Installing the Arduino Library

We'll be using the WM8960 audio codec and connecting to the differential microphone input ‎pins. The SparkFun Arduino library can be downloaded with the Arduino library manager by ‎searching 'SparkFun Audio Codec Breakout WM8960' or you can grab the zip here from ‎the GitHub repository to manually install.‎

SPARKFUN WM8960 ARDUINO LIBRARY (ZIP)‎

Arduino Example

Note: We used espressif's v2.0.6 board package for the SparkFun IoT RedBoard - ESP32. ‎Previous versions of the board package seem to save the channels differently in the buffer. When ‎reading the WM8960's I2S left microphone channel with v2.0.5 and this example, the Serial ‎Plotter would only display the "right channel."‎

From the menu, select the following: File > Examples > SparkFun WM8960 Arduino ‎Library > Example_15_VolumePlotter_MEMS_Mic_Differential. If you have not already, ‎select your Board (in this case the SparkFun ESP32 IoT RedBoard), and associated COM port. ‎Then hit the upload button.‎

Open the Arduino Serial Plotter and set it to 115200 baud to view the output. Make some noise ‎by saying "Woooo!," clapping, or rubbing your fingers on the microphone. You should see an ‎output showing the left input microphone's audio signal!‎

open_16

Try placing the microphone next to a loud amplified speaker and adjusting the PGA as necessary ‎for your application. Or add a second MEMS microphone to the right channel and adjusting code ‎to include the right channel.‎

Note: To adjust the code to include the right channel as well, you will need to adjust the mean ‎for both the left and right channels in the if (result == ESP_OK){} statement. You will then ‎need to calculate and plot the values as comma separated values (CSV) for the Arduino Serial ‎Plotter to display properly. Below is how the adjusted code should look like. ‎

Copy Code
  if (result == ESP_OK)
  {
    // Read I2S data buffer
    int16_t samples_read = bytesIn / 8;
    if (samples_read > 0) {
      float meanLeft = 0;
      float meanRight = 0;
      // Only looking at left signal samples in the buffer (e.g. 0,2,4,6,8...)
      // Notice in our for loop here, we are incrementing the index by 2.
      for (int16_t i = 0; i < samples_read; i += 2) {
        meanLeft += (sBuffer[i]);
      }
      
      // Only looking at right signal samples in the buffer (e.g. 1,2,5,7,9...)
      // Notice in our for loop here, we are incrementing the index by 2.
      for (int16_t i = 1; i < samples_read; i += 2) {
        meanRight += (sBuffer[i]);
      }

      // Average the data reading
      // Calculate left input for this example. So we must divide by
      // "half of samples read" (because it is stereo I2S audio data)
      meanLeft /= (samples_read / 2); 
      
      // Calculate right input for this example. So we must divide by
      // "half of samples read" (because it is stereo I2S audio data)
      meanRight /= (samples_read / 2);

      // Print to serial plotter
      Serial.print(meanLeft);
      Serial.print(",");
      Serial.println(meanRight);
    }

Troubleshooting

Not working as expected and need help? ‎

If you need technical assistance and more information on a product that is not working as you ‎expected, we recommend heading on over to the SparkFun Technical Assistance page for some ‎initial troubleshooting.

SPARKFUN TECHNICAL ASSISTANCE PAGE‎

If you don't find what you need there, our SparkFun Forums are a great place to find and ask for ‎help.

SPARKFUN FORUMS

Resources and Going Further

Now that you've connected your MEMS microphone breakout, it's time to incorporate it into your ‎own project! For more information on the board, check out the resources below:‎

Número de parte del fabricante 21537
SPARKFUN ANALOG MEMS MICROPHONE
SparkFun Electronics
Número de parte del fabricante 12002
BREADBOARD - SELF-ADHESIVE (WHIT
SparkFun Electronics
Número de parte del fabricante 00553
BREAK AWAY MALE HEADERS - RIGHT
SparkFun Electronics
Número de parte del fabricante 19177
SPARKFUN IOT REDBOARD - ESP32 DE
SparkFun Electronics
$44.30
Ver más Details
Número de parte del fabricante 15424
CBL USB2.0 A PLUG TO C PLG 6.56'
SparkFun Electronics
$10.50
Ver más Details
Número de parte del fabricante 08032
AUDIO JACK 3.5MM
SparkFun Electronics
Número de parte del fabricante 08431
JUMPER WIRE M/M 6" 10PCS
SparkFun Electronics
Número de parte del fabricante 17258
FLEXIBLE QWIIC CABLE - 200MM
SparkFun Electronics
Número de parte del fabricante 15663
SPARKFUN THING PLUS ESP32 WROOM
SparkFun Electronics
$24.95
Ver más Details
Número de parte del fabricante 20168
THING PLUS ESP32 WROOM USB-C
SparkFun Electronics
$33.73
Ver más Details
Número de parte del fabricante 11375
HOOK-UP WIRE ASSORT STRAND 22AWG
SparkFun Electronics
$25.85
Ver más Details
Número de parte del fabricante 14681
SPARKFUN BEGINNER TOOL KIT
SparkFun Electronics
$62.50
Ver más Details
Número de parte del fabricante 09741
TEST LEAD HOOK TO TIP PLUG 2.5"
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.