Maker.io main logo

Adafruit MAX17048 LiPoly/LiIon Fuel ‎Gauge and Battery Monitor

1,002

2024-04-23 | By Adafruit Industries

License: See Original Project Batteries STEMMA

Courtesy of Adafruit

Guide by Liz Clark

Overview

board_1

Low-cost Lithium Polymer batteries have revolutionized electronics - ‎they're thin, they're light, they can be regulated down to 3.3V and ‎they're easy to charge. On your phone, there's a little image of a ‎battery cell that tells you the percentage of charge - so you know ‎when you absolutely need to plug it in and when you can stay ‎untethered.‎

board_2

The Adafruit MAX17048 LiPoly / LiIon Fuel Gauge and Battery ‎Monitor does the same thing. Connect it to your Lipoly or LiIon ‎battery and it will let you know the voltage of the cell, it does the ‎annoying math of decoding the non-linear voltage to get you a valid ‎percentage as well!‎

Since this nice chip is I2C, it works with any and all microcontroller or ‎microcomputer boards, from the Arduino UNO up to the Raspberry ‎Pi. And you don't have to worry about logic level, as the gauge runs ‎with 3.3V or 5.0V power and logic equally fine.‎

chip_3

To use, connect a 1S 3.7-4.2V Lithium Ion or Polymer battery to one of ‎the JST 2 PH ports (either one). Then use the included JST PH jumper ‎cable to connect to your boost converter, Feather, whatever! Use the ‎I2C interface and our Arduino or CircuitPython/Python library code to ‎read the voltage and percentage whenever you like. There are ‎various alerts, low power modes that can be customized as desired.

connect_4

To get you going fast, we spun up a custom-made PCB in ‎the STEMMA QT form factor, making it easy to interface with. ‎The STEMMA QT connectors on either side are compatible with ‎the SparkFun Qwiic I2C connectors. This allows you to make ‎solderless connections between your development board and the ‎MAX17048 or to chain it with a wide range of other sensors and ‎accessories using a compatible cable. QT Cable is not included, but ‎we have a variety in the shop.

Pinouts

pinouts_5

The default I2C address is 0x36.

Power Pins

  • VIN - The chip can safely run from 3-5VDC. To power the board, ‎give it the same power as the logic level of your microcontroller ‎‎- e.g., for a 5V microcontroller like Arduino, use 5V.‎

  • Bat - Output from the battery input voltage.‎

  • GND - common ground for power and logic.‎

The MAX17048 is powered by the connected battery, not by VIN or ‎the STEMMA/QT connector. If no battery is plugged in, or the battery ‎is too low, the MAX17048 will not respond to I2C scans or commands.‎

I2C Logic Pins

  • SCL - This is the I2C clock pin SCL, connect to your ‎microcontroller's I2C clock line. There's a 10K pullup on this pin.‎

  • SDI - This is the I2C data pin SDA, connect to your ‎microcontroller's I2C data line. There's a 10K pullup on this pin.‎

  • STEMMA QT - These connectors allow you to connect to dev ‎boards with STEMMA QT connectors or to other things ‎with various associated accessories.

JST Ports

There are two JST ports, they are equivalent. Connect the battery to ‎either one, then the load/charger to the other. Watch out for battery ‎polarity if not using an Adafruit battery!‎

The two ports simply connect together, and to the battery. You can ‎use/charge the battery while connected by having the battery on ‎one port, and then connecting a charger/project to the other.‎

Other Pins

  • INT - Interrupt signal out, you can set this up to pull low when ‎the voltage or percentage drops below a threshold. Pulled up to ‎VIN with a 10K resistor.‎

  • QStart - Quick-start input. It allows reset of the MAX17048 ‎through hardware.‎

Power LED and Jumper

  • Power LED - This LED is a green LED located on the front of ‎the board. It is labeled on.‎

  • LED jumper - This jumper is located on the back of the board. ‎Cut the trace on this jumper to cut power to the "on" LED.‎

Python & CircuitPython

It's easy to use the MAX17048 with Python or CircuitPython, and ‎the Adafruit_CircuitPython_MAX1704x module. This module allows ‎you to easily write Python code that reads the values from ‎the MAX17048's battery monitoring and alert functions. You can use ‎this sensor with any CircuitPython microcontroller board or with a ‎computer that has GPIO and Python thanks to Adafruit_Blinka, our ‎CircuitPython-for-Python compatibility library.‎

CircuitPython Microcontroller Wiring

First, wire up a MAX17048 to your board exactly as shown below. ‎Here's an example of wiring a Feather M4 to the sensor with I2C ‎using one of the handy STEMMA QT connectors:‎

STEMMA

  • Board 3V to sensor VIN (red wire)

  • Board GND to sensor GND (black wire)

  • Board SCL to sensor SCL (yellow wire)

  • Board SDA to sensor SDA (blue wire)

Battery

  • Plug a 3.7/4.2V lithium polymer or lithium-ion rechargeable ‎battery into either of the JST battery ports on the board.‎

  • Plug the other board JST Battery port into the Feather JST ‎port using the cable included with the board.‎

diagram_6

You can also use standard 0.100" pitch headers to wire it up on a ‎breadboard:‎

STEMMA

  • Board 3V to sensor VIN (red wire)‎

  • Board GND to sensor GND (black wire)‎

  • Board SCL to sensor SCL (yellow wire)‎

  • Board SDA to sensor SDA (blue wire)‎

Battery

  • Plug a 3.7/4.2V lithium polymer or lithium-ion rechargeable ‎battery into either of the JST battery ports on the board.‎

  • Plug the other board JST Battery port into the Feather JST ‎port using the cable included with the board.‎

diagram_7

Watch out for battery polarity! A reversed battery will damage the ‎monitor. There are + and - symbols on the PCB to indicate which is ‎which.‎

Python Computer Wiring

Since there's dozens of Linux computers/boards you can use, below ‎shows wiring for Raspberry Pi. For other platforms, please visit the ‎guide for CircuitPython on Linux to see whether your platform is ‎supported. ‎

Here's the Raspberry Pi wired to the sensor using I2C and a STEMMA ‎QT connector:‎

  • Pi 3V to sensor VIN (red wire)

  • Pi GND to sensor GND (black wire)

  • Pi SCL to sensor SCL (yellow wire)‎

  • Pi SDA to sensor SDA (blue wire)‎

Plug a 3.7/4.2V lithium polymer or lithium-ion rechargeable battery ‎into either of the JST battery ports.‎

plug_7

Finally, here is an example of how to wire up a Raspberry Pi to the ‎sensor using a solderless breadboard:‎

  • Pi 3V to sensor VIN (red wire)

  • Pi GND to sensor GND (black wire)

  • Pi SCL to sensor SCL (yellow wire)

  • Pi SDA to sensor SDA (blue wire)‎

Plug a 3.7/4.2V lithium polymer or lithium-ion rechargeable battery ‎into either of the JST battery ports.‎

plug_8

Python Installation of MAX1704X Library

You'll need to install the Adafruit_Blinka library that provides the ‎CircuitPython support in Python. This may also require enabling I2C ‎on your platform and verifying you are running Python 3. Since each ‎platform is a little different, and Linux changes often, please visit the ‎CircuitPython on Linux guide to get your computer ready!‎

Once that's done, from your command line run the following ‎command:‎

  • pip3 install adafruit-circuitpython-max1704x

If your default Python is version 3, you may need to run pip instead. ‎Make sure you aren't trying to use CircuitPython on Python 2.x, it ‎isn't supported!‎

CircuitPython Usage

To use with CircuitPython, you need to first install the MAX1704X ‎library, and its dependencies, into the lib folder on ‎your CIRCUITPY drive. Then you need to update code.py with the ‎example script.‎

Thankfully, we can do this in one go. In the example below, click ‎the Download Project Bundle button below to download the ‎necessary libraries and the code.py file in a zip file. Extract the ‎contents of the zip file and copy the entire lib folder and ‎the code.py file to your CIRCUITPY drive.‎

Your CIRCUITPY/lib folder should contain the following folders and ‎file:‎

  • adafruit_bus_device/‎

  • adafruit_register/

  • adafruit_max1704x.mpy

file_9

Python Usage

Once you have the library pip3 installed on your computer, copy, or ‎download the following example to your computer, and run the ‎following, replacing code.py with whatever you named the file:‎

python3 code.py

Example Code - Simple Test

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: Copyright (c) 2022 ladyada for Adafruit Industries
#
# SPDX-License-Identifier: Unlicense

import time
import board
import adafruit_max1704x

i2c = board.I2C()  # uses board.SCL and board.SDA
# i2c = board.STEMMA_I2C()  # For using the built-in STEMMA QT connector on a microcontroller
max17 = adafruit_max1704x.MAX17048(i2c)

print(
    "Found MAX1704x with chip version",
    hex(max17.chip_version),
    "and id",
    hex(max17.chip_id),
)

# Quick starting allows an instant 'auto-calibration' of the battery. However, its a bad idea
# to do this right when the battery is first plugged in or if there's a lot of load on the battery
# so uncomment only if you're sure you want to 'reset' the chips charge calculator.
# print("Quick starting")
# max17.quick_start = True

while True:
    print(f"Battery voltage: {max17.cell_voltage:.2f} Volts")
    print(f"Battery state  : {max17.cell_percent:.1f} %")
    print("")
    time.sleep(1)

View on GitHub

If running CircuitPython: Once everything is saved to ‎the CIRCUITPY drive, connect to the serial console to see the data ‎printed out!‎

If running Python: The console output will appear wherever you are ‎running Python.‎

data_10

In the max1704x_simpletest.py example, the MAX17048 ‎is instantiated on I2C. The chip version and chip ID is printed to the ‎REPL. ‎

In the loop, the battery's voltage and charge percentage is printed to ‎the REPL every second.‎

Example Code - Advanced Test

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: Copyright (c) 2022 ladyada for Adafruit Industries
#
# SPDX-License-Identifier: Unlicense

import time
import board
import adafruit_max1704x

i2c = board.I2C()  # uses board.SCL and board.SDA
# i2c = board.STEMMA_I2C()  # For using the built-in STEMMA QT connector on a microcontroller
max17 = adafruit_max1704x.MAX17048(i2c)

print(
    "Found MAX1704x with chip version",
    hex(max17.chip_version),
    "and id",
    hex(max17.chip_id),
)

# Quick starting allows an instant 'auto-calibration' of the battery. However, its a bad idea
# to do this right when the battery is first plugged in or if there's a lot of load on the battery
# so uncomment only if you're sure you want to 'reset' the chips charge calculator.
# print("Quick starting")
max17.quick_start = True

# The reset voltage is what the chip considers 'battery has been removed and replaced'
# The default is 3.0 Volts but you can change it here:
# max17.reset_voltage = 2.5
print("MAX1704x reset voltage = %0.1f V" % max17.reset_voltage)

# The analog comparator is used to detect the rest voltage, if you don't think the battery
# will ever be removed this can reduce current usage (see datasheet on VRESET.Dis)
print("Analog comparator is ", end="")
if max17.comparator_disabled:
    print("disabled")
else:
    print("enabled")

# Hibernation mode reduces how often the ADC is read, for power reduction. There is an automatic
# enter/exit mode but you can also customize the activity threshold both as voltage and charge rate
# max17.activity_threshold = 0.15
print("MAX1704x activity threshold = %0.2f V" % max17.activity_threshold)

# max17.hibernation_threshold = 5
print("MAX1704x hibernation threshold = %0.2f %%" % max17.hibernation_threshold)

# You can also 'force' hibernation mode!
# max17.hibernate()
# ...or force it to wake up!
# max17.wake()

# The alert pin can be used to detect when the voltage of the battery goes below or
# above a voltage, you can also query the alert in the loop.
max17.voltage_alert_min = 3.5
print("Voltage alert minimum = %0.2f V" % max17.voltage_alert_min)
max17.voltage_alert_max = 4.1
print("Voltage alert maximum = %0.2f V" % max17.voltage_alert_max)

print("")
while True:
    print(f"Battery voltage: {max17.cell_voltage:.2f} Volts")
    print(f"Battery state  : {max17.cell_percent:.1f} %")

    # we can check if we're hibernating or not
    if max17.hibernating:
        print("Hibernating!")

    if max17.active_alert:
        print("Alert!")
        if max17.reset_alert:
            print("  Reset indicator")
            max17.reset_alert = False  # clear the alert

        if max17.voltage_high_alert:
            print("  Voltage high")
            max17.voltage_high_alert = False  # clear the alert

        if max17.voltage_low_alert:
            print("  Voltage low")
            max17.voltage_low_alert = False  # clear the alert

        if max17.voltage_reset_alert:
            print("  Voltage reset")
            max17.voltage_reset_alert = False  # clear the alert

        if max17.SOC_low_alert:
            print("  Charge low")
            max17.SOC_low_alert = False  # clear the alert

        if max17.SOC_change_alert:
            print("  Charge changed")
            max17.SOC_change_alert = False  # clear the alert
    print("")
    time.sleep(1)

View on GitHub

In the max1704x_advanced.py example, the MAX17048 ‎is instantiated on I2C. The chip version and chip ID is printed to the ‎REPL along with thresholds for the alerts that are available in the ‎library.‎

In the loop, the battery's voltage, charge percentage and any active ‎alerts are printed to the REPL every second.‎

Voltage High Alert:‎

alert_11

Voltage Low Alert:‎

alert_12

Hibernating Alert:‎

alert_13

Arduino

Using the MAX17048 with Arduino involves wiring up the sensor to ‎your Arduino-compatible microcontroller, installing ‎the Adafruit_MAX1704X library and running the provided example ‎code.‎

Wiring

Wire as shown for a 5V board like an Uno. If you are using a 3V board, ‎like an Adafruit Feather, wire the board's 3V pin to the MAX17048 ‎VIN.‎

Here is an Adafruit Metro wired up to the MAX17048 using the ‎STEMMA QT connector:‎

  • Board 5V to sensor VIN (red wire)

  • Board GND to sensor GND (black wire)

  • Board SCL to sensor SCL (yellow wire)

  • Board SDA to sensor SDA (blue wire)‎

Plug a 3.7/4.2V lithium polymer or lithium-ion rechargeable battery ‎into either of the JST battery ports.‎

wiring_14

Here is an Adafruit Metro wired up using a solderless breadboard:‎

 

  • Board 5V to sensor VIN (red wire)‎

  • Board GND to sensor GND (black wire)

  • Board SCL to sensor SCL (yellow wire)

  • Board SDA to sensor SDA (blue wire)‎

Plug a 3.7/4.2V lithium polymer or lithium-ion rechargeable battery ‎into either of the JST battery ports.‎

wiring_15

Library Installation

You can install the Adafruit MAX1704X library for Arduino using the ‎Library Manager in the Arduino IDE.‎

install_16

Click the Manage Libraries ... menu item, search for Adafruit ‎MAX1704X, and select the Adafruit MAX1704X library:‎

libraries_17

If asked about dependencies, click "Install all".‎

click_18

If the "Dependencies" window does not come up, then you already ‎have the dependencies installed. ‎

If the dependencies are already installed, you must make sure you ‎update them through the Arduino Library Manager before loading ‎the example!‎

Example Code – Basic

‎Download File

Copy Code
#include "Adafruit_MAX1704X.h"

Adafruit_MAX17048 maxlipo;

void setup() {
  Serial.begin(115200);
  while (!Serial) delay(10);    // wait until serial monitor opens

  Serial.println(F("\nAdafruit MAX17048 simple demo"));

  if (!maxlipo.begin()) {
    Serial.println(F("Couldnt find Adafruit MAX17048?\nMake sure a battery is plugged in!"));
    while (1) delay(10);
  }
  Serial.print(F("Found MAX17048"));
  Serial.print(F(" with Chip ID: 0x")); 
  Serial.println(maxlipo.getChipID(), HEX);
}

void loop() {
  Serial.print(F("Batt Voltage: ")); Serial.print(maxlipo.cellVoltage(), 3); Serial.println(" V");
  Serial.print(F("Batt Percent: ")); Serial.print(maxlipo.cellPercent(), 1); Serial.println(" %");
  Serial.println();

  delay(2000);  // dont query too often!
}

View on GitHub

com_19

Upload the sketch to your board and open up the Serial Monitor ‎‎(Tools -> Serial Monitor) at 115200 baud. You should see the battery's ‎voltage and charge percentage being printed out. You'll see the ‎values change depending on the battery's status.‎

Example Code – Advanced

Download File

Copy Code
#include "Adafruit_MAX1704X.h"

Adafruit_MAX17048 maxlipo;

void setup() {
  Serial.begin(115200);
  while (!Serial) delay(10);    // wait until serial monitor opens

  Serial.println(F("\nAdafruit MAX17048 advanced demo"));

  if (!maxlipo.begin()) {
    Serial.println(F("Couldnt find Adafruit MAX17048?\nMake sure a battery is plugged in!"));
    while (1) delay(10);
  }
  Serial.print(F("Found MAX17048"));
  Serial.print(F(" with Chip ID: 0x")); 
  Serial.println(maxlipo.getChipID(), HEX);

  // Quick starting allows an instant 'auto-calibration' of the battery. However, its a bad idea
  // to do this right when the battery is first plugged in or if there's a lot of load on the battery
  // so uncomment only if you're sure you want to 'reset' the chips charge calculator.
  // Serial.println("Quick starting");
  // maxlipo.quickStart();
  
  // The reset voltage is what the chip considers 'battery has been removed and replaced'
  // The default is 3.0 Volts but you can change it here: 
  //maxlipo.setResetVoltage(2.5);
  Serial.print(F("Reset voltage = ")); 
  Serial.print(maxlipo.getResetVoltage());
  Serial.println(" V");

  // Hibernation mode reduces how often the ADC is read, for power reduction. There is an automatic
  // enter/exit mode but you can also customize the activity threshold both as voltage and charge rate

  //maxlipo.setActivityThreshold(0.15);
  Serial.print(F("Activity threshold = ")); 
  Serial.print(maxlipo.getActivityThreshold()); 
  Serial.println(" V change");

  //maxlipo.setHibernationThreshold(5);
  Serial.print(F("Hibernation threshold = "));
  Serial.print(maxlipo.getHibernationThreshold()); 
  Serial.println(" %/hour");

  // You can also 'force' hibernation mode!
  // maxlipo.hibernate();
  // ...or force it to wake up!
  // maxlipo.wake();

  // The alert pin can be used to detect when the voltage of the battery goes below or
  // above a voltage, you can also query the alert in the loop.
  maxlipo.setAlertVoltages(2.0, 4.2);

  float alert_min, alert_max;
  maxlipo.getAlertVoltages(alert_min, alert_max);
  Serial.print("Alert voltages: "); 
  Serial.print(alert_min); Serial.print(" ~ "); 
  Serial.print(alert_max); Serial.println(" V");
}

void loop() {
  Serial.print(F("Batt Voltage: ")); Serial.print(maxlipo.cellVoltage(), 3); Serial.println(" V");
  Serial.print(F("Batt Percent: ")); Serial.print(maxlipo.cellPercent(), 1); Serial.println(" %");
  Serial.print(F("(Dis)Charge rate : ")); Serial.print(maxlipo.chargeRate(), 1); Serial.println(" %/hr");

  // we can check if we're hibernating or not
  if (maxlipo.isHibernating()) {
    Serial.println(F("Hibernating!"));
  }


  if (maxlipo.isActiveAlert()) {
    uint8_t status_flags = maxlipo.getAlertStatus();
    Serial.print(F("ALERT! flags = 0x"));
    Serial.print(status_flags, HEX);
    
    if (status_flags & MAX1704X_ALERTFLAG_SOC_CHANGE) {
      Serial.print(", SOC Change");
      maxlipo.clearAlertFlag(MAX1704X_ALERTFLAG_SOC_CHANGE); // clear the alert
    }
    if (status_flags & MAX1704X_ALERTFLAG_SOC_LOW) {
      Serial.print(", SOC Low");
      maxlipo.clearAlertFlag(MAX1704X_ALERTFLAG_SOC_LOW); // clear the alert
    }
    if (status_flags & MAX1704X_ALERTFLAG_VOLTAGE_RESET) {
      Serial.print(", Voltage reset");
      maxlipo.clearAlertFlag(MAX1704X_ALERTFLAG_VOLTAGE_RESET); // clear the alert
    }
    if (status_flags & MAX1704X_ALERTFLAG_VOLTAGE_LOW) {
      Serial.print(", Voltage low");
      maxlipo.clearAlertFlag(MAX1704X_ALERTFLAG_VOLTAGE_LOW); // clear the alert
    }
    if (status_flags & MAX1704X_ALERTFLAG_VOLTAGE_HIGH) {
      Serial.print(", Voltage high");
      maxlipo.clearAlertFlag(MAX1704X_ALERTFLAG_VOLTAGE_HIGH); // clear the alert
    }
    if (status_flags & MAX1704X_ALERTFLAG_RESET_INDICATOR) {
      Serial.print(", Reset Indicator");
      maxlipo.clearAlertFlag(MAX1704X_ALERTFLAG_RESET_INDICATOR); // clear the alert
    }
    Serial.println();
  }
  Serial.println();
  Serial.println();

  delay(2000);  // dont query too often!
}

View on GitHub

com_20

Upload the sketch to your board and open up the Serial Monitor ‎‎(Tools -> Serial Monitor) at 115200 baud. You should see the battery's ‎voltage, charge percentage, charge/discharge rate and any alert ‎status messages being printed out. You'll see the values change ‎depending on the battery's status.‎

WipperSnapper

wippersnapper_21

What is WipperSnapper

WipperSnapper is a firmware designed to turn any WiFi-capable ‎board into an Internet-of-Things device without programming a ‎single line of code. WipperSnapper connects to Adafruit IO, a ‎web platform designed (by Adafruit!) to display, respond, ‎and interact with your project's data.‎

Simply load the WipperSnapper firmware onto your board, add ‎credentials, and plug it into power. Your board will automatically ‎register itself with your Adafruit IO account.‎

From there, you can add components to your board such as buttons, ‎switches, potentiometers, sensors, and more! ‎Components are dynamically added to hardware, so you ‎can immediately start interacting, logging, and streaming the data ‎your projects produce without writing code.‎

If you've never used WipperSnapper, click below to read through the ‎quick start guide before continuing.‎

Quickstart: Adafruit IO WipperSnapper

Wiring

First, wire up a MAX17048 to your board exactly as follows (note that ‎some boards might already have the sensor integrated on the PCB.)‎

Here is an example of the MAX17048 wired to an Adafruit ESP32 ‎Feather V2 using I2C with a STEMMA QT cable (no soldering required.)

  • Board 3V to sensor VIN (red wire on STEMMA QT)

  • Board GND to sensor GND (black wire on STEMMA QT)‎

  • Board SCL to sensor SCL (yellow wire on STEMMA QT)

  • Board SDA to sensor SDA (blue wire on STEMMA QT)‎

diagrams_22

diagrams_23

Usage

Connect your board to Adafruit IO Wippersnapper and navigate to ‎the WipperSnapper board list.‎

On this page, select the WipperSnapper board you're using to be ‎brought to the board's interface page.‎

page_24

If you do not see your board listed here - you need to connect your ‎board to Adafruit IO first.‎

On the device page, quickly check that you're running the latest ‎version of the WipperSnapper firmware.‎

The device tile on the left indicates the version number of the ‎firmware running on the connected board.‎

tile_25

tile_26

Next, make sure the sensor is plugged into your board and click ‎the I2C Scan button.‎

button_27

You should see the MAX17048's default I2C address of 0x36 pop-up in ‎the I2C scan list.‎

list_28

I don't see the sensor's I2C address listed!‎

First, double-check the connection and/or wiring between the sensor ‎and the board.‎

Then, reset the board and let it re-connect to Adafruit IO ‎WipperSnapper.‎

With the sensor detected in an I2C scan, you're ready to add the ‎sensor to your board.‎

Click the New Component button or the + button to bring up the ‎component picker.‎

picker_29

Adafruit IO supports a large amount of components. To quickly find ‎your sensor, type MAX17048 into the search bar, then select ‎the MAX17048 component.‎

search_30

On the component configuration page, the MAX17048's sensor ‎address should be listed along with the sensor's settings.‎

The Send Every option is specific to each sensor's measurements. ‎This option will tell the Feather how often it should read from the ‎MAX17048 sensor and send the data to Adafruit IO. Measurements ‎can range from every 30 seconds to every 24 hours.‎

For this example, set the Send Every interval to every 30 seconds.‎

page_31

Your device interface should now show the sensor components you ‎created. After the interval you configured elapses, WipperSnapper ‎will automatically read values from the sensor(s) and send them to ‎Adafruit IO.‎

interface_32

To view the data that has been logged from the sensor, click on the ‎graph next to the sensor name.‎

interface_33

Here you can see the feed history and edit things about the feed ‎such as the name, privacy, webhooks associated with the feed and ‎more. If you want to learn more about how feeds work, check out ‎this page.‎

feed_34

Downloads

Files

Schematic and Fab Print

scheme_35

fab_36

‎3D Model‎

model_37

Número de parte del fabricante 4714
JST-PH 2-PIN JUMPER CABLE - 100M
Adafruit Industries LLC
Número de parte del fabricante 5580
ADAFRUIT MAX17048 LIPOLY / LIION
Adafruit Industries LLC
Número de parte del fabricante 4399
STEMMA QWIIC JST SH CABLE 50MM
Adafruit Industries LLC
Número de parte del fabricante 4397
STEMMA QT QWIIC JST SH CABLE 150
Adafruit Industries LLC
Número de parte del fabricante 4398
CBL ASSY RECT 4P PL-GATOR 0.49'
Adafruit Industries LLC
Número de parte del fabricante 4210
JST SH 4-PIN CABLE - QWIIC COMPA
Adafruit Industries LLC
Número de parte del fabricante 5400
ESP32 FEATHER V2 STEMMA QT
Adafruit Industries LLC
$19.95
Ver más Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.