Will You Be Using Matter to Make IoT Devices in 2023?

You’ll be hearing a lot about Matter in 2023; will you also be using it? The 1.0 specification was announced by the Connectivity Standards Alliance in October 2022 as an interoperable application layer software suite designed to simplify the development of secure Internet of Things (IoT) and smart home devices. It operates over Ethernet, Wi-Fi, and Thread and uses Bluetooth Low Energy (BLE) for device commissioning. Matter uses bridging to integrate seamlessly with existing IoT networks like Amazon Alexa, Apple HomeKit, Google Home, Samsung SmartThings, and other platforms like Z-Wave and Wi-SUN.

Let’s review the basic structure of the Matter software stack, look at how Matter networks function, and how Matter integrates existing IoT networks. We’ll close by presenting Matter compatible devices from NXP and Silicon Laboratories, along with development platforms that support the rapid development of Matter-based IoT devices.

What is Matter?

Matter is an exciting opportunity for smart home developers, and if you use it, you’ll be in good company. It’s an open-source protocol managed by the CSA that is designed to act as a control layer to connect and manage smart home devices. It supports existing platforms and sharing of control between the platforms with multiple administration functions. It sits below the application layer and provides a common interface to the TCP and UDP layers in the IPv6 communications stack (Figure 1). It’s licensed under Apache 2.0, has global membership, and is supported by some of the biggest companies in the smart home arena.

Figure 1: Matter sits below the application layer (not shown) and interfaces with the TCP and UDP functions in the IPv6 layer. (Image source: NXP Semiconductors)

So, how does Matter work?

The top layer of the Matter stack is the Data Model that defines the action and data elements available with the Application. Once a data or action element has been received by the Data Model layer, it’s structured and passed to the Interaction Model layer that defines the corresponding interactions, such as reading or writing information. Next, Action Framing packages the defined interactions, making them suitable for encoding and network transmission. Security is a very important element of Matter. The Action Framing layer passes the packaged interactions to the Security layer for encryption and the addition of an authentication code to enable the receiving device to authenticate the transmission.

In the final step, Matter’s Message layer creates an encrypted communications payload that is suitable for passing to the transport layer for transmission. When a message is received, it goes through the reverse process, beginning with decryption and authentication and then moving up the stack to the Application.

What does a Matter network comprise?

A Matter 1.0 network can include six types of devices:

  • Thread sleepy End Nodes that include sensors and actuators
  • Edge Nodes are Thread based sensors or actuators that connect to End Nodes and can function as Thread mesh extenders and connect to Gateways or Thread border routers
  • Thread Border Routers connect the Wi-Fi and Thread networks
  • Gateways connect the Matter network to the cloud
  • Bridges provide a connection between legacy networks and a Matter network
  • Controllers are used to provision Matter devices to the system

Making things with Matter

Now that we’ve reviewed some Matter basics, let’s look at two development kits you can use to kickstart a Matter development program.

First is the IOTZTB-DK006 development kit from NXP that supports the development of battery-powered devices (Figure 2). It’s designed for use with the K32W061 and K32W041 Wireless MCUs, such as the K32W041AMZ and the K32W041AZ. These ultra-low-current wireless devices support Zigbee 3.0, Thread, IEEE 802.15.4, and BLE. The dev kit makes it easy for you to get started working with Matter. It includes:

  • Three motherboards
  • One NFC reader board
  • One generic switch expansion board
  • One light/sensor expansion board
  • Three K32W061 upgrade boards
  • Three JN5189 upgrade boards
  • One K32W USB dongle
  • Three USB cables

Figure 2: You can use NXP’s IOTZTB-DK006 dev kit to develop battery-powered Matter devices. (Image source: NXP Semiconductors)

Developing AC powered Matter devices

If you’re interested in developing AC-powered Matter devices like gateways, smart lights, and voice assistants, you can use the SLWSTK6006A mesh starter kit with the SLWRB4181C radio board from Silicon Labs to evaluate the EFR32xG21 Wireless Gecko Series 2 system on chip (SoC) devices. An example from the line is the EFR32MG21A010F1024IM32-BR MCU with an 80 megahertz (MHz) Arm Cortex-M33 and a 2.4 gigahertz (GHz) radio (Figure 3). Support software includes design tools, precompiled demos, application notes, and examples. You’ll also have access to advanced tools like network analysis and energy profiling. RF performance includes +20 decibels referenced to one milliwatt (dBm) output power and up to +124.5 dB link budget.

Figure 3: The SLWSTK6006A dev kit supports the development of AC-powered Matter devices. (Image source: Silicon Labs)

Conclusion

Matter is an exciting opportunity for designers of smart home IoT devices. Using it, you can develop interoperable smart home networks that integrate seamlessly, regardless of device manufacturer or wireless interface. Development platforms that support battery and AC-powered Matter designs and provide extensive software and applications support are readily available to help you get started.

Recommended reading

IoT Security Fundamentals—Part 1: Using Cryptography

Acerca de este autor

Image of Jeff Shepard

Jeff ha estado escribiendo sobre electrónica de potencia, componentes electrónicos y otros temas de tecnología durante más de 30 años. Empezó a escribir sobre electrónica de potencia como editor senior en el EETimes. Posteriormente fundó Powertechniques, una revista de diseño de electrónica de potencia, y más tarde fundó Darnell Group, una empresa global de investigación y publicación de electrónica de potencia. Entre sus actividades, el Grupo Darnell publicó PowerPulse.net, que proporcionaba noticias diarias a la comunidad mundial de ingeniería en electrónica de potencia. Es el autor de un libro de texto sobre fuentes de alimentación conmutadas, titulado "Fuentes de alimentación", publicado por la división Reston de Prentice Hall.

Jeff también cofundó Jeta Power Systems, un fabricante de fuentes de alimentación conmutadas de alto voltaje, que fue adquirido por Computer Products. Jeff es también un inventor, ya que su nombre figura en 17 patentes de los Estados Unidos en los campos de la recolección de energía térmica y los metamateriales ópticos, y es una fuente de la industria y un frecuente orador sobre las tendencias mundiales en la electrónica de potencia. Tiene una maestría en Métodos cuantitativos y Matemáticas de la Universidad de California.

More posts by Jeff Shepard
 TechForum

Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.

Visit TechForum