Johanson Technology's 2450AT42E010xx Chip Antenna

Johanson Technology's 2450AT42E010xx Chip Antenna (Image source: Johanson Technology)

Miniature ceramic RF chip antennas are commonly used in 2.4 GHz wireless applications such as Bluetooth, WiFi, and ZigBee because they are low cost and small in physical size. Johanson Technology’s 2450AT42E010xx chip antennas have these features, but also provide another unique benefit. The antennas were specifically designed for applications where metal is directly underneath the antenna and is actually required for the antenna to perform optimally. The benefit of this characteristic is that the performance of the antenna will not be negatively affected by proximity to a coin cell battery or display containing metal. This allows smaller PCB designs and provides flexibility in the form factor and placement of the end product.

More information about this product can be found on EEWiki, and if there are any questions, feel free to ask them in the TechForum.

Acerca de este autor

Image of Scott Raeker

Scott Raeker, ingeniero de Aplicaciones principales en DigiKey, ha trabajado en la empresa desde 2006 y su principal responsabilidad es ayudar a los clientes en el mundo inalámbrico. Tiene más de 35 años de experiencia en la industria electrónica y se graduó como ingeniero eléctrico en la Universidad de Minnesota. En su tiempo libre, Scott disfruta arreglar su granja de principios de siglo.

More posts by Scott Raeker
 TechForum

Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.

Visit TechForum