Use Rugged Modules to Move Industrial I/O Closer to the Machine

When I started working on control systems, input/output (I/O) was typically centralized in a few control cabinets. That might have sufficed in the analog days (yes, I’m showing my age), but modern control systems must manage more endpoints across increasingly diverse environments. As a result, many designers are turning to machine-mount remote I/O.

How machine-mount remote I/O works

As the name suggests, this approach relocates I/O modules from the control cabinet and mounts them on or near the sensors and actuators they connect to. These distributed I/O modules offer several compelling benefits:

  • Reduced wiring costs: Machine-mount I/O reduces the need for long, complex cable runs, cutting both material and labor costs.
  • Space savings: Smaller control cabinets make it easier to squeeze more I/O into space-restricted environments.
  • Support for Industry 4.0: These modules enable real-time data collection and diagnostics for what were once simple sensors and actuators.

Because machine-mount remote I/O lacks the protection of a cabinet, it must be ruggedized to withstand harsh environments. The new ADAM-200PN series from Advantech demonstrates how this is achieved:

  • Ruggedized design: The modules carry an IP67 rating for resistance to dust and water ingress. They operate across a temperature range of -40 to 60°C and are designed for demanding transportation and industrial environments, with EN 50155 compliance and vibration/shock testing for high-vibration applications.
  • M12 connectors: The modules support screw-lock and push-pull fast-lock M12 connectors for fast, secure installation. D, A, and L-coded connectors ensure the appropriate cables are used for networking, I/O, and power, respectively.
  • Multiple mounting options: Front, sidewall, and direct machine mounting are supported for cabinet-free installation.

The ADAM-250PN-A (Figure 1) is the first member of the ADAM-200PN series. It features 16 configurable digital I/O channels, with support for IEC 61131-2 Type 3 sink digital inputs and fast-response source digital outputs for reliable industrial signaling. For network connectivity, the module natively supports both PROFINET and Modbus/TCP, ensuring compatibility with a wide range of industrial Ethernet controllers.

Figure 1 : The ADAM-250PN-A provides dual Ethernet and power ports and 16 I/O channels, all via M12 connectors. (Image source: Advantech)

How the ADAM-250PN-A supports distributed I/O at scale

A key feature of the ADAM-250PN-A is its support for daisy-chaining (Figure 2). The module provides dual Ethernet ports and a built-in switch, allowing multiple modules to be connected in series. This can significantly reduce cabling compared with a star topology, in which each module requires its own home-run cable back to the control cabinet.

Figure 2 : Daisy-chain Ethernet and power connections allow multiple distributed I/O modules to be placed near field devices while reducing home-run cabling to the control cabinet. (Image source: Advantech)

Power can also be daisy-chained using the module’s 24 volt DC (VDC) power I/O ports, subject to normal power budget and voltage-drop considerations.

The module also provides power to sensors, actuators, and encoders from each I/O port, organized into two power domains: US for the system and sensor supply, and UA for the actuator and load supply. This further simplifies wiring by reducing the need for separate local power supplies. The US half can output up to 0.5 amperes (A) per channel. The UA half can output up to 2 A per channel, allowing the module to directly drive devices such as solenoid valves, DC contactors, and indicator lights.

Additionally, the module provides I/O and power diagnostics, LED status indication, and configurable output behavior during controller faults. These features matter in distributed systems because faults are no longer concentrated in one cabinet. Instead, technicians need local and network-visible indicators to quickly identify wiring, power, and channel-level problems.

Applications that benefit from machine-mount I/O

Thanks to its daisy-chaining capability, the ADAM-250PN-A is particularly suited for deployments where sensors and actuators are distributed across large sites. Wind turbines and other renewable energy assets are good examples, as these large-scale installations can benefit from a significant reduction in wiring complexity.

The use of M12 connectors makes the module a good match for equipment that is frequently reconfigured or moved because they enable quick connection and disconnection. Examples include outdoor material-handling systems, harbor cranes, and port automation.

Even when the ADAM-250PN-A is installed in a cabinet, its ruggedized design still provides benefits. For example, because the I/O module does not require a clean, dry, vibration-free environment, designers can relax some cabinet requirements. This is an important consideration for areas such as railway way-sides and food and beverage washdown zones.

Conclusion

Unlike my younger self, today’s control and automation designers are no longer confined to massive control cabinets with wires routed back from every sensor and actuator. Machine-mount I/O modules, such as the rugged Advantech ADAM-250PN-A, can simplify cabling, enable more flexible installations, and bring industrial Ethernet connectivity closer to the machine.

Acerca de este autor

Image of Kenton Williston

Kenton Williston se licenció en Ingeniería eléctrica en 2000 y comenzó su carrera como analista de referencias de procesadores. Desde entonces ha trabajado como redactor en el grupo EE Times y ha ayudado a lanzar y dirigir múltiples publicaciones y conferencias al servicio de la industria electrónica.

More posts by Kenton Williston
 TechForum

Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.

Visit TechForum