New Product Discoveries - Hillcrest Laboratories' BN0080 IMU and Bosch's Transport Data Logger

You want the most advanced technology at the lowest possible cost. At DigiKey we understand this, which is why we strive to offer the widest breadth of cutting-edge electronic components from over 750 of the world’s leading suppliers. The New Product Discovery series showcases some of the newest and most interesting technology on the market today.

Today I have two new products I’m sure will grab your interest. The first device is from Hillcrest Laboratories in the form of a System-in-Package, or SIP. A SIP is a way of packaging multiple kinds of devices in one package for space savings and efficiency. For example, you might have a power device alongside a microprocessor next to an analog device. Each element is its own die; however, they are packaged together in the same enclosure appearing as one integrated circuit.

That being said, the SIP device I have today is the BNO080 Inertial Measurement Unit or IMU. This IMU is made up of a 32-bit ARM processor, tri-axial accelerometer, tri-axial gyroscope, and a tri-axial magnetometer giving you a complete 9 degrees of freedom. Popular applications include VR (virtual reality) headsets, drones, and robotics. The BNO080 is android compatible and has built-in memory allowing it to be programmed directly; it has field programming capabilities for firmware updates as well. Scott, one of our Applications Engineers, provides an in-depth look at the BNO080 in his blog post.

The second device I want to make you aware of is the TDL110 Transport Data Logger from Bosch Connected Devices and Solutions. We know that our customers come from varied backgrounds, and, in order to better support those of you in an industrial automation setting, we have been taking on suppliers with a focus on this industry. The TDL110 is a battery-operated data logger that is capable of saving the contents in memory for up to two years (based on standard usage). This device can record shock, humidity, temperature, and tilt. The data is then able to be wirelessly pulled from the data logger via a Bluetooth link. If you are looking for more information on transport data loggers check out the TDL110 blog from our AE Technician Lindsay.

Thank you for watching!

 

Acerca de este autor

Image of Randy Restle

Randall Restle tiene más de 40 años de experiencia en la industria de los componentes electrónicos. Ahora está semijubilado y se desmpeñó como Vicepresidente de Ingeniería de Aplicaciones de DigiKey. Su experiencia incluye la dirección de equipos de ingenieros de aplicación, técnicos y personal de gestión cualificados para desarrollar productos originales y únicos de tecnología avanzada.

Sus actividades personales incluyen el procesamiento de señales digitales, la implementación de lógica programable, mejoras en el control del movimiento y el diseño de software. Es titular de patentes en múltiples industrias y es miembro senior del IEEE. Randall tiene títulos de BSEE, MS y MBA de la Universidad de Cincinnati.

More posts by Randall Restle
 TechForum

Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.

Visit TechForum