Basics of USB

Choosing the correct USB can be a difficult task, especially for someone who is unfamiliar with all the different types. An article I recently wrote lays out the background of USBs and the different options, along with a visual providing what the male and female version of each looks like. Some of the more widely used types are called out below to help ease the selection process.


  • Type A
    • Flash Drive
    • Power Cables

  • Type Micro B
    • Cell phone charging

  • Type C
    • Newly adopted as cell phone charging connectors
    • Only current reversible option

There are many other types covered in the article, along with the different speeds each type is capable of supporting, a bit of history on the connector, and links to the product on DigiKey’s website. Shown in the image is a Type A Male to Type Micro B Male cable assembly.

Acerca de este autor

Image of Ashley Awalt

Ashley Awalt es una técnica de ingeniería de aplicaciones que ha estado con DigiKey desde 2011. Obtuvo su título de Asociada de Ciencias Aplicadas en Tecnología Electrónica y Sistemas Automatizados del Northland Community & Technical College a través del programa de becas DigiKey. Su papel actual es ayudar a crear proyectos técnicos únicos, documentar el proceso y, en última instancia, participar en la producción de la cobertura de los medios de comunicación de vídeo para los proyectos. En su tiempo libre, a Ashley le gusta - oh, espera, ¿hay tal cosa como el tiempo libre cuando eres madre?

More posts by Ashley Awalt
 TechForum

Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.

Visit TechForum