What is the Capacitance of this Capacitor?

Por Steve Maloy, TDK Components USA, Inc.

Frequently asked questions regarding aging and its effect on capacitance.

Question 1: What is “aging”?

Aging is generally referred to as a decrease in capacitance over time in EIA Class II capacitors. It is a natural and unavoidable phenomenon that occurs in all ferroelectric formulations used as the dielectric material. Aging is reversible and occurs due to changes in the dielectric’s crystal structure with temperature and time. Aging is typically reported as a percent capacitance loss per decade of time. Because aging is logarithmic in nature, the loss of capacitance is greatest in the first 10 hours of age.

Graph of capacitance aging characteristic

Figure 1: Capacitance aging characteristic.

Note: The dissipation factor also ages, decreasing several times faster than the capacitance. Also, EIA Class III and IV also exhibit aging characteristics. Industry “official” definitions of aging can be found in EIA-521 and IEC-384-9.

Question 2: What is the difference between a Class I capacitor and a Class II capacitor?

A Class I capacitor1 (C0G, C0H, C0K, etc.) is made from ceramic materials that are not sensitive to temperature changes, thus the capacitance value of a capacitor measured at a low temperature (example -25°C) will not significantly vary from the same capacitor measured at a higher temperature (ex. 75°C). EIA refers to these as “temperature compensating,” and are measured in ppm/°C. These capacitors typically have low capacitance values because of the ceramic material used to manufacture them but they exhibit nearly perfect capacitance stability regardless of their temperature, making them an excellent choice for applications in which frequency control is needed such as in radio or television tuners. An example of such is found below:

  • C0G = ±30 PPM over a temperature range of -55°C to +85°C

A Class II capacitor2 (X5R, X6S, X7R) is made from ceramic materials that are derived from a barium titanate base which is temperature sensitive. Thus the various temperature classifications stating the extent of the sensitivity over a given temperature range. These capacitors allow for larger capacitance values in the small surface-mount packages.

Examples of Class II Temperature Characteristics3 are below:

  • X5R = ±15% over a temperature range of -55°C to +85°C
  • X6S = ±22% over a temperature range of -55°C to +105°C
  • X7R = ±15% over a temperature range of -55°C to +125°C

Additionally, capacitors made from barium titanate bases (Class II, III, and IV) are ferroelectric and therefore susceptible to “aging” in which a capacitor’s ability to hold capacitance will decrease over time if left in an unheated and/or uncharged state. Class I capacitors are not ferroelectric and therefore do not age.

Question 3: Why and how do capacitors of barium titanate age?

Over time, the internal molecular structure changes in such a way as to create an alignment of electrical dipoles. This alignment results in a molecular structure that can hold less electrical charge than when the molecules are in a totally random state, such as at the time of heating or mounting (soldering) on a printed circuit board.4

Diagram of alignment of electric dipoles

Figure 2: Alignment of electric dipoles.

Question 4: What is de-aging?

De-aging is a heat treatment used to reset the aging phenomena. Simply put, it restarts the aging process, but it does not prevent it. Heating the capacitor above its Curie Temperature causes the crystalline structure to return to its optimum unaligned configuration resulting in maximum capacitance. TDK recommends 150°C/1 hour for de-aging. Note: It is important to record the time of last heat (TOLH), or de-aging time, for future capacitance measurements.

Question 5: Is “aging” just a TDK phenomenon?

No. The “aging” that is observed is common to all manufacturers of Class II, III, and IV ceramic capacitors. Since aging is formulation dependent, the aging rate will vary from manufacturer to manufacturer.

Question 6: How does a capacitor manufacturer compensate for aging?

Since the capacitance of BaTiO3-based capacitors changes with time, aging poses a unique problem for component manufacturers – that is, ‘what is the capacitance of this capacitor?’

Like voltage and frequency test conditions, the industry has long recognized the aging issue and has determined a standard by which all capacitors should be measured: IEC-384-9. Simply stated the capacitance must be within the specified tolerance at 1000 hours age (or TOLH).5

The capacitor manufacturer uses the material’s known aging rate and mathematically determines the capacitance tolerance limits for any point in time after de-aging (see Figures 3 and 4 below). The components are 100% electrically sorted with respect to their aging rate and TOLH. For example, a +/-10% tolerance part may be sorted at +13/-7% if the dielectric material’s aging rate is 3%. By utilizing this technique manufacturers can guarantee all capacitors to be within cap tolerance at 1000 hours based on TOLH.

Image of example sorting limits for Class I material

Figure 3: Example sorting limits for Class I material, K Tolerance.

Graph of example sorting limits for Class II material

Figure 4: Example sorting limits for Class II material, K Tolerance.

NOTE : Because aging causes a decrease in capacitance over time, it is possible for the capacitance to be above the upper tolerance limit at times less than 1000 hours from TOLH, and less than the lower tolerance limit at times greater than 1000 hours from TOLH.

Question 7: How should a capacitor user compensate for aging?

The capacitor user should expect the Class II, III, and IV capacitors to be within cap tolerance ~ 6 weeks (1000 hrs) from TOLH, the approximate lead time of most components from manufacturer to user. The capacitor user should not expect the Class II, III, or IV component to be within the cap tolerance immediately after solder, glue curing, or any other elevated temperature processes (capacitor will have consequently de-aged).

In predicting aging/de-aging behavior, in circuit test systems may need to be widened to allow for capacitor aging.

References:

  1. EIA-198-D, Page I-1
  2. EIA-198-D, Page I-1
  3. EIA-198-D, Page I-3
  4. Halliday and Resnick, Fundamentals of Physics, 2nd Edition, 1981, Page 492
  5. IEC-384-9 (1988), Appendix A

Acknowledgements:

  1. Gene Williams, TDK Components USA, Inc.

Descargo de responsabilidad: Las opiniones, creencias y puntos de vista expresados por los autores o participantes del foro de este sitio web no reflejan necesariamente las opiniones, las creencias y los puntos de vista de DigiKey o de las políticas oficiales de DigiKey.

Acerca de este autor

Steve Maloy, TDK Components USA, Inc.