Thermal Optimization of GaN HEMT Transistor Power Amplifiers

Por Cree, Inc.

Colaboración de DigiKey

Gallium nitride power transistors have very high RF power densities which range from 4 to 12 watts per mm of gate periphery, depending on operating drain voltage. Even though GaN/AIGaN on SiC substrates have high thermal conductivity, it is necessary to be aware of channel temperature rise incurred by both DC and RF stimuli when designing power amplifiers. Thermal management is even more important for broadband amplifiers (a very popular application), where drain efficiencies can vary considerably as a function of frequency.

A new self-heating feature in Cree's GaN HEMT large-signal models automatically affects both DC and RF parameters as a function of transistor drawn current. We will use the CGH40025F transistor in a 2 to 6 GHz broadband amplifier and demonstrate how the transistor operating temperature can be minimized during the simulation phase of the design. The default thermal resistance is set for the CGH40025F at 4.8°C/watt. The operating case temperature (Tease) is user defined. The self-heating engine automatically calculates the rise in temperature (Trise) of the HEMT channel above Tease.

Trise can be used as a function of other parameters such as frequency, output power, and efficiency. This article will show the direct lowering of Trise using optimization in unison with the maintenance of output power. Such thermal optimization assures reliable operation as well as improved performance since the transistors are operating cooler.

Basic amplifier design

2 GHz to 6 GHz demonstration amplifier simulation

2 to 6 GHz, 25 W Broadband PA Schematic (click for full-size)

Figure 1: 2 to 6 GHz, 25 W broadband PA schematic.


Figure 1 shows the basic schematic of a broadband, 2 to 6 GHz power amplifier utilizing a Cree CGH40025F GaN HEMT transistor. This device operates from a nominal 28 volt rail. The transistor symbol in the schematic shows a four port device - gate, drain, source and temperature monitor - a voltmeter serves as the "thermometer".

Initial circuit design was concentrated on achieving broadband and flat, small-signal gain across the required frequency range (Figure 2). The power transfer characteristics of the amplifier were then simulated. For example, at a constant CW input power of 38 dBm the output power is plotted as a function of frequency in Figure 3 where it can be seen that the output power varies somewhat due to different levels of compression and impedance match.

Simulated performance prior to optimization

521, 511 and 522 prior to optimization

Figure 2: 521, 511 and 522 prior to optimization.

Output Power vs. frequency

Figure 3: Output Power vs. frequency at Pin=38 dBm prior to optimization.

The self-heating feature of the large-signal model automatically calculates the thermal rise in the transistor from package flange to channel. This is shown in Figure 4 for the amplifier before any specific attention has been taken to decreasing operating drain current. Optimization parameters were set up in Microwave Office for output power, gain and temperature rise as a function of frequency. The intention of the optimization is to ensure that the transistor's channel temperature never exceeds 225°C at a case temperature of 85°C (i.e., a temperature rise of 140°C).

Transistor temperature rise

Figure 4: Transistor temperature rise above Tease prior to optimization.

Following thermal optimization, the small signal parameters are re-simulated as shown in Figure 5, where there is little change in gain and some improvement in output return loss. Figure 6 shows the CW output power as a function of frequency- again there is general improvement in output power over the band even though the "profile" has changed.

521, 511 and 522 after optimization

Figure 5: 521, 511 and 522 after optimization.

Output Power vs. frequency

Figure 6: Output Power vs. frequency at Pin=38 dBm after optimization.

Figure 7 is a plot of transistor drain current as a function of frequency which indicates drain current reduction of as much as 12% compared to the original design. Figure 8 indicates the temperature rise after thermal optimization showing temperature decreases of as much as 35°C compared to the original design.

Drain current vs. frequency

Figure 7: Drain current vs. frequency at Pin of 38 dBm after optimization.

Transistor temperature rise

Figure 8: Transistor temperature rise above Tease after optimization.

This article has shown a demonstration of how to use the self-heating feature of Cree's large-signal GaN HEMT models to calculate transistor temperature rise as a function of other parameters such as frequency and RF power level. Specifically, the self-heating engine has been used, via optimization, to lower transistor temperature by minimizing Trise while maintaining output power.
 
DigiKey logo

Descargo de responsabilidad: Las opiniones, creencias y puntos de vista expresados por los autores o participantes del foro de este sitio web no reflejan necesariamente las opiniones, las creencias y los puntos de vista de DigiKey o de las políticas oficiales de DigiKey.

Acerca de este autor

Cree, Inc.

Acerca de este editor

DigiKey

DigiKey, con sede en Thief River Falls, Minnesota, es un proveedor global de servicios completos de prototipo y diseño, así como de volúmenes de producción de componentes electrónicos que ofrece más de tres millones de productos de más de 750 fabricantes de marcas de calidad en DigiKey.