LED Specs - Understanding the Color White

Por Richard Comerford

Colaboración de Electronic Products


When LEDs were primarily used as indicators on electronic equipment, a color palette of green, amber, and red was enough. And it wasn’t all that important that the color indicators be precisely consistent from one LED to the next. But with the adoption of LEDs for general lighting applications, color precision is vital.

Today, lighting system designers for commercial and residential use must be able to specify the precise color of the light source, and be sure the color is consistent from one product to the next. As a result, design engineers must understand exactly how and with what precision the color of light can be specified.

The American National Standards Institute (ANSI) and other standards organizations have defined standards for specifying the color of a light source’s output. Although the basis for the standards dates to early in the last century, they are continuously being refined based on new developments.

The fundamental way of describing color was established by the Commission Internationale de l'Eclairage (International Commission on Lighting, or CIE) in 1931. Space is described in terms of three coordinates – x, y, and z – in which x, y describe the chromaticity (color) while z defines the luminance (brightness). Thus, using the diagram seen in Figure 1, a color could be specified simply by giving its x, y coordinates.

Image

Figure 1: CIE xy 1931 chromaticity diagram including the Planckian locus. Lines crossing the locus are lines of constant correlated color temperature. Monochromatic wavelengths are shown in blue in units of nanometers.

Within the CIE 1931 x, y chromaticity space, a line is drawn to represent the color that an incandescent black-body would appear to radiate with changes in the black body’s temperature (called color temperature and given in kelvins). This line is called the "black body locus" or "Planckian locus". The lines crossing the locus indicate lines of constant correlated color temperature, where the perceived color most closely resembles that of an ideal radiator at the same brightness and under specified viewing conditions.

Color temperatures of interest for most general-purpose white lighting range from 2700 K (the beginning of warm white) through 4000 K (neutral white) to 6500 K (coolest white). The CIE 1931 x, y space is the basis for ANSI’s determination of acceptable color variance among light sources. Figure 2 shows eight quadrilaterals, which define the colors within the nominal CCT space for 2700 K, 3000 K, 3500 K, 4000 K, 4500 K, 5000 K, 5700 K, and 6500 K. Thus any color within the 2700 K quadrilateral can be referred to as having a color temperature of 2700 K.

The quadrilaterals roughly coincide with the lavender ellipses called MacAdam ellipses, named for David Lewis MacAdam, who, in the 1940s at Eastman Kodak, attempted to measure how people perceived variations in color. The size of the ellipse is based on standard variance, called "steps." A one-step MacAdam ellipse is one in which every point of the circumference is exactly one standard variance from the center point. Such a region defines what x, y chromaticity coordinates can be acceptably associated with a target CCT.

The MacAdam ellipses shown in Figure 2 are seven-step ellipses, which the U.S. Department of Energy had set as a standard for compact fluorescent bulbs. The ANSI chromaticity specification was developed to be as consistent as possible with existing fluorescent lamp standards, and to reflect the current and near future state of SSL technology and color binning capabilities. ANSI recommends that lamp manufacturers stay within a four-step ellipse.

Image

Figure 2: CIE 1931 chromaticity diagram with ANSI’s eight nominal CCT quadrangles about the Planckian locus and DOE 7-step MacAdam ellipse for CFL. (Source: "ANSI_NEMA_ANSLG C78.377-2008, American National Standard for electric lamps—Specifications for the Chromaticity of Solid State Lighting Products," Approved January 9, 2008).

According to OSRAM SYLVANIA, this tighter requirement gives lamp manufacturers a fairly wide range of perceptible differences, since a point on the circumference of a four-step ellipse is eight steps from a point directly opposite it on the circumference. For its fine white binning, OSRAM bases its CCT quadrilaterals, commonly referred to as bins, on a three-step ellipse (Figure 3). Other manufacturers, such as Cree and Avago, also use refined binning to provide closer matching of color. Each manufacturer typically publishes these binning charts in their datasheets.

Image

Figure 3: OSRAM chromaticity chart for its white fine binning, with CCT quadrilaterals based on a three-step MacAdam ellipse. (Source: OSRAM)

According to OSRAM, differences in the colors enclosed in a three-step ellipse are indistinguishable by most people. However, some industry professionals claim that under some circumstances, even differences in colors within a two-step ellipse may be discernable. But what is certain is that users can purchase LEDs today and know exactly what color range they will be working with.

References:
  1. "ANSI_NEMA_ANSLG C78.377-2008, American National Standard for electric lamps - Specifications for the Chromaticity of Solid State Lighting Products," American National Standard Lighting Group, 2008
  2. "ENERGY STAR® Program Requirements for Solid State Lighting Luminaires Eligibility Criteria - Version 1.1", December 19, 2008
  3. "The importance of LED color consistency," Michael Godwin, Electronic Products, May 2011
  4. "What are MacAdam Ellipses or color ovals?" FAQ0026-0999, OSRAM SYLVANIA National Customer Support Center, 2000
  5. "MacAdam Ellipses," Mike Wood, Out of the Wood, Fall 2010
  6. "When white light isn’t white," Mike Wood, Out of the Wood, Spring 2008
  7. "ASMT-Ax00 1W Power LED Light Source Data Sheet," Avago Technologies Inc., January 25, 2011
  8. "OSLON SSL Data Sheet," OSRAM Opto Semiconductors GmbH, 2010-09-22
  9. "XLamp XM-L LED Data Sheet," CLD-AP44 Rev 1, Cree Inc., 2011

Descargo de responsabilidad: Las opiniones, creencias y puntos de vista expresados por los autores o participantes del foro de este sitio web no reflejan necesariamente las opiniones, las creencias y los puntos de vista de DigiKey o de las políticas oficiales de DigiKey.

Acerca de este autor

Richard Comerford

Editor Richard Comerford is responsible for Electronic Products magazine’s coverage of lighting and optoelectronics, mechatronics, packaging and enclosures, sensors and transducers, and test and measurement. Comerford is an electrical engineer who has spent more than 30 years writing about electronics for major industry publications and serving as a professional consultant for numerous test and measurement projects.

Acerca de este editor

Electronic Products

La revista Electronic Products y ElectronicProducts.com ofrece ingenieros y gerentes de ingeniería responsables de diseñar equipos y sistemas electrónicos.