Multilayer Ceramic Capacitors (MLCCs)

Por Ashley Awalt

Colaboración de DigiKey

Introduction

This document will cover the basics of multilayer ceramic capacitors, the proper procedure to test them, and a description of the aging/de-aging process.

Description

MLCC (multilayer ceramic capacitors) are the most prevalent capacitors utilized in the electronics industry. Class I ceramic capacitors (ex. NP0, C0G) offer high stability and low losses in resonant circuits, but low volumetric efficiency. These do not require any aging corrections. Class II and Class III (X7R, X5R, etc.) offer high volumetric efficiency, but a lower stability than Class I dielectrics. These can sometimes require aging correction if they are outside of the manufacturer’s referee time. The referee time is the timeframe the manufacturer deems the capacitor to be within the specified tolerance range.

Image of typical MLCC

Figure 1:Typical MLCC

Testing

Most LCR meters are unable to test high value (1 µF and higher) MLCCs due to their internal impedance. The impedance is so low at 1 KHz that it virtually drains the current supplied by the meter, ultimately dropping the specified voltage to 0, never allowing the capacitor to be exposed to the required voltage for testing. To verify, measure the voltage across a capacitor under test with a true RMS meter. If the voltage is less than 0.4 VRMS, the capacitance reading will be low. Select LCR meters have an impedance matching capability function called Automatic Level Control (ALC). These meters will decrease their own impedance until it’s lower than the device being tested. More often than not, this is still not enough and an amplifier unit is necessary to increase the current through the capacitor until the voltage across it reaches a pre-set level from 0.5 VRMS-1 VRMS.

Aging

Capacitors classified as having a high dielectric constant will decrease in capacitance over time. This is typically noted as a percentage drop per decade of time. Temperature compensating capacitors (Class I) don’t have aging characteristics.

De-Aging

If aging has affected a capacitor, it can be reversed by heating it above its Curie temperature. The Curie temperature for most manufacturer specifications is approximately 125°C or higher, and is often achieved during the soldering process. Be sure to check the manufacturer’s specs before attempting this. Heating the capacitor above the Curie temperature will realign the molecular structure of the dielectric material, restoring the MLCCs capacitance. The capacitance will often measure high at this point, and one should wait until the referee time has passed so the capacitor will be within the spec tolerance again. After the capacitor has cooled, the aging process will restart.

References

  1. Kemet Measure Capacitance of Class-II and Class-III Ceramic Capacitors PDF
  2. Murata Ceramic Capacitors FAQ
  3. TDK Corporation Ceramic Capacitors FAQ PDF
  4. DigiKey Testing High Capacitance MLCCs Forum
DigiKey logo

Descargo de responsabilidad: Las opiniones, creencias y puntos de vista expresados por los autores o participantes del foro de este sitio web no reflejan necesariamente las opiniones, las creencias y los puntos de vista de DigiKey o de las políticas oficiales de DigiKey.

Acerca de este autor

Image of Ashley Awalt

Ashley Awalt

Ashley Awalt es una técnica de ingeniería de aplicaciones que ha estado con DigiKey desde 2011. Obtuvo su título de Asociada de Ciencias Aplicadas en Tecnología Electrónica y Sistemas Automatizados del Northland Community & Technical College a través del programa de becas DigiKey. Su papel actual es ayudar a crear proyectos técnicos únicos, documentar el proceso y, en última instancia, participar en la producción de la cobertura de los medios de comunicación de vídeo para los proyectos. En su tiempo libre, a Ashley le gusta - oh, espera, ¿hay tal cosa como el tiempo libre cuando eres madre?

Acerca de este editor

DigiKey

DigiKey, con sede en Thief River Falls, Minnesota, es un proveedor global de servicios completos de prototipo y diseño, así como de volúmenes de producción de componentes electrónicos que ofrece más de tres millones de productos de más de 750 fabricantes de marcas de calidad en DigiKey.